This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TDA4VM:针对 RTOS SDK 测试的 CCS 设置

Guru**** 1456330 points
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1365600/tda4vm-ccs-setup-for-rtos-sdk-test

器件型号:TDA4VM

按照指南在 Ubuntu 22.04上设置 CCS

https://software-dl.ti.com/jacinto7/esd/processor-sdk-rtos-jacinto7/09_02_00_05/exports/docs/psdk_rtos/docs/user_guide/ccs_setup_j721e.html#debugging-without-hlos-running-on-a72-rtos-only-baremetal

脚本控制台:

js:> loadJSfile ("/home/tony/ti/ti-processor-sdk-rtos-j721e-evm-09_02_00_05/pdk_jacinto_09_02_00_30/packages/ti/drv/sciclient/tools/ccsLoadDmsc/j721e/launch.js")
Connecting to DMSC_Cortex_M3_0!
Fill R5F ATCM memory...
Writing While(1) for R5F
Loading DMSC Firmware ... /ti/ti-processor-sdk-rtos-j721e-evm-09_02_00_05/pdk_jacinto_09_02_00_30/packages/ti/drv/sciclient/soc/sysfw/binaries/ti-fs-firmware-j721e-gp.bin
DMSC Firmware Load Done...
DMSC Firmware run starting now...
Running the DDR configuration... Wait till it completes!
Connecting to MCU Cortex_R5_0!
 WKUP Boot Mode is 56
 Main Boot Mode is 65
Disable MCU Timer for ROM clean up
Error evaluating "GEL_Load("/ti/ti-processor-sdk-rtos-j721e-evm-09_02_00_05/pdk_jacinto_09_02_00_30/packages/ti/drv/sciclient/tools/ccsLoadDmsc/j721e/sciclient_ccs_init_mcu1_0_release.xer5f")": Unable to open file: /ti/ti-processor-sdk-rtos-j721e-evm-09_02_00_05/pdk_jacinto_09_02_00_30/packages/ti/drv/sciclient/tools/ccsLoadDmsc/j721e/sciclient_ccs_init_mcu1_0_release.xer5f
     at GEL_Load("/ti/ti-processor-sdk-rtos-j721e-evm-09_02_00_05/pdk_jacinto_09_02_00_30/packages/ti/drv/sciclient/tools/ccsLoadDmsc/j721e/sciclient_ccs_init_mcu1_0_release.xer5f") (/home/tony/ti/ti-processor-sdk-rtos-j721e-evm-09_02_00_05/pdk_jacinto_09_02_00_30/packages/ti/drv/sciclient/tools/ccsLoadDmsc/j721e/launch.js#153)
js:> 

控制台输出停止在下面,我认为问题是路径:/ti/ti-processor-sdk-rtos-j721e-evm-09_02_00_05 ,有时它从系统根目录开始:/home/user ,有时从用户的根目录开始。

DMSC_Cortex_M3_0: GEL Output: Setting DDR PLL + HSDIV to 933MHz
DMSC_Cortex_M3_0: GEL Output: DDR PLL Calibration Control MMR value: 0x80170000
DMSC_Cortex_M3_0: GEL Output: DDR PLL Calibration Control MMR value: 0x80000E17
DMSC_Cortex_M3_0: GEL Output: DDR PLL + HSDIV set to 933MHz.
DMSC_Cortex_M3_0: GEL Output: Frequency change request type 2 received from controller 
DMSC_Cortex_M3_0: GEL Output: Setting DDR PLL + HSDIV to 933MHz
DMSC_Cortex_M3_0: GEL Output: DDR PLL Calibration Control MMR value: 0x80170000
DMSC_Cortex_M3_0: GEL Output: DDR PLL Calibration Control MMR value: 0x80000E18
DMSC_Cortex_M3_0: GEL Output: DDR PLL + HSDIV set to 933MHz.
DMSC_Cortex_M3_0: GEL Output: --->>> All frequency change requests have completed... <<<---
DMSC_Cortex_M3_0: GEL Output: --->>> LPDDR4 Initialization is DONE! <<<---
MCU_Cortex_R5_0: GEL: Unable to open file: /ti/ti-processor-sdk-rtos-j721e-evm-09_02_00_05/pdk_jacinto_09_02_00_30/packages/ti/drv/sciclient/tools/ccsLoadDmsc/j721e/sciclient_ccs_init_mcu1_0_release.xer5f

我更改了用绝对路径替换的行、然后它可以执行到下一个类似的加载固件行。

    if ((bootMode != 0x38) || (mainBootMode != 0x11))
    {
        print("Disable MCU Timer for ROM clean up");
        dsMCU1_0.memory.writeWord(0, 0x40400010, 0x1); /* Write reset to MCU Timer 0. Left running by ROM */
        dsMCU1_0.memory.writeWord(0, 0x40F80430, 0xFFFFFFFF); /* Clear Pending Interrupts */
        dsMCU1_0.memory.writeWord(0, 0x40F80018, 0x0); /* Clear Pending Interrupts */
        // Reset the R5F to be in clean state.
        dsMCU1_0.target.reset();
        // Load the board configuration init file.
        //dsMCU1_0.expression.evaluate('GEL_Load("'+ ccs_init_elf_file +'")');
        dsMCU1_0.expression.evaluate('GEL_Load("/home/tony/ti/ti-processor-sdk-rtos-j721e-evm-09_02_00_05/pdk_jacinto_09_02_00_30/packages/ti/drv/sciclient/tools/ccsLoadDmsc/j721e/sciclient_ccs_init_mcu1_0_release.xer5f")');
        // Run Asynchronously
        dsMCU1_0.target.runAsynch();
        print ("Running Async");
        // Halt the R5F and re-run.
        dsMCU1_0.target.halt();
    }

js:> loadJSfile ("/home/tony/ti/ti-processor-sdk-rtos-j721e-evm-09_02_00_05/pdk_jacinto_09_02_00_30/packages/ti/drv/sciclient/tools/ccsLoadDmsc/j721e/launch.js")
Connecting to DMSC_Cortex_M3_0!
Fill R5F ATCM memory...
Writing While(1) for R5F
Loading DMSC Firmware ... /ti/ti-processor-sdk-rtos-j721e-evm-09_02_00_05/pdk_jacinto_09_02_00_30/packages/ti/drv/sciclient/soc/sysfw/binaries/ti-fs-firmware-j721e-gp.bin
DMSC Firmware Load Done...
DMSC Firmware run starting now...
Running the DDR configuration... Wait till it completes!
Connecting to MCU Cortex_R5_0!
 WKUP Boot Mode is 56
 Main Boot Mode is 65
Disable MCU Timer for ROM clean up
Running Async
Running the board configuration initialization from R5!
Running DDR Memory Checks....
Clearing CLEC Secure Claim...
######################################################################################
Loading Sciserver Application on MCU1_0. This will service RM/PM messages
If you do not want this to be loaded update the launch script to make loadSciserverFlag = 0
If you want to load and run other cores, please run the MCU1_0 core after Sciserver is loaded. 
######################################################################################
Error evaluating "GEL_Load("/ti/ti-processor-sdk-rtos-j721e-evm-09_02_00_05/pdk_jacinto_09_02_00_30/packages/ti/drv/sciclient/tools/ccsLoadDmsc/j721e/sciserver_testapp_freertos_mcu1_0_release.xer5f")": Unable to open file: /ti/ti-processor-sdk-rtos-j721e-evm-09_02_00_05/pdk_jacinto_09_02_00_30/packages/ti/drv/sciclient/tools/ccsLoadDmsc/j721e/sciserver_testapp_freertos_mcu1_0_release.xer5f
	 at GEL_Load("/ti/ti-processor-sdk-rtos-j721e-evm-09_02_00_05/pdk_jacinto_09_02_00_30/packages/ti/drv/sciclient/tools/ccsLoadDmsc/j721e/sciserver_testapp_freertos_mcu1_0_release.xer5f") (/home/tony/ti/ti-processor-sdk-rtos-j721e-evm-09_02_00_05/pdk_jacinto_09_02_00_30/packages/ti/drv/sciclient/tools/ccsLoadDmsc/j721e/launch.js#222)
js:> 

我的问题:只有我有这个问题? 您这边可以吗?

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    尊敬的 Tony:

    您使用的是 TI EVM 还是定制电路板?

    请确保根据此文档将引导模式设置为"不引导"

    此外、launch.js 文件中的"pdkPath"变量可能不是绝对路径。 确保将其设置为/home/tony/ti/ti-processor... 而不是/ti/ti-processor...

    谢谢。

    内哈尔

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    这可能是你在 launch.js 文件中的"pdkPath"变量不是绝对路径。 确保将其设置为/home/tony/ti/ti-processor... 而不是/ti/ti-processor...

    谢谢。

    [/报价]

    我的问题得到了解决。