This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TDA4VE-Q1:初始化完成后、MCU2_1内核中止

Guru**** 2539500 points


请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1378988/tda4ve-q1-mcu2_1-core-has-aborted-after-init-done

器件型号:TDA4VE-Q1

工具与软件:

尊敬的专家:

在 TDA4VE 平台上、SDK 版本为9.2、  MCU2_1内核在初始化完成后中止。 有关 MCU2_1的日志如下:

[220428-17:42:29.257][MCU2_1] 2.702436 s:CIO:init……Done!!
[220428-17:42:29.257][MCU2_1] 2.702491 s:### CPU 频率= 1000000000Hz
[220428-17:42:29.257][MCU2_1] 2.702515 s:CPU 正在运行 FreeRTOS
[220428-17:42:29.257][MCU2_1] 2.702530 s:app:init…!!
[220428-17:42:29.257][MCU2_1] 2.702559 s:SCICLIENT:init……!!
[220428-17:42:29.257][MCU2_1] 2.702670 s:SCICLIENT:DMSC 固件版本[9.2.4--v09.02.04 (Kool Koala)]
[220428-17:42:29.257][MCU2_1] 2.702699 s:SCICLIENT:DMSC 固件版本0x9
[220428-17:42:29.257][MCU2_1] 2.702718 s:SCICLIENT:DMSC FW ABI 修订版3.1
[220428-17:42:29.257][MCU2_1] 2.702738 s:SCICLIENT:init……done!
[220428-17:42:29.257][MCU2_1] 2.702756 s:uDMA:init……!!
[220428-17:42:29.257][MCU2_1] 2.703605 s:uDMA:init……Done!!
[220428-17:42:29.257][MCU2_1] 2.703634 s:MEM:init……!!
[220428-17:42:29.257][MCU2_1] 2.703656 s:MEM:已创建堆(DDR_LOCAL_MEM、id=0、flags=0x00000004)@ ba000000的大小16777216字节!!
[220428-17:42:29.257][MCU2_1] 2.703699 s:MEM:init……done!
[220428-17:42:29.257][MCU2_1] 2.703715 s:IPC:init…!!
[220428-17:42:29.257][MCU2_1] 2.703748 s:IPC:5个 CPU 参与 IPC!!
[220428-17:42:29.257][MCU2_1] 2.703773 s:IPC:等待 HLOS 准备就绪...!!
[220428-17:42:30.633][MCU2_1] 11.355179 s:IPC:HLOS 已准备就绪!!
[220428-17:42:30.633][MCU2_1] 11.358040 s:IPC:init…done!!
[220428-17:42:30.633][MCU2_1] 11.358074 s:应用程序:与4个 CPU 同步...!!
[220428-17:42:30.633][MCU2_1] 11.358103 s:应用程序:与4个 CPU 同步...完成!!
[220428-17:42:30.633][MCU2_1] 11.358126 s:remote_service:init……!!
[220428-17:42:30.633][MCU2_1] 11.358353 s:remote_service:init……done!
[220428-17:42:30.633][MCU2_1] 11.358389 s:FVID2:init ...!!
[220428-17:42:30.633][MCU2_1] 11.358469 s:FVID2:初始化...完成!!
[220428-17:42:30.633][MCU2_1] 11.358538 s:VHWA:DMPAC:init ...!!
[220428-17:42:30.633][MCU2_1] 11.358593s:SCICLIENT:Sciclient_pmSetModuleState 模块=58 state=2
[220428-17:42:30.633][MCU2_1] 11.358735s:SCICLIENT:Sciclient_pmSetModuleState 成功
[220428-17:42:30.633][MCU2_1] 11.358761 s:SCICLIENT:Sciclient_pmSetModuleState 模块=62 state=2
[220428-17:42:30.633][MCU2_1] 11.358827s:SCICLIENT:Sciclient_pmSetModuleState 成功
[220428-17:42:30.633][MCU2_1] 11.358849 s:VHWA:DOF Init ...!!
[220428-17:42:30.633][MCU2_1] 11.362584 s:VHWA:DOF Init……完成!!
[220428-17:42:30.633][MCU2_1] 11.362621 s:VHWA:SDE Init ...!!
[220428-17:42:30.633][MCU2_1] 11.363780 s:VHWA:SDE 初始化...完成!!
[220428-17:42:30.633][MCU2_1] 11.363809 s:VHWA:DMPAC:init……Done!
[220428-17:42:30.633][MCU2_1] 11.363840 s:vx_zone_init:Enabled
[220428-17:42:30.633][MCU2_1] 11.363858s:vx_zone_error:Enabled
[220428-17:42:30.633][MCU2_1] 11.363874 s:vx_zone_warning:Enabled
[220428-17:42:30.633][MCU2_1] 11.365038 s:vx_zone_init:[tivxPlatformCreateTargetId:116]添加了目标 MCU2-1
[220428-17:42:30.633][MCU2_1] 11.365124 s:vx_zone_init:[tivxPlatformCreateTargetId:116]添加了目标 DMPAC_SDE
[220428-17:42:30.633][MCU2_1] 11.365219 s:vx_zone_init:[tivxPlatformCreateTargetId:116]添加了目标 DMPAC_DOF
[220428-17:42:30.633][MCU2_1] 11.365255 s:vx_zone_init:[tivxInitLocal:136]初始化已完成!!
[220428-17:42:30.633][MCU2_1] 11.365279 s:app:OpenVX Target kernel init ...!!
[220428-17:42:30.633][MCU2_1] 11.365426 s:app:OpenVX Target kernel init... done!
[220428-17:42:30.633][MCU2_1] 11.365453 s:uDMA 复制:init ...!!
[220428-17:42:30.633][MCU2_1] 11.366310 s:uDMA 复制:初始化...完成!!
[220428-17:42:30.633][MCU2_1] 11.366346 s:应用程序:初始化...完成!!
[220428-17:42:30.633][MCU2_1] 11.366364 s:应用程序:运行...!!
[220428-17:42:30.633][MCU2_1] 11.366379 s:IPC:Starting echo test ..
[220428-17:42:30.633][MCU2_1] 11.366474 s:应用程序:运行...完成!!
[220428-17:42:30.633][MCU2_1] 11.366902 s:IPC:echo status:mpu1_0[x] MCU2_0[x] MCU2_1[s] C7X_1[P] C7X_2[]。]
[220428-17:42:30.633][MCU2_1] 11.366999 s:IPC:echo status:mpu1_0[x] MCU2_0[x] MCU2_1[s] C7X_1[P] C7X_2[P]
[220428-17:42:30.633][MCU2_1] 11.367048 s:[致命]:内核已中止!!
[220428-17:42:30.633][MCU2_1] DFAR =0x29a0100 DFSR =0x808
[220428-17:42:30.633][MCU2_1] 11.367078s:IFAR =0x0 IFSR =0x0
[220428-17:42:30.633][MCU2_1] 11.367095s:CPSR =0x20000197 SP =0xa5ffe0
[220428-17:42:30.633][MCU2_1] 11.367114s:lr =0x8000009f R0 =0x8000009f
[220428-17:42:30.633][MCU2_1] 11.367133 s:r1 =0x0 R2 =0xa42ef938
[220428-17:42:30.633][MCU2_1] 11.367150s:r3 =0xa42ef934 r4 =0x8
[220428-17:42:30.633][MCU2_1] 11.367166 s:r5 =0x676ebee R6 =0xa4428dd8
[220428-17:42:30.633][MCU2_1] 11.367184 s:r7 =0x29a0100 R8 =0x1c030100
[220428-17:42:30.633][MCU2_1] 11.367202 s:R9 =0x298010c R10 =0xad727e
[220428-17:42:30.633][MCU2_1] 11.367221s:R11 =0x11111111 R12 =0xa4428eb8

此致

Hawayi.