This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TDA4VM:问题:刷写 QNX 映像后、在 TDA4暂挂上、它无法启动。

Guru**** 2673895 points

Other Parts Discussed in Thread: TDA4VM

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1395624/tda4vm-issue-after-flashing-the-qnx-image-on-tda4-boad-it-fails-to-boot-up

器件型号:TDA4VM

工具与软件:

您好!  

我将使用以下软件包构建 QNX+RTOS SDK

RTOS:ti-processor-sdk-rtos-j721e-evm-09_00_01_01
QNX:ti-processor-sdk-qnx_j721e_09_00_00_03

QNX: qnx710

QNX BSP:/qnx710/bsp/ BSP_ti-j721e-tda4vm-sk_br-710_be-710_SVN981674_JBN18.zip

按照中提到的构建步骤进行操作:

在 QNX + RTOS 模式下编译成功。 但是、当我使用 SD 卡启动电路板时、我没有获得稳定的映像 u-boot 启动。

附加供参考的日志:

Issue MAPC/SYNC/INVALL commands for ICID 0
update CWRITER to 0x00000060
Waiting for all commands to be processed ... Done in 1 tries
Enable LPIs in GICR_CTLR @ 0000000001900000 for CPU0
Total Available L3 cache (MSMC SRAM): 0 bytes
Loading IFS...
U-Boot SPL 2023.04-g756ba776d4 (Jul 13 2023 - 05:36:12 +0000)
SYSFW ABI: 3.1 (firmware rev 0x0009 '9.0.6--v09.00.06 (Kool Koala)')
Trying to boot from MMC2
Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted
Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted
Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted
Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted
Warning: Detected image signing certificate on GP device. Skipping certificate to prev+-----------------------------+l if the image was also encrypted
Loading Environment from nowhere... OK                                                |                             |
Starting ATF on ARM64 core...                                                         |  Cannot open /dev/ttyUSB2!  |
                                                                                      |                             |
NOTICE:  BL31: v2.8(release):v2.8-226-g2fcd408bb3-dirty                               +-----------------------------+
NOTICE:  BL31: Built : 00:42:57, Jan 13 2023
I/TC: 
I/TC: OP-TEE version: 3.20.0 (gcc version 11.3.0 (GCC)) #1 Fri Jan 20 15:42:54 UTC 2023 aarch64
I/TC: WARNING: This OP-TEE configuration might be insecure!
I/TC: WARNING: Please check optee.readthedocs.io/.../porting_guidelines.html
I/TC: Primary CPU initializing
I/TC: SYSFW ABI: 3.1 (firmware rev 0x0009 '9.0.6--v09.00.06 (Kool Koala)')
I/TC: HUK Initialized
I/TC: Activated SA2UL device
I/TC: Fixing SA2UL firewall owner for GP device
I/TC: Enabled firewalls for SA2UL TRNG device
I/TC: SA2UL TRNG initialized
I/TC: SA2UL Drivers initialized
I/TC: Primary CPU switching to normal world boot


请告诉我如何调试此问题。
注意:我有 QNX 许可证7.1、并已安装依赖项部分中提到的所有软件包。