工具与软件:
您好!
我尝试 使用在 J721S2 EVM 上运行视觉应用
- QNX SDP 8.0版
- QNX 10.0.0.4 SDK。
- RTOS 10.0.0.5 SDK。
我在 板载闪存 QNX - 10.0 SDK 时得到以下日志。 启动 sshd 失败 错误的 addr 或主机: (名称未解析)
U-Boot SPL 2024.04-ti-g818c76aed67f (Aug 01 2024 - 19:19:47 +0000) SYSFW ABI: 4.0 (firmware rev 0x000a '10.0.8--v10.00.08 (Fiery Fox)') SPL initial stack usage: 13456 bytes Trying to boot from MMC2 Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted Loading Environment from nowhere... OK Starting ATF on ARM64 core... NOTICE: BL31: v2.10.0(release):v2.10.0-367-g00f1ec6b87-dirty NOTICE: BL31: Built : 16:09:05, Feb 9 2024 I/TC: I/TC: OP-TEE version: 4.2.0-dev (gcc version 13.3.0 (GCC)) #1 Fri Apr 12 09:51:21 UTC 2024 aarch64 I/TC: WARNING: This OP-TEE configuration might be insecure! I/TC: WARNING: Please check optee.readthedocs.io/.../porting_guidelines.html I/TC: Primary CPU initializing I/TC: GIC redistributor base address not provided I/TC: Assuming default GIC group status and modifier I/TC: SYSFW ABI: 4.0 (firmware rev 0x000a '10.0.8--v10.00.08 (Fiery Fox)') I/TC: HUK Initialized I/TC: Activated SA2UL device I/TC: Fixing SA2UL firewall owner for GP device I/TC: Enabled firewalls for SA2UL TRNG device I/TC: SA2UL TRNG initialized I/TC: SA2UL Drivers initialized I/TC: Primary CPU switching to normal world boot U-Boot SPL 2024.04-ti-g818c76aed67f (Aug 01 2024 - 19:19:47 +0000) SYSFW ABI: 4.0 (firmware rev 0x000a '10.0.8--v10.00.08 (Fiery Fox)') Trying to boot from MMC2 Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted U-Boot 2024.04-ti-g818c76aed67f (Aug 01 2024 - 19:19:47 +0000) SoC: J721S2 SR1.0 GP Model: Texas Instruments J721S2 EVM Board: J721S2X-PM1-SOM rev E4 DRAM: 2 GiB (effective 16 GiB) Core: 117 devices, 32 uclasses, devicetree: separate Flash: 0 Bytes MMC: mmc@4f80000: 0, mmc@4fb0000: 1 Loading Environment from nowhere... OK In: serial@2880000 Out: serial@2880000 Err: serial@2880000 am65_cpsw_nuss ethernet@46000000: K3 CPSW: nuss_ver: 0x6BA02102 cpsw_ver: 0x6BA82102 ale_ver: 0x00293904 Ports:1 Net: eth0: ethernet@46000000port@1 Hit any key to stop autoboot: 0 switch to partitions #0, OK mmc1 is current device SD/MMC found on device 1 1258 bytes read in 26 ms (46.9 KiB/s) Loaded env from uEnv.txt Importing environment from mmc1 ... Running uenvcmd ... k3_r5f_rproc r5f@41000000: Core 1 is already in use. No rproc commands work k3_r5f_rproc r5f@41400000: Core 2 is already in use. No rproc commands work 867724 bytes read in 36 ms (23 MiB/s) Load Remote Processor 2 with data@addr=0x82000000 867724 bytes: Success! 322708 bytes read in 31 ms (9.9 MiB/s) Load Remote Processor 3 with data@addr=0x82000000 322708 bytes: Success! Failed to load '/lib/firmware/j721s2-main-r5f1_0-fw' Failed to load '/lib/firmware/j721s2-main-r5f1_1-fw' 15044640 bytes read in 106 ms (135.4 MiB/s) Load Remote Processor 6 with data@addr=0x82000000 15044640 bytes: Success! 9482088 bytes read in 46 ms (196.6 MiB/s) Load Remote Processor 7 with data@addr=0x82000000 9482088 bytes: Success! 12692472 bytes read in 171 ms (70.8 MiB/s) 95815 bytes read in 27 ms (3.4 MiB/s) ## Starting application at 0x80080000 ... Hypervisor support disabled MMU: 16-bit ASID 44-bit PA TCR_EL1=00000014b5183519 ARM GIC-500 r1p1, arch v3.0 detected gic_v3_lpi_add_entry for vectors 8192 -> 8447, Ok gic_v3_lpi_add_entry for vectors 8448 -> 65535, Ok No SPI intrinfo. Add default entry for 32 -> 991 vectors, Ok LPI config table #1 @ 0000000080013000, callout vaddr: ffffff8040251000 aarch64_cpuspeed: core speed 2000 cpu0: MPIDR=0000000080000000 cpu0: MIDR=411fd080 Cortex-A72 r1p0 cpu0: CWG=4 ERG=4 Dminline=4 Iminline=4 PIPT cpu0: CLIDR=a200023 LoUU=1 LoC=2 LoUIS=1 cpu0: L1 Icache 48K linesz=64 set/way=256/3 cpu0: L1 Dcache 32K linesz=64 set/way=256/2 cpu0: L2 Unified 1024K linesz=64 set/way=1024/16 Enabling ITS 0 ITS queue at 0000000080030000, num slots: 256 Issue MAPC/SYNC/INVALL commands for ICID 0 update CWRITER to 0x00000060 Waiting for all commands to be processed ... Done in 1 tries Enable LPIs in GICR_CTLR @ 0000000001900000 for CPU0 Display set to A72 Total Available L3 cache (MSMC SRAM): 4194304 bytes Loading IFS...decompressing...done I/TC: Secondary CPU 1 initializing I/TC: Secondary CPU 1 switching to normal world boot aarch64_cpuspeed: core speed 2000 cpu1: MPIDR=0000000080000001 cpu1: MIDR=411fd080 Cortex-A72 r1p0 cpu1: CWG=4 ERG=4 Dminline=4 Iminline=4 PIPT cpu1: CLIDR=a200023 LoUU=1 LoC=2 LoUIS=1 cpu1: L1 Icache 48K linesz=64 set/way=256/3 cpu1: L1 Dcache 32K linesz=64 set/way=256/2 cpu1: L2 Unified 1024K linesz=64 set/way=1024/16 ITS 0 already Enabled ITS queue at 0000000080030000, num slots: 256 Issue MAPC/SYNC/INVALL commands for ICID 1 update CWRITER to 0x000000c0 Waiting for all commands to be processed ... Done in 1 tries Enable LPIs in GICR_CTLR @ 0000000001920000 for CPU1 System page at phys:0000000080022000 user:ffffff8040275000 kern:ffffff8040272000 Starting next program at vffffff8060087740 syspage::hypinfo::flags=0x00000000 Welcome to QNX 8.0.0 on TI_J721S2_EVM_Board ! Starting I2C driver ... start serial driver Starting MMC/SD memory card driver... eMMC Starting MMC/SD memory card driver... SD Starting Flash driver... ldd:FATAL: Could not load library libti-pdk.so.1 Starting XHCI driver Path=0 - am65x target=0 lun=0 Direct-Access(0) - SDMMC: G1M15L Rev: 1.0 Starting devf-ram filesystem ... Setting environment variables... Mounting the sd .. Looking for user script to run: /ti_fs/scripts/user.sh Running user script... user.sh called... Setting additional environment variables... Starting tisci-mgr.. Initializing sciclient in polling mode Starting shmemallocator.. Starting tiipc-mgr.. Starting tiudma-mgr.. Starting ti-vpu-codec-mgr Starting VPU Codec resource manager... Resource Manager loop starting Starting sshd bad addr or host: <NULL> (Name does not resolve) done... J721S2-EVM@QNX:/# uname -a QNX localhost 8.0.0 2024/06/13-12:41:10EDT TI_J721S2_EVM_Board aarch64le J721S2-EVM@QNX:/# ifconfig ifconfig: getifaddrs: Address family not supported by protocol family J721S2-EVM@QNX:/# J721S2-EVM@QNX:/# J721S2-EVM@QNX:/#
请帮助解决此问题。
注意:Linux SDK 10.0中不存在 sshd 问题。 我们仅在 QNX 10.0中观察到它。
谢谢