Other Parts Discussed in Thread: SK-AM62, SK-AM62-LP, SK-AM62B-P1
主题中讨论的其他器件: SK-AM62-LP、 SK-AM62B-P1、SK-AM62
您好!
这是几个月前发布的之前主题帖和讨论的后续内容:
软件/硬件配置:
- TI SDK 09.02.01.09
-定制硬件(各种配置的存储器大小和存储器供应商,不同的 SOC 变体: AM6254、AM6231、AM6252)
-内核来源: https://git.toradex.com/cgit/linux-toradex.git/log/?h=toradex_ti-linux-6.1.y
- U-Boot 源代码: https://git.toradex.com/cgit/u-boot-toradex.git/log/?h=toradex_ti-u-boot-2023.04
- DDR 由我们内部验证, 并由存储器供应商在其办公场所进行验证。 我们有不同尺寸和供应商的存储器型号、它们都受到相同问题的影响
-我们有0.75V 和0.85V VDD_CORE 的变体,没有因为这种行为的差异
在对我们的软件/硬件进行测试期间、我们面临一些不同方式的启动停止问题。 它们都在 -20摄氏度以下发生。
1.系统因以下错误而停止。
[ 86.779029] rcu: INFO: rcu_preempt detected stalls on CPUs/tasks: [ 86.785173] rcu: Tasks blocked on level-0 rcu_node (CPUs 0-0): P186/1:b..l [ 86.792151] (detected by 0, t=18276 jiffies, g=6889, q=115 ncpus=1) [ 86.798506] task:systemd-udevd state:R running task stack:0 pid:186 ppid:173 flags:0x00000a04 [ 86.808424] Call trace: [ 86.810870] __switch_to+0xd4/0x130 [ 86.814374] __schedule+0x230/0x664 [ 86.817863] preempt_schedule_irq+0x44/0xd0 [ 86.822047] el1_interrupt+0x4c/0x70 [ 86.825626] el1h_64_irq_handler+0x18/0x2c [ 86.829725] el1h_64_irq+0x64/0x68 [ 86.833130] set_root+0x64/0xfc [ 86.836275] nd_jump_root+0xb8/0xf0 [ 86.839764] path_init+0x2d0/0x380 [ 86.843167] path_parentat+0x20/0xb0 [ 86.846743] __filename_parentat+0xa4/0x1c0 [ 86.850927] do_unlinkat+0x68/0x270 [ 86.854416] __arm64_sys_unlinkat+0x40/0x84 [ 86.858600] invoke_syscall+0x48/0x114 [ 86.862352] el0_svc_common.constprop.0+0xd4/0xfc [ 86.867057] do_el0_svc+0x20/0x30 [ 86.870372] el0_svc+0x28/0xa0 [ 86.873428] el0t_64_sync_handler+0xbc/0x140 [ 86.877701] el0t_64_sync+0x18c/0x190 [ 86.881364] rcu: rcu_preempt kthread timer wakeup didn't happen for 18273 jiffies! g6889 f0x0 RCU_GP_WAIT_FQS(5) ->state=0x402 [ 86.892749] rcu: Possible timer handling issue on cpu=0 timer-softirq=2071 [ 86.899705] rcu: rcu_preempt kthread starved for 18274 jiffies! g6889 f0x0 RCU_GP_WAIT_FQS(5) ->state=0x402 ->cpu=0 [ 86.910136] rcu: Unless rcu_preempt kthread gets sufficient CPU time, OOM is now expected behavior. [ 86.919260] rcu: RCU grace-period kthread stack dump: [ 86.924305] task:rcu_preempt state:I stack:0 pid:14 ppid:2 flags:0x00000008 [ 86.932656] Call trace: [ 86.935099] __switch_to+0xd4/0x130 [ 86.938587] __schedule+0x230/0x664 [ 86.942074] schedule+0x5c/0xcc [ 86.945216] schedule_timeout+0x84/0xfc [ 86.949055] rcu_gp_fqs_loop+0x12c/0x46c [ 86.952983] rcu_gp_kthread+0x128/0x164 [ 86.956820] kthread+0x10c/0x110 [ 86.960051] ret_from_fork+0x10/0x20 [ 86.963627] rcu: Stack dump where RCU GP kthread last ran: [ 86.969111] CPU: 0 PID: 181 Comm: systemd-udevd Not tainted 6.1.80+git.0d9f1748ac17 #1 [ 86.977026] Hardware name: Toradex Verdin AM62 WB on Verdin Development Board (DT) [ 86.984591] pstate: 60000005 (nZCv daif -PAN -UAO -TCO -DIT -SSBS BTYPE=--) [ 86.991550] pc : iomap_read_reg+0x10/0x30 [m_can_platform] [ 86.997049] lr : m_can_get_berr_counter+0x3c/0x10c [m_can] [ 87.002548] sp : ffff8000099735f0 [ 87.005858] x29: ffff8000099735f0 x28: 0000000000000240 x27: ffff800000cca1a0 [ 87.012998] x26: ffff000003f9e000 x25: ffff000003f9e240 x24: 0000000000000000 [ 87.020137] x23: 0000000000000000 x22: ffff0000002ae410 x21: ffff0000035f8000 [ 87.027276] x20: ffff0000035f8980 x19: ffff80000997362c x18: 0000000000000000 [ 87.034414] x17: ffff800014add000 x16: ffff800008000000 x15: 0000000000000000 [ 87.041552] x14: 000000000000022f x13: 0000000000000001 x12: 0000000000000001 [ 87.048691] x11: 0000000000000000 x10: 00000000000009b0 x9 : ffff8000099731e0 [ 87.055829] x8 : ffff00001da1b180 x7 : 0000010000108100 x6 : ffff0000002ae590 [ 87.062968] x5 : 0000000000000000 x4 : 0000000000000000 x3 : 0000000000000000 [ 87.070106] x2 : ffff800000ca4000 x1 : 0000000000000040 x0 : 000000000071ff00 [ 87.077244] Call trace: [ 87.079687] iomap_read_reg+0x10/0x30 [m_can_platform] [ 87.084832] can_fill_info+0x108/0x524 [can_dev] [ 87.089477] rtnl_fill_ifinfo+0x844/0x11b0 [ 87.093578] rtnl_getlink+0x23c/0x424 [ 87.097239] rtnetlink_rcv_msg+0x130/0x3a0 [ 87.101334] netlink_rcv_skb+0x60/0x130 [ 87.105174] rtnetlink_rcv+0x18/0x2c [ 87.108755] netlink_unicast+0x2f0/0x360 [ 87.112677] netlink_sendmsg+0x1b0/0x420 [ 87.116600] __sys_sendto+0x138/0x174 [ 87.120265] __arm64_sys_sendto+0x28/0x3c [ 87.124275] invoke_syscall+0x48/0x114 [ 87.128024] el0_svc_common.constprop.0+0xd4/0xfc [ 87.132729] do_el0_svc+0x20/0x30 [ 87.136044] el0_svc+0x28/0xa0 [ 87.139100] el0t_64_sync_handler+0xbc/0x140 [ 87.143372] el0t_64_sync+0x18c/0x190
完整日志:
e2e.ti.com/.../24_2D00_04_2D00_17_5F00_22_2D00_12_2D00_36_2D00_Fail.txt
2.没有任何消息的引导停止。
不过、根据我可以告诉您的、没有有关正在发生什么的提示、请参阅所附的日志
e2e.ti.com/.../24_2D00_04_2D00_17_5F00_18_2D00_29_2D00_29_2D00_Fail.txt