工具与软件:
您好!
Yocto SDK: 09_01_00
EVM:AM62A SK EVM
我们已基于 AM62A SK EVM 设计了定制 ME 电路板。 我们唯一做的更改是将 DDR 从4GB 更改为1GB。 DDR 更改后、我们遇到了 CMA 内存池分配问题。 我在下面添加了错误的内核日志。
Starting kernel ... [ 0.000000] Booting Linux on physical CPU 0x0000000000 [0x410fd034] [ 0.000000] Linux version 6.1.46-rt13-gb871cdee8c (oe-user@oe-host) (aarch64-oe-linux-gcc (GCC) 11.4.0, GNU ld (GNU Binutils) 2.38.20220708) #1 SMP PREEMPT_RT Thu Dec 7 23:52:13 UTC 2023 [ 0.000000] Machine model: Texas Instruments AM62A7 SK [ 0.000000] earlycon: ns16550a0 at MMIO32 0x0000000002800000 (options '') [ 0.000000] printk: bootconsole [ns16550a0] enabled [ 0.000000] efi: UEFI not found. [ 0.000000] OF: reserved mem: failed to allocate memory for node 'linux,cma': size 576 MiB [ 0.000000] Reserved memory: created DMA memory pool at 0x0000000099800000, size 1 MiB [ 0.000000] OF: reserved mem: initialized node c7x-dma-memory@99800000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x0000000099900000, size 30 MiB [ 0.000000] OF: reserved mem: initialized node c7x-memory@99900000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x000000009b800000, size 1 MiB [ 0.000000] OF: reserved mem: initialized node r5f-dma-memory@9b800000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x000000009b900000, size 15 MiB [ 0.000000] OF: reserved mem: initialized node r5f-dma-memory@9b900000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x000000009c800000, size 1 MiB [ 0.000000] OF: reserved mem: initialized node r5f-dma-memory@9c800000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x000000009c900000, size 30 MiB [ 0.000000] OF: reserved mem: initialized node r5f-dma-memory@9c900000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a1000000, size 32 MiB [ 0.000000] OF: reserved mem: initialized node edgeai-dma-memory@a1000000, compatible id shared-dma-pool [ 0.000000] OF: reserved mem: initialized node edgeai_shared-memories, compatible id dma-heap-carveout [ 0.000000] Zone ranges: [ 0.000000] DMA [mem 0x0000000080000000-0x00000000bfffffff] [ 0.000000] DMA32 empty [ 0.000000] Normal empty [ 0.000000] Movable zone start for each node [ 0.000000] Early memory node ranges [ 0.000000] node 0: [mem 0x0000000080000000-0x00000000997fffff] [ 0.000000] node 0: [mem 0x0000000099800000-0x000000009b7fefff] [ 0.000000] node 0: [mem 0x000000009b800000-0x000000009e6fffff] [ 0.000000] node 0: [mem 0x000000009e700000-0x000000009e77ffff] [ 0.000000] node 0: [mem 0x000000009e780000-0x00000000a2ffffff] [ 0.000000] node 0: [mem 0x00000000a3000000-0x00000000bfffffff] [ 0.000000] Initmem setup node 0 [mem 0x0000000080000000-0x00000000bfffffff] [ 0.000000] On node 0, zone DMA: 1 pages in unavailable ranges [ 0.000000] cma: Reserved 32 MiB at 0x00000000bce00000
日志 AS 中出现错误 "of: reserved mem: failed to allocation memory for node 'Linux,CMA': size 576 MiB"(共:保留内存:无法为节点"Linux,CMA"分配内存:大小576 MiB")。 这可能是由于 DDR 的大小为1GB 所致。
由于这种分配错误、当我们从摄像机传感器开始流式传输视频时、内核会崩溃。 我们使用的是1920x1200分辨率- 10位模式。 从摄像头传感器流式传输或捕获图像时、我们收到以下 CAM 分配错误。
k location=frame%d.rawheight=1200, framerate=120/1, format=rggb10 ! multifilesink Setting pipeline to PAUSED ... Pipeline is live and does not need PREROLL ... Pipeline is PREROLLED ... Setting pipeline to PLAYING ... New clock: GstSystemClock /GstPipeline:pipeline0/GstV4l2Src:v4l2src0.GstPad:src: caps = video/x-bayer, width=(int)1920, height=(int)1200, framerate=(fraction)120/1, format=(string)rggb10, interlace-mode=(string)progressive, colorimetry=(string)2:4:7:1 /GstPipeline:pipeline0/GstCapsFilter:capsfilter0.GstPad:src: caps = video/x-bayer, width=(int)1920, height=(int)1200, framerate=(fraction)120/1, format=(string)rggb10, interlace-mode=(string)progressive, colorimetry=(string)2:4:7:1 /GstPipeline:pipeline0/GstMultiFileSink:multifilesink0.GstPad:sink: caps = video/x-bayer, width=(int)1920, height=(int)1200, framerate=(fraction)120/1, format=(string)rggb10, interlace-mode=(string)progressive, colorimetry=(string)2:4:7:1 /GstPipeline:pipeline0/GstCapsFilter:capsfilter0.GstPad:sink: caps = video/x-bayer, width=(int)1920, height=(int)1200, framerate=(fraction)120/1, format=(string)rggb10, interlace-mode=(string)progressive, colorimetry=(string)2:4:7:1 [ 28.111966] ar0235 2-0036: exposure value = 1499 Redistribute latency... [ 28.333950] cma: cma_alloc: reserved: alloc failed, req-size: 1125 pages, ret: -12 [ 28.333987] ------------[ cut here ]------------ [ 28.333990] WARNING: CPU: 3 PID: 678 at mm/page_alloc.c:5535 0xffff80000813e470 [ 28.333999] Modules linked in: overlay cfg80211 rfkill xhci_plat_hcd dwc3 rpmsg_ctrl rpmsg_char cdns_csi2rx spidev crct10dif_ce phy_can_transceiver e5010_jpeg_enc dwc3_am62 k3_j72xx_bandgap rtc_ti_k3 ti_k3_r5_remoteproc ti_k3_dsp_remoteproc tidss virtio_rpmsg_bus rpmsg_ns drm_dma_helper ti_k3_common wave5 j721e_csi2rx drm_kms_helper sa2ul v4l2_mem2mem syscopyarea sysfillrect sysimgblt fb_sys_fops videobuf2_dma_contig videobuf2_memops videobuf2_v4l2 videobuf2_common cdns_dphy_rx tps6598x ar0235 typec v4l2_fwnode m_can_platform v4l2_async m_can videodev pwm_tiehrpwm mc can_dev spi_omap2_mcspi optee_rng rng_core cryptodev(O) fuse drm drm_panel_orientation_quirks ipv6 [ 28.334149] CPU: 3 PID: 678 Comm: v4l2src0:src Tainted: G O 6.1.46-rt13-gb871cdee8c #1 [ 28.334158] Hardware name: Texas Instruments AM62A7 SK (DT) [ 28.334162] pstate: 20000005 (nzCv daif -PAN -UAO -TCO -DIT -SSBS BTYPE=--) [ 28.334171] pc : 0xffff80000813e470 [ 28.334174] lr : 0xffff8000080a2bb0 [ 28.334176] sp : ffff00000893b860 [ 28.334179] x29: ffff00000893b860 x28: ffff000005691860 x27: 0000000000000001 [ 28.334189] x26: 000000000000000b x25: ffff000004d812d0 x24: ffff8000080a1a18 [ 28.334200] x23: ffff0000001bac10 x22: ffff0000054f9920 x21: ffff0000001bac10 [ 28.334210] x20: 0000000000000cc0 x19: 0000000000000000 x18: ffffffffffffffff [ 28.334220] x17: 6572202c73656761 x16: 702035323131203a x15: 657a69732d716572 [ 28.334230] x14: 202c64656c696166 x13: 32312d203a746572 x12: 202c736567617020 [ 28.334240] x11: 35323131203a657a x10: 69732d716572202c x9 : ffff800008e5d050 [ 28.334251] x8 : 0000000000000000 x7 : ffff800008eb7718 x6 : 0000000000000000 [ 28.334261] x5 : 0000000000000001 x4 : 0000000000000035 x3 : 0000000000000000 [ 28.334270] x2 : 0000000000000000 x1 : 0000000000000001 x0 : ffff800008f59000 [ 28.334280] Call trace: [ 28.334283] 0xffff80000813e470 [ 28.334287] 0xffff8000080a2bb0 [ 28.334289] 0xffff8000080a2d64 [ 28.334292] 0xffff8000080a1a18 [ 28.334295] 0xffff800000bbf94c [ 28.334297] 0xffff800000ba65f4 [ 28.334300] 0xffff800000ba6c80 [ 28.334303] 0xffff800000bb13bc [ 28.334305] 0xffff800000bb1810 [ 28.334308] 0xffff800000b40564 [ 28.334311] 0xffff800000b40880 [ 28.334314] 0xffff800000b41774 [ 28.334316] 0xffff800000b41ba4 [ 28.334319] 0xffff800000b3a16c [ 28.334321] 0xffff800008182b60 [ 28.334324] 0xffff80000801de8c [ 28.334327] 0xffff80000801df80 [ 28.334329] 0xffff800008a1ccf0 [ 28.334332] 0xffff800008a1e1a4 [ 28.334335] 0xffff800008011488 [ 28.334338] ---[ end trace 0000000000000000 ]--- [ 28.334348] ti-udma 4e230000.dma-controller: dma alloc of size 4608000 failed
我们正在对视频流进行 JPEG 编码和 ISP 处理。 我们如何避免 CMA 内存分配错误、使其不会影响我们的流媒体功能?
此致、
Jay