This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] AM625:u-boot SDK 10.00.07.04与 Linux SDK 09.01.00.08兼容

Guru**** 2540720 points


请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1433311/am625-u-boot-sdk-10-00-07-04-compatible-with-linux-sdk-09-01-00-08

器件型号:AM625

工具与软件:

您好!

我将从 SDK 10.00.07.04运行 tiboot3、tisbl 和 u-boot、并从 SDK 09.01.00.08运行 Linux、但时钟存在一些问题。

从 Linux 打印出来。

[0.160786]   ti-sci 440430.system-controller:abi:4.0 (固件版本0x000a '10.0.8--v10.00.08 (Fiery Fox)')
[   0.171131] ti-sci-clk 440430.system-controller:clock-controller:recalc-rate failed for dev=13、clk=7、ret=-19
[   0.172894] ti-sci-clk 440430.system-controller:clock-controller:recalc-rate failed for dev=36、clk=9、ret=-19
[   0.173516] ti-sci-clk 440430.system-controller:clock-controller:recalc-rate failed for dev=36、clk=15、ret=-19
[   0.173616] ti-sci-clk 440430.system-controller:clock-controller:recalc-rate failed for dev=36、clk=16、ret=-19
[   0.173736] ti-sci-clk 440430.system-controller:clock-controller:recalc-rate failed for dev=36、clk=17、ret=-19
[   0.173836] ti-sci-clk 440430.system-controller:clock-controller:recalc-rate failed for dev=36、clk=18、ret=-19
[   0.174891] ti-sci-clk 440430.system-controller:clock-controller:recalc-rate failed for dev=37、clk=9、ret=-19
[   0.175509] ti-sci-clk 440430.system-controller:clock-controller:recalc-rate failed for dev=37、clk=15、ret=-19
[   0.175604] ti-sci-clk 440430.system-controller:clock-controller:recalc-rate failed for dev=37、clk=16、ret=-19
[   0.175727] ti-sci-clk 440430.system-controller:clock-controller:recalc-rate failed for dev=37、clk=17、ret=-19
[   0.175825] ti-sci-clk 440430.system-controller:clock-controller:recalc-rate failed for dev=37、clk=18、ret=-19
[   0.177836] ti-sci-clk 440430.system-controller:clock-controller:recalc-rate failed for dev=38、clk=9、ret=-19
[   0.178485] ti-sci-clk 440430.system-controller:clock-controller:recalc-rate failed for dev=38、clk=15、ret=-19
[   0.178584] ti-sci-clk 440430.system-controller:clock-controller:recalc-rate failed for dev=38、clk=16、ret=-19
[   0.178710] ti-sci-clk 440430.system-controller:clock-controller:recalc-rate failed for dev=38、clk=17、ret=-19
[   0.178807] ti-sci-clk 440430.system-controller:clock-controller:recalc-rate failed for dev=38、clk=18、ret=-19
[   0.179876] ti-sci-clk 440430.system-controller:clock-controller:recalc-rate failed for dev=39、clk=9、ret=-19
[   0.180541] ti-sci-clk 440430.system-controller:clock-controller:recalc-rate 失败(dev=39、clk=15、ret=-19)
[   0.180644] ti-sci-clk 440430.system-controller:clock-controller:recalc-rate failed for dev=39、clk=16、ret=-19
[   0.180774] ti-sci-clk 440430.system-controller:clock-controller:recalc-rate failed for dev=39、clk=17、ret=-19
[   0.180872] ti-sci-clk 440430.system-controller:clock-controller:recalc-rate failed for dev=39、clk=18、ret=-19
[   0.181928] ti-sci-clk 440430.system-controller:clock-controller:recalc-rate failed for dev=40、clk=9、ret=-19
[   0.182564] ti-sci-clk 440430.system-controller:clock-controller:recalc-rate failed for dev=40、clk=15、ret=-19
[   0.182676] ti-sci-clk 440430.system-controller:clock-controller:recalc-rate failed for dev=40、clk=16、ret=-19
[   0.182775] ti-sci-clk 440430.system-controller:clock-controller:recalc-rate failed for dev=40、clk=17、ret=-19
[   0.182901] ti-sci-clk 440430.system-controller:clock-controller:recalc-rate failed for dev=40、clk=18、ret=-19
[   0.183987] ti-sci-clk 440430.system-controller:clock-controller:recalc-rate failed for dev=41、clk=9、ret=-19
[   0.184662] ti-sci-clk 440430.system-controller:clock-controller:recalc-rate failed for dev=41、clk=15、ret=-19
[   0.184794] ti-sci-clk 440430.system-controller:clock-controller:recalc-rate 失败(dev=41、clk=16、ret=-19)
[   0.184895] ti-sci-clk 440430.system-controller:clock-controller:recalc-rate failed for dev=41、clk=17、ret=-19
[   0.185046] ti-sci-clk 440430.system-controller:clock-controller:recalc-rate failed for dev=41、clk=18、ret=-19
[   0.186130] ti-sci-clk 440430.system-controller:clock-controller:recalc-rate failed for dev=42、clk=9、ret=-19
[   0.186760] ti-sci-clk 440430.system-controller:clock-controller:recalc-rate failed for dev=42、clk=15、ret=-19
[   0.186888] ti-sci-clk 440430.system-controller:clock-controller:recalc-rate failed for dev=42、clk=16、ret=-19
[   0.186991] ti-sci-clk 440430.system-controller:clock-controller:recalc-rate failed for dev=42、clk=17、ret=-19
[   0.187120] ti-sci-clk 440430.system-controller:clock-controller:recalc-rate failed for dev=42、clk=18、ret=-19
[   0.188226] ti-sci-clk 440430.system-controller:clock-controller:recalc-rate failed for dev=43、clk=9、ret=-19
[   0.188921] ti-sci-clk 440430.system-controller:clock-controller:recalc-rate failed for dev=43、clk=15、ret=-19
[   0.189050] ti-sci-clk 440430.system-controller:clock-controller:recalc-rate failed for dev=43、clk=16、ret=-19
[   0.189156] ti-sci-clk 440430.system-controller:clock-controller:recalc-rate failed for dev=43、clk=17、ret=-19
[   0.189283] ti-sci-clk 440430.system-controller:clock-controller:recalc-rate failed for dev=43、clk=18、ret=-19
[   0.192501] ti-sci-clk 440430.system-controller:clock-controller:recalc-rate failed for dev=81、clk=7、ret=-19
[   0.193072] ti-sci-clk 440430.system-controller:clock-controller:recalc-rate failed for dev=81、clk=20、ret=-19
[   0.213365] LM75 0-0048:使用虚拟稳压器时、电源与未找到之间的关系
[   0.236826] hwmon hwmon0:TEMP1_INPUT 未连接到任何热区

SDK 10.00.07.04中的 SBL 和 U-boot 是否与 SDK 09.01.00.08中的 Linux 兼容?

此致

Magnus

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好!

    10.0 SDK 中有一些 ti-sci 更新。 此外、建议使用相同版本的 U-boot 和 Linux。

    此致、
    Aparna

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    我知道建议使用相同版本的 U-boot 和 Linux。

    但我的问题是。

    SDK 10.00.07.04中的 SBL 和 U-boot 是否与 SDK 09.01.00.08中的 Linux 兼容?

    是或否。。。

     

    我之所以提出这个问题、是因为我们的软件下载流程会首先更新 SBL 和 U-Boots。 重新启动、然后更新系统的其余部分。 在下面的场景中、我们会 从 SDK 10.00.07.04和 Linux (SDK 09.01.00.08)运行 U-boot。

     

    /马格努斯

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好!

    我们不测试交叉版本兼容性。 因此、我不能以"是"或"否"回答 它可能总是起作用、也可能不总是起作用。

    此致、
    Aparna