请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:TDA4VM 工具与软件:
您好!
现在我需要在 TDA4上运行两个 PIPELLINE 进程。 如果这两个进程分别运行、它们可以正常运行、
但是、如果它们同时运行、则第二个 PIPELLINE 进程将报告错误。 错误日志如下所示:
(), line<626>: App Create Graph Done! 0.000000 s: VX_ZONE_ERROR:[ownContextSendCmd:875] Command ack message returned failure cmd_status: -1 0.000000 s: VX_ZONE_ERROR:[ownNodeKernelInit:590] Target kernel, TIVX_CMD_NODE_CREATE failed for node capture_node 0.000000 s: VX_ZONE_ERROR:[ownNodeKernelInit:591] Please be sure the target callbacks have been registered for this core 0.000000 s: VX_ZONE_ERROR:[ownNodeKernelInit:592] If the target callbacks have been registered, please ensure no errors are occurring within the create callback of this kernel 0.000000 s: VX_ZONE_ERROR:[ownGraphNodeKernelInit:608] kernel init for node 0, kernel com.ti.capture ... failed !!! 0.000000 s: VX_ZONE_ERROR:[vxVerifyGraph:2159] Node kernel init failed 0.000000 s: VX_ZONE_ERROR:[vxVerifyGraph:2213] Graph verify failed /home/hzhang37/second1TB/jwan4/tda4-w39-1-project/application_tda4_2box/a72/rear_cam_app/source/rear_cam_main.c, in function: app_rear_cam_main(), line<648>: App Run Graph Done! Capture delete done! VISS delete done! AEWB delete done!
请问原因是甚么? 可以在 TDA4上同时运行两个 PIPELLINE 进程。