主题中讨论的其他器件:TMUX1574
工具与软件:
你(们)好 尊敬的专家:
由于设计注意事项、客户可能会移除"VDD_MMC1_SD" SD 负载开关。
EVM 参考如下。
D-Note,
This power switch, along with the reset logic, and the host IO power supply circuit is required to support UHS-I SD Cards which begins communications using 3.3V signal levels and later change to 1.8V signal levels when changing to one of the faster data transfer speeds. Cycling power to the SD Card is the only way to put it back into 3.3V mode since SD Cards do not have a reset pin. The host IO power supply must power off/on and change voltage at the same time as the SD Card.
下面是一些问题:
(1) VDDSHV_SDIO 由 来自 PMIC 的 VOUT_LDO1控制。 PMIC 如何知道如何将 VDDSHV_SDIO 从3.3V 更改为1.8V、从 SD 默认速度更改为 UHS?
(2)当 AM62A 执行软件重新启动(Linux 重新启动)时、RESETSTATz 是否再次"低电平有效"?
(3)当我们移除 "负载开关(TPS22918DBVR)"并让 VDD_MMC1_SD 始终保持3.3V。 这意味着 SD 没有机会重置 并返回默认速度。
我认为 PMIC 的 VDDSHV_SDIO VOUT_LDO1应返回到3.3V、但 SD I/O 电平应保持为1.8V (mmc1_d0~D3)。 它是否有任何损坏?
非常感谢
Gibbs