工具与软件:
您好、一直在尝试在 AM6442上启动以太网。 我们在 PRU_ICSSG1上使用 RGMII 端口。 在初始化期间、出现以下错误:
[ 11.753582] icssg-prueth icssg1-eth: port 2: using random MAC addr: ae:b4:6b:b9:81:11 [ 11.753635] icssg-prueth icssg1-eth: registering netdevs [ 11.754561] icssg-prueth icssg1-eth: couldn't connect to phy ethernet-phy@1 [ 11.754583] icssg-prueth icssg1-eth: can't connect to MII0 PHY, error --19 (deferring)
您能否验证下面连接的设备树:
icssg1_rgmii1_pins_default: icssg1-rgmii1-pins-default {
pinctrl-single,pins = <
AM64X_IOPAD(0x00b8, PIN_INPUT, 2) /* (Y7) PRG1_PRU0_GPO0.PRG1_RGMII1_RD0 */
AM64X_IOPAD(0x00bc, PIN_INPUT, 2) /* (U8) PRG1_PRU0_GPO1.PRG1_RGMII1_RD1 */
AM64X_IOPAD(0x00c0, PIN_INPUT, 2) /* (W8) PRG1_PRU0_GPO2.PRG1_RGMII1_RD2 */
AM64X_IOPAD(0x00c4, PIN_INPUT, 2) /* (V8) PRG1_PRU0_GPO3.PRG1_RGMII1_RD3 */
AM64X_IOPAD(0x00c8, PIN_INPUT, 2) /* (Y8) PRG1_PRU0_GPO4.PRG1_RGMII1_RX_CTL */
AM64X_IOPAD(0x00d0, PIN_INPUT, 2) /* (AA7) PRG1_PRU0_GPO6.PRG1_RGMII1_RXC */
AM64X_IOPAD(0x00e4, PIN_OUTPUT, 2) /* (AA8) PRG1_PRU0_GPO11.PRG1_RGMII1_TD0 */
AM64X_IOPAD(0x00e8, PIN_OUTPUT, 2) /* (U9) PRG1_PRU0_GPO12.PRG1_RGMII1_TD1 */
AM64X_IOPAD(0x00ec, PIN_OUTPUT, 2) /* (W9) PRG1_PRU0_GPO13.PRG1_RGMII1_TD2 */
AM64X_IOPAD(0x00f0, PIN_OUTPUT, 2) /* (AA9) PRG1_PRU0_GPO14.PRG1_RGMII1_TD3 */
AM64X_IOPAD(0x00f4, PIN_OUTPUT, 2) /* (Y9) PRG1_PRU0_GPO15.PRG1_RGMII1_TX_CTL */
AM64X_IOPAD(0x00f8, PIN_OUTPUT, 2) /* (V9) PRG1_PRU0_GPO16.PRG1_RGMII1_TXC */
>;
};
icssg1_rgmii2_pins_default: icssg1-rgmii2-pins-default {
pinctrl-single,pins = <
AM64X_IOPAD(0x0108, PIN_INPUT, 2) /* (W11) PRG1_PRU1_GPO0.PRG1_RGMII2_RD0 */
AM64X_IOPAD(0x010c, PIN_INPUT, 2) /* (V11) PRG1_PRU1_GPO1.PRG1_RGMII2_RD1 */
AM64X_IOPAD(0x0110, PIN_INPUT, 2) /* (AA12) PRG1_PRU1_GPO2.PRG1_RGMII2_RD2 */
AM64X_IOPAD(0x0114, PIN_INPUT, 2) /* (Y12) PRG1_PRU1_GPO3.PRG1_RGMII2_RD3 */
AM64X_IOPAD(0x0118, PIN_INPUT, 2) /* (W12) PRG1_PRU1_GPO4.PRG1_RGMII2_RX_CTL */
AM64X_IOPAD(0x0120, PIN_INPUT, 2) /* (U11) PRG1_PRU1_GPO6.PRG1_RGMII2_RXC */
AM64X_IOPAD(0x0134, PIN_OUTPUT, 2) /* (AA10) PRG1_PRU1_GPO11.PRG1_RGMII2_TD0 */
AM64X_IOPAD(0x0138, PIN_OUTPUT, 2) /* (V10) PRG1_PRU1_GPO12.PRG1_RGMII2_TD1 */
AM64X_IOPAD(0x013c, PIN_OUTPUT, 2) /* (U10) PRG1_PRU1_GPO13.PRG1_RGMII2_TD2 */
AM64X_IOPAD(0x0140, PIN_OUTPUT, 2) /* (AA11) PRG1_PRU1_GPO14.PRG1_RGMII2_TD3 */
AM64X_IOPAD(0x0144, PIN_OUTPUT, 2) /* (Y11) PRG1_PRU1_GPO15.PRG1_RGMII2_TX_CTL */
AM64X_IOPAD(0x0148, PIN_OUTPUT, 2) /* (AA4) PRG1_PRU1_GPO16.PRG1_RGMII2_TXC */
>;
};
&icssg1_mdio {
status = "okay";
pinctrl-names = "default";
pinctrl-0 = <&icssg1_mdio_pins_default &clkout1_pins_default>;
icssg1_phy1: ethernet-phy@1 {
status = "okay";
compatible = "ethernet-phy-ieee802.3-c22";
reg = <0x1>;
reset-gpios = <&main_gpio1 17 GPIO_ACTIVE_LOW>;
reset-assert-us = <1000>;
reset-deassert-us = <1000>;
};
icssg1_phy2: ethernet-phy@2 {
status = "okay";
compatible = "ethernet-phy-ieee802.3-c22";
reg = <0x0>;
reset-gpios = <&main_gpio1 17 GPIO_ACTIVE_LOW>;
reset-assert-us = <1000>;
reset-deassert-us = <1000>;
};
};
icssg1_eth: icssg1-eth {
compatible = "ti,am642-icssg-prueth";
pinctrl-names = "default";
pinctrl-0 = <&icssg1_rgmii1_pins_default &icssg1_rgmii2_pins_default>;
sram = <&oc_sram>;
ti,prus = <&pru1_0>, <&rtu1_0>, <&tx_pru1_0>, <&pru1_1>, <&rtu1_1>, <&tx_pru1_1>;
firmware-name = "ti-pruss/am65x-sr2-pru0-prueth-fw.elf",
"ti-pruss/am65x-sr2-rtu0-prueth-fw.elf",
"ti-pruss/am65x-sr2-txpru0-prueth-fw.elf",
"ti-pruss/am65x-sr2-pru1-prueth-fw.elf",
"ti-pruss/am65x-sr2-rtu1-prueth-fw.elf",
"ti-pruss/am65x-sr2-txpru1-prueth-fw.elf";
ti,pruss-gp-mux-sel = <2>, /* MII mode */
<2>,
<2>,
<2>, /* MII mode */
<2>,
<2>;
ti,mii-g-rt = <&icssg1_mii_g_rt>;
ti,mii-rt = <&icssg1_mii_rt>;
ti,iep = <&icssg1_iep0>, <&icssg1_iep1>;
interrupt-parent = <&icssg1_intc>;
interrupts = <24 0 2>, <25 1 3>;
interrupt-names = "tx_ts0", "tx_ts1";
dmas = <&main_pktdma 0xc200 15>, /* egress slice 0 */
<&main_pktdma 0xc201 15>, /* egress slice 0 */
<&main_pktdma 0xc202 15>, /* egress slice 0 */
<&main_pktdma 0xc203 15>, /* egress slice 0 */
<&main_pktdma 0xc204 15>, /* egress slice 1 */
<&main_pktdma 0xc205 15>, /* egress slice 1 */
<&main_pktdma 0xc206 15>, /* egress slice 1 */
<&main_pktdma 0xc207 15>, /* egress slice 1 */
<&main_pktdma 0x4200 15>, /* ingress slice 0 */
<&main_pktdma 0x4201 15>; /* ingress slice 1 */
dma-names = "tx0-0", "tx0-1", "tx0-2", "tx0-3",
"tx1-0", "tx1-1", "tx1-2", "tx1-3",
"rx0", "rx1";
ethernet-ports {
#address-cells = <1>;
#size-cells = <0>;
icssg1_emac0: port@0 {
reg = <0>;
phy-handle = <&icssg1_phy1>;
phy-mode = "rgmii-txid";
ti,syscon-rgmii-delay = <&main_conf 0x4110>;
/* Filled in by bootloader */
local-mac-address = [00 00 00 00 00 00];
};
icssg1_emac1: port@1 {
reg = <1>;
phy-handle = <&icssg1_phy2>;
phy-mode = "rgmii-txid";
ti,syscon-rgmii-delay = <&main_conf 0x4114>;
/* Filled in by bootloader */
local-mac-address = [00 00 00 00 00 00];
};
};
};
};我们使用 phy。 我们将使用内核6.11和自定义 Yocto 构建。
谢谢