请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:TDA4VM Thread 中讨论的其他器件:CSD
工具与软件:
1、我们进行了16小时的高温和低温压力测试,发现我们的睡眠文件在压力测试后损坏
root@j721e-evm:~# ls -l /bin/ [ 7052.671361] EXT4-fs error (device mmcblk0p2): ext4_lookup:1851: inode #39: comm ls: iget: bad extended attribute block 141733921779 ls: cannot access '/bin/sleep': Structure needs cleaning lrwxrwxrwx 1 1083 1083 14 Mar 9 2018 sh -> /bin/bash.bash l????????? ? ? ? ? ? sleep -rwxr-xr-x 1 1083 1083 39496 Mar 9 2018 sleep.coreutils
2 μ s 与、的睡眠文件 MD5相比、发现了更改
root@j721e-evm:~# md5sum /bin/sleep [ 7183.920146] EXT4-fs error (device mmcblk0p2): ext4_lookup:1851: inode #39: comm md5sum: iget: bad extended attribute block 141733921779 md5sum: /bin/sleep: Structure needs cleaning root@j721e-evm:~# md5sum /bin/sleep.coreutils 1cf18ac911052676f370fdcd9ecb71f7 /bin/sleep.coreutils root@j721e-evm:~# md5sum /run/media/bin/sleep.coreutils media/ root@j721e-evm:~# md5sum /run/media/rootfs-mmcblk0p3/bin/sleep.coreutils 1cf18ac911052676f370fdcd9ecb71f7 /run/media/rootfs-mmcblk0p3/bin/sleep.coreutils root@j721e-evm:~# md5sum /run/media/rootfs-mmcblk0p3/bin/sleep 1cf18ac911052676f370fdcd9ecb71f7 /run/media/rootfs-mmcblk0p3/bin/sleep root@j721e-evm:~#
3、log
[ 970.942709] EXT4-fs error (device mmcblk0p2): ext4_lookup:1851: inode #39: comm sh: iget: bad extended attribute block 141733921779 [ 974.278923] EXT4-fs error (device mmcblk0p2): ext4_lookup:1851: inode #39: comm sh: iget: bad extended attribute block 141733921779 [ 974.290866] EXT4-fs error (device mmcblk0p2): ext4_lookup:1851: inode #39: comm sh: iget: bad extended attribute block 141733921779 l[ 976.369471] EXT4-fs error (device mmcblk0p2): ext4_lookup:1851: inode #39: comm sh: iget: bad extended attribute block 141733921779 [ 976.381406] EXT4-fs error (device mmcblk0p2): ext4_lookup:1851: inode #39: comm sh: iget: bad extended attribute block 141733921779
4、eMMC 压力测试出现问题后、读取和写入无异常
Start Emmc Test time:56 ####################### Thu Apr 28 19:36:29 UTC 2022 ########################### clock: 200000000 Hz actual clock: 200000000 Hz vdd: 7 (1.65 - 1.95 V) bus mode: 2 (push-pull) chip select: 0 (don't care) power mode: 2 (on) bus width: 3 (8 bits) timing spec: 9 (mmc HS200) signal voltage: 1 (1.80 V) driver type: 0 (driver type B) Start dd 2048M test.bin 2141192192 bytes (2.1 GB, 2.0 GiB) copied, 54 s, 39.6 MB/s 2048+0 records in 2048+0 records out 2147483648 bytes (2.1 GB, 2.0 GiB) copied, 54.1581 s, 39.7 MB/s End dd 2048M test.bin Start rm test.bin End rm test.bin eMMC Life Time Estimation A [EXT_CSD_DEVICE_LIFE_TIME_EST_TYP_A]: 0x01 eMMC Life Time Estimation B [EXT_CSD_DEVICE_LIFE_TIME_EST_TYP_B]: 0x01 eMMC Pre EOL information [EXT_CSD_PRE_EOL_INFO]: 0x01 End Emmc Test time:56 ######################## Thu Apr 28 19:37:24 UTC 2022 ###########################
、Ω eMMC 模型 KLM8G1GEUF-B04%