请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:AM623 工具与软件:
您好!
我们在项目中使用 AM623定制电路板、但我们的电路板设计不包含 EEPROM 组件。 尽管如此、我们在引导过程或操作期间会观察到与 EEPROM 相关的日志消息。 这些日志在我们的设置中是不必要的、会在调试过程中引起混淆。
您能否指导我们如何从系统日志中抑制或删除这些与 EEPROM 相关的消息? 如果需要更改配置、修改内核或更新设备树、请提供详细说明。
U-Boot SPL 2023.04-ti-gf9b966c67473 (Mar 19 2024 - 20:31:40 +0000) SYSFW ABI: 3.1 (firmware rev 0x0009 '9.2.7--v09.02.07 (Kool Koala)') SPL initial stack usage: 1856 bytes ** Bad device specification mmc 1 ** Couldn't find partition mmc 1:1 Error: could not access storage. Trying to boot from MMC1 Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted U-Boot 2023.04-ti-gf9b966c67473 (Mar 19 2024 - 20:31:40 +0000) SoC: AM62X SR1.0 GP Model: Texas Instruments AM625 SK EEPROM not available at 80, trying to read at 81 Reading on-board EEPROM at 0x51 failed -121 DRAM: no bloblist found!2 GiB Core: 65 devices, 30 uclasses, devicetree: separate MMC: mmc@fa10000: 0 Loading Environment from nowhere... OK In: serial Out: serial Err: serial EEPROM not available at 80, trying to read at 81 Reading on-board EEPROM at 0x51 failed -121 Net: eth0: ethernet@8000000port@1 Hit any key to stop autoboot: 0 switch to partitions #2, OK mmc0(part 2) is current device
此致、vikash