工具与软件:
PSDK 版本:RTOS (8.4.0.6)+ Linux (8.4.0.11)
您好!
我们的工程没有任何网络要求、因此我们从 SDK 中删除了网络驱动程序。 我们的压力测试目前存在问题、MCU2_0中偶尔会出现 UDMA 初始化故障。我们的修改如下。 是否有任何其他需要修改的内容?
引导模式:SBL + CAN_BOOT_APP
代码 修改:
1 μ s)ETH
psdkra/vision_apps/vision_apps_build_flags.mak
BUILD_ENABLE_ETHFW=否
2)禁用 Linux dts 节点 cpsw9g_virt_mac 和 cpsw9g_virt_maconly
日志:
[MCU2_0] 0.375992 s: CIO: Init ... Done !!! [MCU2_0] 0.376068 s: ### CPU Frequency = 1000000000 Hz [MCU2_0] 0.376116 s: APP: Init ... !!! [MCU2_0] 0.376144 s: SCICLIENT: Init ... !!! [MCU2_0] 0.381851 s: SCICLIENT: DMSC FW version [8.4.1--v08.04.01 (Jolly Jellyfi] [MCU2_0] 0.381921 s: SCICLIENT: DMSC FW revision 0x8 [MCU2_0] 0.381965 s: SCICLIENT: DMSC FW ABI revision 3.1 [MCU2_0] 0.382007 s: SCICLIENT: Init ... Done !!! [MCU2_0] 0.382038 s: UDMA: Init ... !!! [MCU2_0] 0.393503 s: [UDMA] [MCU2_0] 0.393550 s: [Error] SciClient Set proxy config failed!!! [MCU2_0] 0.393594 s: UDMA: ERROR: Udma_init failed !!! [MCU2_0] 0.393631 s: UDMA: Init ... Done !!! [MCU2_1] 0.333004 s: CIO: Init ... Done !!! [MCU2_1] 0.333076 s: ### CPU Frequency = 1000000000 Hz [MCU2_1] 0.333120 s: APP: Init ... !!! [MCU2_1] 0.333145 s: SCICLIENT: Init ... !!! [MCU2_1] 0.333429 s: SCICLIENT: DMSC FW version [8.4.1--v08.04.01 (Jolly Jellyfi] [MCU2_1] 0.333484 s: SCICLIENT: DMSC FW revision 0x8 [MCU2_1] 0.333521 s: SCICLIENT: DMSC FW ABI revision 3.1 [MCU2_1] 0.333558 s: SCICLIENT: Init ... Done !!! [MCU2_1] 0.333586 s: UDMA: Init ... !!! [MCU2_1] 0.339346 s: UDMA: Init ... Done !!! [MCU2_1] 0.339410 s: MEM: Init ... !!! [MCU2_1] 0.339457 s: MEM: Created heap (DDR_LOCAL_MEM, id=0, flags=0x00000004) @ d7000000 of size 16777216 bytes !!! [MCU2_1] 0.339531 s: MEM: Created heap (L3_MEM, id=1, flags=0x00000001) @ 3640000 of size 262144 bytes !!! [MCU2_1] 0.339590 s: MEM: Init ... Done !!! [MCU2_1] 0.339628 s: IPC: Init ... !!! [MCU2_1] 0.339692 s: IPC: 6 CPUs participating in IPC !!! [MCU2_1] 0.339740 s: IPC: Waiting for HLOS to be ready ... !!! [MCU2_1] 4.944300 s: IPC: HLOS is ready !!! [MCU2_1] 4.964996 s: IPC: Init ... Done !!! [MCU2_1] 4.965064 s: APP: Syncing with 5 CPUs ... !!!
谢谢。