This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] SK-AM62A-LP:无法在 DL 加速器上使用自定义样式模型执行推理

Guru**** 2481755 points


请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1449522/sk-am62a-lp-unable-to-perform-inferencing-using-custom-tflite-model-on-dl-accelerator

器件型号:SK-AM62A-LP

工具与软件:

团队成员、您好!

我的团队和我正在努力运行 ML 模型、该模型能够在 AM62A EVM 上执行弱光图像增强。 我们正在尝试将一些处理转移到 DL 加速器。 我们能够使用 edgeai_tidl_tools 编译模型并生成模型的工件。  

我们使用了 edgeai_gst_apps 来运行该模型。 我们编写了以下配置文件:  

title: "Low Light Enhancement"
log_level: 2
inputs:
    input0:
        source: /dev/video-usb-cam0
        format: jpeg
        width: 1280
        height: 720
        framerate: 30
    input1:
        source: /home/weston/image.jpg
        width: 600
        height: 400
        index: 0
        framerate: 1
        loop: False
models:
    model0:
        model_path: /opt/model_zoo/zero_dce_model
outputs:
    output0:
        sink: kmssink
        width: 1920
        height: 1080
        overlay-perf-type: graph
    output1:
        sink: /home/weston/image_enhanced.jpg  
        width: 600
        height: 400
flows:
    flow0: [input1,model0,output1]

已验证配置文件中提供的路径。 但是、运行 app_edgeai.py 脚本会提供以下输出、并且不会生成增强的映像:

 Number of subgraphs:8 , 43 nodes delegated out of 51 nodes

APP: Init ... !!!
    72.527621 s: MEM: Init ... !!!
    72.527692 s: MEM: Initialized DMA HEAP (fd=6) !!!
    72.527880 s: MEM: Init ... Done !!!
    72.527909 s: IPC: Init ... !!!
    72.544456 s: IPC: Init ... Done !!!
REMOTE_SERVICE: Init ... !!!
REMOTE_SERVICE: Init ... Done !!!
    72.552242 s: GTC Frequency = 200 MHz
APP: Init ... Done !!!
    72.555707 s:  VX_ZONE_INIT:Enabled
    72.555749 s:  VX_ZONE_ERROR:Enabled
    72.555759 s:  VX_ZONE_WARNING:Enabled
    72.556967 s:  VX_ZONE_INIT:[tivxPlatformCreateTargetId:124] Added target MPU-0
    72.557151 s:  VX_ZONE_INIT:[tivxPlatformCreateTargetId:124] Added target MPU-1
    72.557257 s:  VX_ZONE_INIT:[tivxPlatformCreateTargetId:124] Added target MPU-2
    72.557352 s:  VX_ZONE_INIT:[tivxPlatformCreateTargetId:124] Added target MPU-3
    72.557366 s:  VX_ZONE_INIT:[tivxInitLocal:136] Initialization Done !!!
    72.558931 s:  VX_ZONE_INIT:[tivxHostInitLocal:106] Initialization Done for HOST !!!
INFO: Created TensorFlow Lite XNNPACK delegate for CPU.
==========[INPUT PIPELINE(S)]==========

[PIPE-0]

multifilesrc location=/home/weston/image.jpg index=1 ! jpegdec ! videoscale qos=True ! capsfilter caps="video/x-raw, width=(int)600, height=(int)400;" ! tiovxdlcolorconvert ! capsfilter caps="video/x-raw, format=(string)NV12;" ! tiovxmultiscaler name=split_01  
split_01. ! queue ! capsfilter caps="video/x-raw, width=(int)600, height=(int)400;" ! tiovxdlcolorconvert out-pool-size=4 ! capsfilter caps="video/x-raw, format=(string)RGB;" ! appsink max-buffers=2 drop=True name=sen_0
split_01. ! queue ! capsfilter caps="video/x-raw, width=(int)600, height=(int)400;" ! videoscale qos=True ! capsfilter caps="video/x-raw, width=(int)600, height=(int)600;" ! tiovxdlpreproc out-pool-size=4 channel-order=1 ! capsfilter caps="application/x-tensor-tiovx;" ! appsink max-buffers=2 drop=True name=pre_0


==========[OUTPUT PIPELINE]==========

    73.144299 s: MEM: ERROR: Alloc failed with status = 12 !!!
    73.144351 s:  VX_ZONE_ERROR:[tivxMemBufferAlloc:90] Shared mem ptr allocation failed
    73.145215 s: MEM: ERROR: Alloc failed with status = 12 !!!
    73.145253 s:  VX_ZONE_ERROR:[tivxMemBufferAlloc:90] Shared mem ptr allocation failed
    73.151641 s: MEM: ERROR: Alloc failed with status = 12 !!!
    73.151696 s:  VX_ZONE_ERROR:[tivxMemBufferAlloc:90] Shared mem ptr allocation failed
appsrc do-timestamp=True format=3 block=True name=post_0 ! tiovxdlcolorconvert ! capsfilter caps="video/x-raw, format=(string)NV12, width=(int)600, height=(int)400;" ! v4l2jpegenc ! multifilesink sync=False location=/home/weston/image_enhanced.jpg

    73.183287 s: MEM: ERROR: Alloc failed with status = 12 !!!
    73.183343 s:  VX_ZONE_ERROR:[tivxMemBufferAlloc:90] Shared mem ptr allocation failed
    73.184087 s: MEM: ERROR: Alloc failed with status = 12 !!!
    73.184120 s:  VX_ZONE_ERROR:[tivxMemBufferAlloc:90] Shared mem ptr allocation failed
    73.184637 s: MEM: ERROR: Alloc failed with status = 12 !!!
    73.184662 s:  VX_ZONE_ERROR:[tivxMemBufferAlloc:90] Shared mem ptr allocation failed
    73.185169 s: MEM: ERROR: Alloc failed with status = 12 !!!
    73.185190 s:  VX_ZONE_ERROR:[tivxMemBufferAlloc:90] Shared mem ptr allocation failed


 +--------------------------------------------------------------------------+
 | Low Light Enhancement                                                    |
 +--------------------------------------------------------------------------+
 +--------------------------------------------------------------------------+
 | Input Src: /home/weston/image.jpg                                        |
 | Model Name: zero_dce_model                                               |
 | Model Type: custom                                                       |
 +--------------------------------------------------------------------------+
 +--------------------------------------------------------------------------+


 +--------------------------------------------------------------------------+
 | Low Light Enhancement                                                    |
 +--------------------------------------------------------------------------+
 +--------------------------------------------------------------------------+
 | Input Src: /home/weston/image.jpg                                        |
 | Model Name: zero_dce_model                                               |
 | Model Type: custom                                                       |
 +--------------------------------------------------------------------------+
 +--------------------------------------------------------------------------+


    75.493006 s:  VX_ZONE_WARNING:[vxReleaseContext:1213] Found a reference 0xffff781164a8 of type 00000815 at external count 7, internal count 0, releasing it
    75.493056 s:  VX_ZONE_WARNING:[vxReleaseContext:1215] Releasing reference (name=tensor_202) now as a part of garbage collection
    75.493091 s:  VX_ZONE_WARNING:[vxReleaseContext:1213] Found a reference 0xffff780f7a18 of type 00000813 at external count 1, internal count 0, releasing it
    75.493104 s:  VX_ZONE_WARNING:[vxReleaseContext:1215] Releasing reference (name=object_array_208) now as a part of garbage collection
    75.493524 s:  VX_ZONE_WARNING:[vxReleaseContext:1213] Found a reference 0xffff780f7bc0 of type 00000813 at external count 1, internal count 0, releasing it
    75.493539 s:  VX_ZONE_WARNING:[vxReleaseContext:1215] Releasing reference (name=object_array_210) now as a part of garbage collection
    75.493919 s:  VX_ZONE_WARNING:[vxReleaseContext:1213] Found a reference 0xffff780f7d68 of type 00000813 at external count 1, internal count 0, releasing it
    75.493934 s:  VX_ZONE_WARNING:[vxReleaseContext:1215] Releasing reference (name=object_array_214) now as a part of garbage collection
    75.494401 s:  VX_ZONE_INIT:[tivxHostDeInitLocal:120] De-Initialization Done for HOST !!!
    75.499484 s:  VX_ZONE_INIT:[tivxDeInitLocal:206] De-Initialization Done !!!
APP: Deinit ... !!!
REMOTE_SERVICE: Deinit ... !!!
REMOTE_SERVICE: Deinit ... Done !!!
    75.499976 s: IPC: Deinit ... !!!
    75.500485 s: IPC: DeInit ... Done !!!
    75.500532 s: MEM: Deinit ... !!!
    75.500549 s: DDR_SHARED_MEM: Alloc's: 109 alloc's of 200056184 bytes
    75.500561 s: DDR_SHARED_MEM: Free's : 109 free's  of 200056184 bytes
    75.500571 s: DDR_SHARED_MEM: Open's : 0 allocs  of 0 bytes
    75.500587 s: MEM: Deinit ... Done !!!
APP: Deinit ... Done !!!

编译模型
e2e.ti.com/.../zero_5F00_dce_5F00_model.zip

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好!

    我看了一下你的模型和模型工件。 模型不应占用足够的内存/DDR 来运行内存不足、如一些打印输出所示。 更有可能是编译过程中出现故障。  

    由于我们不支持 Square 节点,您的模型有许多子图(请参阅此处的文档以了解支持的操作)。 我建议修改您的模型,将 Square 替换为 MUL 节点,并将张量本身相乘 .

    有时许多子图会引入更高的错误可能性--在这种情况下有更多的临界情况。 对于可以使用1-2个子图(您的有8个、最多为16个)进行编译的模型、这些工具更稳定。

    此外、请将批处理大小设置为1、而不是动态值(如-1)

    在此阶段、我建议在没有完整成像流水线的情况下运行此模型、以便您可以在更简单的应用程序中检查该模型。

    我建议使用 edgeai-tidl-tools/examples/osrt_python/ort/onnxrt_ep.py 进行该测试。 您可以使用它来编译模型、然后将部分存储库传输到 SDK (大多数情况下、您可以传输除 tidl_tools 目录之外的所有内容、该目录仅用于在 x86上进行编译/仿真)。 然后、对于主机仿真模式、以与 PC 上相同的方式运行(python3 onnxrt_ep.py -m model_name)

    在此模式下运行模型时(仅使用单映像)、请运行 debug_level=2。 您可以在模型配置中将其设置为"optional_options" 的一部分、也可以在 common_utils.py 中全局设置。 另外、请在后台运行/opt/vx_app_arm_remote_log.out、然后运行 onnxrt_ep.py 并共享日志。  

    总结:

    -在您的模型中,将 Square 替换为 MUL 或等效节点
    -使用 edgeai-tidl-tools 在目标上重新编译和运行模型。 如果仍然失败、请使用 debug_level=2和运行 后台的/opt/vx_app_arm_remote_log.out 共享编译和运行时日志(仅适用于 EVM)

    BR、
    Reese

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    Reese、您好!

    感谢您的建议。 我们将所有平方节点替换为多路复用节点、在编译模型时、我们能够在一个子图中获得所有节点。

    新的编译模型

    e2e.ti.com/.../zero_5F00_dce_5F00_model_5F00_no_5F00_sq.zip

    关于在 edgeai-tidl-tools 上运行模型的问题、由于我们的模型不属于三个可用类别(分类、检测或分段)中的任何一个类别、因此程序中没有可以处理写入由我们的模型生成的输出图像的逻辑。 而是尝试在 EVM 上的自定义 python 脚本上运行它。

    from tflite_runtime.interpreter import Interpreter as tfl
    from tflite_runtime.interpreter import load_delegate
    import numpy as np
    import cv2
    import time
    
    tidl_delegate_path = '/usr/lib/libtidl_tfl_delegate.so'
    tidl_options = {"artifacts_folder": "zero_dce_model_no_sq/artifacts","debug_level": 2,}
    tidl_delegate = load_delegate(tidl_delegate_path, options=tidl_options)
    
    modelpath = 'zero_dce_model_no_sq/model/zero_dce_model_no_sq.tflite'
    
    input_image = cv2.imread("image.png")
    
    interpret = tfl(model_path=modelpath,experimental_delegates=[tidl_delegate])
    interpret.allocate_tensors()
    input_details = interpret.get_input_details()
    output_details = interpret.get_output_details()
    
    input_image = cv2.resize(input_image, (600, 400))
    input_data = np.array(input_image).astype(np.float32) / 255.0
    input_data = np.expand_dims(input_data, axis=0) 
    interpret.set_tensor(input_details[0]['index'], input_data)
    interpret.invoke()
    
    output_data = interpret.get_tensor(output_details[0]['index'])
    output_image_data = (output_data[0] * 255).clip(0, 255).astype(np.uint8)
    cv2.imwrite("image_processed_no_sq.png", output_image_data)
    print ('Done') 
    print ('Closing')

    此脚本确实运行过、但我们得到的输出是纯黑色图像。

    自定义脚本生成的日志:

    e2e.ti.com/.../prog_5F00_log.txt

    由 在后台运行的 vx_app_arm_remote_log.out 生成的日志

    e2e.ti.com/.../remote_5F00_log.txt

    我注意到的一件事是自定义 Python 脚本的最终打印语句执行得更早(如 prog_log.txt 的第101行所示)。 我认为这里发生的情况是、甚至在 C7x 加速器完成图像处理之前、CPU 也会对输出文件进行写入。 如果是这种情况、是否有办法使两个进程同步?

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好、Joel:

    这种信息/日志是伟大的,感谢您提供。  

    你的日志对我来说很普通--我看不到任何关于它们的东西  

    我注意到的一件事是自定义 Python 脚本的最终打印语句执行得更早(如 prog_log.txt 的第101行所示)。

    这是正常的。  在后台运行 TIDL 推理调用时、会创建多个进程/线程。 这些(加上 python 解释器)可能会并行将数据推送到标准输出(stdout)中、以使某些线交错。 这并不表示存在任何问题、它只是并行处理的(不幸的)副作用-毕竟、AM62A EVM 上有4个 A53内核共同运行 Linux 操作系统。

    您看到的关于层周期的打印内容以及这些打印内容均来自 TIDL 软件栈内部、在 AI 加速器(C7x DSP 内核)上完成推理之后才会开始打印。 否则、打印会减慢模型推理本身并影响性能和任何内部测量

    有关您的精度  

    我的第一个估计是您的网络对量化反应不是很好。 默认情况下、TIDL 使用8位量化来计算最初训练并由浮点值组成的神经网络。 有些网络对此的响应更差、弱光增强模型可能就是其中之一。  

    这些文档有一些调试建议和指导:

    我通常建议将 tensor_bits 设置为16 (默认值为8)、对您的模型进行量化。 以这种方式编译模型、并检查精度是否可接受。 这会降低性能、但是一项有用的检查

    校准也是量化的一个重要部分。 基本上、我们通过您的网络以浮点方式运行映像、并收集有关中间密度的统计数据。 这些帮助我们确定量化参数、以将 fp32范围的一部分映射到整数范围(8位或16位)。 此处使用的图像很重要、因为它们会影响生成的统计数据。 您的模型是针对弱光而构建的、因此使用光照良好的图像可能不会达到正确的激活范围。  

    BR、
    Reese

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    Reese、您好!

    感谢您的建议。 我们在编译模型时更改了用于校准的图像。  

    我们最终能够使用相同的自定义脚本从模型中获取输出。 我们注意到两件事:

    1. 模型的输出实际上是一个双精度归一化值数组(pixel_value/255、然后再除以255)、因此这一行
       
      output_image_data = (output_data[0] * 255).clip(0, 255).astype(np.uint8)

      实际上是在将数据转换为 uint8类型时仅向输出写入零。 我们 必须进行以下更改才能获取输出图像。 我们不知道为什么会这样。
      output_image_data = (output_data[0] * 255 * 255).clip(0, 255).astype(np.uint8)
    2. 这是原始图像:

      这是经过处理的图像:

      输出中有一个奇怪的亮条。 有什么想法为什么会发生这种情况?
  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好!

    这是进步!

    我同意这是奇怪,你需要乘以255再次... 这似乎是错误的、这可能是图像的某些部分饱和的原因。 听起来、网络的输出已包含标准化、这就是您必须执行此操作的原因。 我可以看到这可能会对准确性产生不利影响、尤其是因为数据必须已经经历去量化。 在这种情况下、任何浮点错误都可能会变得更糟。

    一些问题可以帮助您朝着正确的方向发展:

    如果您在 CPU 上运行(不针对 TIDL 委派)、输出结果会是什么样的?

    • 类似地、是否需要进行此附加标准化?
    • 该输出看起来是否正常、还是与卸载到 TIDL 时看到的类似?

    您现在是以16位模式运行此网络、还是仍以8位模式运行?

    类似地、其他输入图像是否具有这种逐行效果?

    BR、
    Reese

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好!

    该模型运行在8位网络上。 我曾尝试使它成为16位、但程序只是挂起。  由  vx_app_arm_remote_log.out 在后台运行生成的日志:
    e2e.ti.com/.../4477.remote_5F00_log.txt

    在 CPU 上运行模型时、输出数据很清晰、仅标准化一次。

    此致、
    Joel Jojo.

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好、Joel:

    感谢这里的信息和日志。 CPU 版本看起来不错、所以可能与量化有关。

    如果原始版本不需要额外的*255 ,那么它实际上是一个带子对真正的问题做这在最终输出。

    你能给我提供你目前的一组文物吗? 我很好奇这些第49/50层是什么--它看起来在其中一层挂起。 我看到很多来自卷积层的警告、但这些警告不会发生挂起的情况。 看起来这是在模型初始化期间发生的、但尚未到达推理阶段。  

    您是否在实际的 AM62A 目标上运行此端口? 我们通常建议在调试精度时以 PC 仿真模式运行、但这不是必需的。 许多人认为在 PC 上进行此调试更为方便。

    BR、
    Reese

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    Reese、您好!

    张量位设置为16时生成的模型伪影:

    e2e.ti.com/.../zero_5F00_dce_5F00_model_5F00_no_5F00_sq_5F00_16.zip

    该模型正在实际的 AM62A 目标上使用。 有没有方法可以在 PC 上仿真 C7x 加速器、因为据我所见、在 PC 上运行代码仿真仅在 ARM 内核上运行代码。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好、Joel:

    您是否还可以为您的模型提供 model_config 条目、或者至少介绍您是如何编译模型的? 我无法重现您遇到的问题。 在校准期间、我在编译期间确实看到了 SEG 故障、这可能是由于没有正确的预处理参数(标称均值和缩放值)而导致的。

    我尝试了使用以下工具、但没有得到合理的输出

        'zero_dce_model_no_sq':
        {
           'model_path' : os.path.join(models_base_path, 'zero_dce_model_no_sq.tflite'),
           'source' : {'model_url': 'dummy', 'opt': True,  'infer_shape' : True},
           'mean': [0,0,0],
           'scale' : [1,1,1],
           'num_images' : numImages,
           'num_classes': 1000,
           'session_name' : 'tflitert' ,
           'model_type': 'low-light',
           'optional_options': { 
             'debug_level': 1,
             'tensor_bits': 8
           }
        },

    我在 tflrt_delegate.py 中添加了一些代码、以将"model_type"设置为"弱光、但会添加您的图像和后处理代码(mul by 255、并剪切到 uint8)。 使用此配置在 CPU 上运行不会产生输出、而使用 TIDL 运行会产生较差的结果。 在我这边(TIDL_TOOLS 10_00_06_00)、tensor_bit 8和 bit 16的编译失败、在定点执行校准期间似乎会发生

    是否有方法可以在 PC 上模拟 C7x 加速器、因为据我所见、在 PC 上运行代码只模拟在 ARM 内核上运行代码。

    是的、PC 上的相同代码(适当设置 TIDL_TOOLS_PATH 环境变量(也是编译所必需的)应该在 PC 的 C7x 仿真器上运行。 如果您的模型仅在 PC 的 CPU 上运行、则可能未正确生成模型工件。  

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    Reese、您好!

    我们在 TIDL 工具中修改了 model_configs.py 文件中的一个模型配置、然后使用 tflrt_delegate.py 脚本来编译它。

    "zero_dce_model_no_sq": create_model_config(
        source=AttrDict(
            model_url="",
        ),
        preprocess=AttrDict(
            resize=(600,400),
            crop=(600,400),
            data_layout="NHWC",
            resize_with_pad=False,
            reverse_channels=False,
        ),
        session=AttrDict(
            session_name="tflitert",
            model_path=os.path.join(models_base_path, "zero_dce_model_no_sq.tflite"),
            input_mean=[0, 0, 0],
            input_scale=[1 / 255, 1 / 255, 1 / 255],
            input_optimization=True,
        ),
        task_type="custom",
        extra_info=AttrDict(num_images=3, num_classes=0),
    ),

    我们通过直接修改 common_utils.py 中的变量更改了张量位

    此致、
    Joel

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好、Joel:

    感谢您通过此配置、现在我可以更有信心地重现您的问题。  

    我还没有找到一个可行的解决方案。 我看到 PC 上使用您的配置基于 CPU 的执行具有很高的精度。 我加入 TIDL 后、我看到8、16和32位伪影的黑色图像(所有输出像素=0)在 PC 上模拟它们以检查准确性-这不是典型的、我怀疑有一个错误。 您已经看到、模型本身的输出是低值浮点。

    我怀疑 Tanh 激活或条纹切片可能会引起一些奇怪的事情。 这不是真的 、但精度下降似乎发生在 StridedSlice 和输出之间的层中。

    • 当我 强制 Tanh 层和此后的一切 CPU (与前面的层模拟加速器),输出看起来合理(视觉特征都存在,但不像你的原始图像那样明亮)。 如果让网络访问 Convs 和 Tanh、则情况也是如此、但强制 StridedSlice 之后的层在 CPU 上运行。

    这告诉我、可能导致此处精确度问题的是多个 Elementwise (add、mul、sub 等)层。 如果使用 debug_level=3运行模型、它将在/tmp 目录下生成跟踪。 可以通过 tool like NumPy 加载二进制文件来检查这些文件

    data_last_og = np.fromfile('/tmp/tidl_trace_75_0049_0001_0001_00001_00003_00600x00400.y', dtype=np.int8)  

    文件名的位置取决于图形的编译方式。 对于 TIDL 运行的每一层、用户都会得到一个.y 输出文件。 当我观察这些时、我看到这些值不是零值、它们仍然包含信息、并且粗略地阅读->重塑->转置->写入到文件显示了有意义的视觉特征(尽管有些暗)。 量化的程度(8或16位)不会对其产生重大影响。

    浮点输出看起来太小了,但我目前看不到比简单地重复*255缩放更好的方法。 在最近的一篇评论中、我非常抱歉向您推了一个不同的方向。 我认为这会在我们堆栈中的某个位置构成一个错误、可能是32位流程中的一些缩放、用于在编译期间收集张量值的范围。  

    因此、我的建议是:

    • 按255*255的比例缩放输出、继续操作
    • 我将在这里收集一些信息、并以一个错误的形式记录--我认为它与 Elementwise 层和一些正在使用的缩放有关

    此外、请注意元件层并非特别高效(在计算利用率和内存方面)、尤其是考虑到这些元件层在3x600x400输入上运行的大小和数量。 这些层对您的模型至关重要、因此我不会直接提供替代方案的建议。 卷积和矩阵乘法将显著提高效率。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    Reese、您好!

    我们将源代码中带条纹的切片运算替换为卷积、然后重新塑造运算。 我们能够从这一变化中获得更好的结果。

    模型的源代码如下: https://colab.research.google.com/drive/17GckQm8LXURnkJDEqVYcAtLJqlShDYYb?usp=sharing

    对您的终端源代码有任何建议?

    此致、
    Joel Jojo.

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    Joel、您好!

    目前没有对模型源代码的直接反馈/建议。

    我很好奇的事实,输出 有这些非常明显的水平条带不同的照明"轮廓",所以说。 该条带的垂直尺寸是多少? 我相信你有600x400的图像,所以6条条每条会占用66行,但图像看起来有几个奇怪的行。 更有可能的是64行有这种行为、我们正在遇到在 Elementwise 层的一些错误

    • 如果我们想要查看是否来自特定层或网络的一部分、可以使用"dny_list"设置来防止某些层随着 TIDL 加速而运行
      • 您 也可以与 max_num_subgraphs 设置配对、以防止被拒绝的层之后的层也与 TIDL 运行。
      • 我在此建议的策略是拒绝一个层并设置 max_num_subgraphs=1、以便网络的其余部分在 Arm 上运行。 从哪一层开始、您会看到这些奇数水平条带?

    这里、量化到 tensor_bits=32时得到的结果是一样的吗? 从技术上讲、这不使用任何量化、而是使用基于自然 C 代码的参考流程(而不是具有加速器内在函数的优化代码)。  

    我也很好奇、您是否看到其他输入图像的行为相同。 我想您会的。

    BR、
    Reese