This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] AM6442:R5 SPL 无法在 HS-SE 器件上加载下一个工件

Guru**** 2557290 points
Other Parts Discussed in Thread: AM6442

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1463538/am6442-r5-spl-is-failing-to-load-the-next-artifact-on-hs-se-device

器件型号:AM6442

工具与软件:

我正在使用 AM6442 HS-SE (保险丝熔断)器件、并成功使 R5 SPL 运行、可能 SYSFW 也正在运行。
我现在遇到这个错误:

U-Boot SPL 2024.04-ti-g1eeee680688b (Jan 15 2025 - 18:01:08 +0000)
R5 Hardware (Murat's key)
Reset Source: COLD_BOOT
Resetting on cold boot to workaround ErrataID:i2331
Please resend tiboot3.bin in case of UART/DFU boot
resetting ...

U-Boot SPL 2024.04-ti-g1eeee680688b (Jan 15 2025 - 18:01:08 +0000)
R5 Hardware (Murat's key)
Reset Source: SW_MCU_WARMRST
SYSFW ABI: 3.1 (firmware rev 0x0009 '9.2.7--v09.02.07 (Kool Koala)')
EEPROM not available at 0x50, trying to read at 0x51
Reading on-board EEPROM at 0x51 failed -121
SPL initial stack usage: 13400 bytes
Trying to boot from MMC1
spl_mmc_load: 0 2048
spl_mmc_load: mcc dev 0
spl_mmc_load: spl_mmc_boot_mode 3
spl: MMCSD_MODE_EMMCBOOT
spl: mmc boot mode: raw
spl_mmc_load: raw_sect got set to 2048
spl_mmc_load: CONFIG_SYS_MMCSD_RAW_MODE_U_BOOT_USE_SECTOR
_spl_load: reading from offset 0x100000
_spl_load: header magic FDT_MAGIC
## Checking hash(es) for config conf-0 ... OK
## Checking hash(es) for Image atf ... OK
## Checking hash(es) for Image tee ... OK
## Checking hash(es) for Image dm ... OK
## Checking hash(es) for Image spl ... OK
ti_sci system-controller@44043000: Message not acknowledged
Authentication failed!
### ERROR ### Please RESET the board ###

问题:
1) 1)此时 SYSFW 是否成功运行?

2)哪种工件未能验证身份? tispl.bin?

3) 3)在哪里可以找到有关 tispl.bin 内部结构的文档、以便对问题进行调试?