请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:AM625 工具与软件:
问题说明:
尝试测试 GPIO N20、M21和 V25时出现问题。
GPIO 设置输出模式、设置0/1、测量发现电平没有变化;
GPIO 设置为输入模式、外部干预高/低电平、读取值不会改变。

我的 操作:



我的 DTS:


This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
工具与软件:
问题说明:
尝试测试 GPIO N20、M21和 V25时出现问题。
GPIO 设置输出模式、设置0/1、测量发现电平没有变化;
GPIO 设置为输入模式、外部干预高/低电平、读取值不会改变。

我的 操作:



我的 DTS:


您好!
在器件中、您将需要一个参考节点。 请参阅该主题的示例: https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1268671/sk-am62-using-the-gpios-in-the-40-pin-user-expansion-port/4804378
或者看到如下所示的内容:
diff --git a/arch/arm64/boot/dts/ti/k3-am62x-sk-common.dtsi b/arch/arm64/boot/dts/ti/k3-am62x-sk-common.dtsi
index b1980b85c..6a34c9eeb 100644
--- a/arch/arm64/boot/dts/ti/k3-am62x-sk-common.dtsi
+++ b/arch/arm64/boot/dts/ti/k3-am62x-sk-common.dtsi
@@ -186,6 +186,20 @@ AM62X_IOPAD(0x1cc, PIN_OUTPUT, 0) /* (E14/E11) UART0_TXD */
>;
};
+ main_gpio0_pins_default: main-gpio0-default-pins {
+ pinctrl-single,pins = <
+ AM62X_IOPAD(0x009c, PIN_INPUT, 7) /* (V25) GPMC0_WAIT1.GPIO0_38 */
+ AM62X_IOPAD(0x00ac, PIN_INPUT, 7) /* (L21) GPMC0_CSn1.GPIO0_42 */
+ >;
+ };
+
+ main_gpio1_pins_default: main-gpio1-default-pins {
+ pinctrl-single,pins = <
+ AM62X_IOPAD(0x01b4, PIN_INPUT, 7) /* (A13) SPI0_CS0.GPIO1_15 */
+ AM62X_IOPAD(0x01d0, PIN_INPUT, 7) /* (A15) UART0_CTSn.GPIO1_22 */
+ >;
+ };
+
main_i2c0_pins_default: main-i2c0-pins-default {
pinctrl-single,pins = <
AM62X_IOPAD(0x1e0, PIN_INPUT_PULLUP, 0) /* (B16/E12) I2C0_SCL */
@@ -329,6 +343,29 @@ AM62X_IOPAD(0x0078, PIN_OUTPUT, 1) /* (U24) GPMC0_AD15.VOUT0_DATA23 */
};
};
+&mcu_pmx0 {
+ mcugpio0_pins_default: mcugpio0-default-pins {
+ pinctrl-single,pins = <
+ AM62X_MCU_IOPAD(0x003c, PIN_INPUT, 7) /* (E5) MCU_MCAN1_TX.MCU_GPIO0_15 */
+ AM62X_MCU_IOPAD(0x0040, PIN_INPUT, 7) /* (D4) MCU_MCAN1_RX.MCU_GPIO0_16 */
+ >;
+ };
+};
+
+&main_gpio0 {
+ status = "okay";
+ pinctrl-names = "default";
+ pinctrl-0 = <&main_gpio0_pins_default>;
+
+};
+
+&main_gpio1 {
+ status = "okay";
+ pinctrl-names = "default";
+ pinctrl-0 = <&main_gpio1_pins_default>;
+
+};
+
&wkup_uart0 {
/* WKUP UART0 is used by DM firmware */
status = "reserved";
@@ -578,11 +615,13 @@ dpi1_out: endpoint {
};
};
-/* mcu_gpio0 and mcu_gpio_intr are reserved for mcu firmware usage */
+/* mcu_gpio0 and mcu_gpio_intr are reserved for mcu firmware usage */
&mcu_gpio0 {
- status = "reserved";
+ status = "okay";
+ pinctrl-names = "default";
+ pinctrl-0 = <&mcugpio0_pins_default>;
};
&mcu_gpio_intr {
- status = "reserved";
+ status = "okay";
};
此致、
Anshu