This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TRF37.0417万EVM:射频输出回路损耗

Guru**** 2614265 points


请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/rf-microwave-group/rf-microwave/f/rf-microwave-forum/1094083/trf370417evm-rf-output-return-loss

部件号:TRF37.0417万EVM
主题中讨论的其他部件:TRF37.0417万

测量TRF37.0417万评估板RF输出的返回损耗,从4GHz或更高频率来看,它似乎小于5dB。 事实上,在5.5GHz时,它小于2dB。 仅当5VDC提供给主板时才会出现此情况。 直流电源关闭时看起来更好。  输出缓冲区的外观有一些问题。

TI是否具有此端口的S参数,而不带系列电容器,我可以使用这些电容器来提高此输出的50欧姆匹配?