This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] AFE7900EVM:SPIA 无法控制 PLL 页面

Guru**** 2763545 points

Other Parts Discussed in Thread: AFE7900EVM

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/rf-microwave-group/rf-microwave/f/rf-microwave-forum/1221154/afe7900evm-spia-has-not-got-control-of-pll-pages

器件型号:AFE7900EVM

大家好!

我已经运行了所有例程、但是每个例程都有一个问题、即 SPIA 无法控制 PLL 页面。

我真的希望有人能帮助我。

#======
#Executing .. AFE79xx/bringup/setup.py
#Start Time 2023-04-27 15:57:29.120000 
AFE79xxLibraryPG1p0
spi - USB Instrument created.
resetDevice
Purge
MPSSE mode set
Kintex RegProgrammer - USB Instrument created.
Kintex RegProgrammer - USB Instrument created.
Kintex RegProgrammer - USB Instrument created.
#Done executing .. AFE79xx/bringup/setup.py
#End Time 2023-04-27 15:57:34.380000
#Execution Time = 5.26000022888 s 
#================ ERRORS:0, WARNINGS:0 ================#
#======
#Executing .. AFE79xx/bringup/devInit.py
#Start Time 2023-04-27 15:57:38.257000 
Power Card - USB Instrument created.
Reset the FPGA and try again.
Loaded Libraries
#Done executing .. AFE79xx/bringup/devInit.py
#End Time 2023-04-27 15:57:56.272000
#Execution Time = 18.0150001049 s 
#================ ERRORS:1, WARNINGS:0 ================#
#======
#Executing .. AFE79xx/bringup/reperter.py
#Start Time 2023-04-27 15:58:01.644000 
The External Sysref Frequency should be an integer factor of: 3.84MHz
2T2R1F Number: 0
Valid Configuration: True
laneRateRx: 9830.4
laneRateFb: 9830.4
laneRateTx: 9830.4
2T2R1F Number: 1
Valid Configuration: True
laneRateRx: 9830.4
laneRateFb: 9830.4
laneRateTx: 9830.4
Device Initialization for ChipVersion: 2.0
LMK Clock Divider - Device registers reset.
LMK Clock Divider - Device registers reset.
REFCLOCK is used from LMK source, ensure board connections are ok to do the same
DONOT_OPEN_Atharv_FULL - Device registers reset.
chipType: 0xa
chipId: 0x78
chipVersion: 0x20
SPIA has got control of PLL pages
PLL Pages SPI control relinquished.
Fuse farm load autoload done successful
No autload error
Fuse farm load autoload done successful
No autload error
SPIA has got control of PLL pages
PLL Locked
PLL Pages SPI control relinquished.
SPIA has got control of PLL pages
PLL Pages SPI control relinquished.
SPIA has Not got control of PLL pages
PLL Pages SPI control relinquished.
SPIA has Not got control of PLL pages
PLL Pages SPI control relinquished.
Sysref Read as expected
Waiting for MACRO_READY bit to go high, Count: 1
Waiting for MACRO_READY bit to go high, Count: 2
Waiting for MACRO_READY bit to go high, Count: 3
Waiting for MACRO_READY bit to go high, Count: 4
Waiting for MACRO_READY bit to go high, Count: 5
Waiting for MACRO_READY bit to go high, Count: 6
'''
Validation :  AFE79xx Library Version 
				v1.67, v1.74
Case			RX					TX						   FB						CLK					Notes
----	-----------------	  -----------------			-----------------			-----------			------------
1		245.76Msps, 24410     491.52Msps, 44210			491.52Msps, 22210			FADC=2949.12M       DAC in interleaved mode
		SerDes=9830.4Mbps     SerDes=9830.4Mbps			SerDes=9830.4Mbps			FDAC=8847.36M
		PLL0, NCO=3500M		  PLL0, NCO=3500M			NCO=3500M                   REF=491.52M
		
2		245.76Msps, 24410     491.52Msps, 44210			491.52Msps, 22210			FADC=2949.12M       DAC in straight mode
		SerDes=9830.4Mbps     SerDes=9830.4Mbps			SerDes=9830.4Mbps			FDAC=8847.36M
		PLL0, NCO=3500M		  PLL0, NCO=3500M			NCO=3500M                   REF=491.52M
'''
setupParams.skipFpga 				= 1
sysParams							= AFE.systemParams
setupParams.fpgaRefClk 				= 245.76	
AFE.systemStatus.loadTrims			= 1

sysParams.FRef                    	= 491.52
sysParams.FadcRx                  	= 2949.12
sysParams.FadcFb				  	= 2949.12
sysParams.Fdac                    	= 2949.12*3

sysParams.enableDacInterleavedMode	= False 					#DAC interleave mode to save power consumption. Fs/2 - Fin spur occurs

sysParams.modeTdd 					= 0		
										# 0- Single TDD Pin for all Channels
										# 1- Separate Control for 2T/2R/1F
										# 2- Separate Control for 1T/1R/1F			

sysParams.topLevelSystemMode		= 'StaticTDDMode'
sysParams.RRFMode 					= 0   #4T4R2F FDD mode
sysParams.jesdSystemMode			= [1,1]
										#SystemMode 0:	2R1F-FDD						; rx1-rx2-fb-fb
										#SystemMode 1:	1R1F-FDD						; rx1-rx1-fb-fb
										#SystemMode 2:	2R-FDD							; rx1-rx1-rx2-rx2
										#SystemMode 3:	1R								; rx1-rx1-rx1-rx1
										#SystemMode 4:	1F								; fb-fb-fb-fb
										#SystemMode 5:	1R1F-TDD						; rx1/fb-rx1/fb-rx1/fb-rx1/fb
										#SystemMode 8:	1R1F-TDD 1R-FDD	(FB-2Lanes)(RX1 RX2 interchanged)		; rx2/fb-rx2/fb-rx1-rx1


sysParams.jesdLoopbackEn			= 0 #Make it 1 to Enable the JESDTX to JESDRX internal loopback
sysParams.LMFSHdRx                	=['24410', '24410', '24410', '24410']	
										# The 2nd and 4th are valid only for jesdSystemMode values in (2,6,7,8). For other modes, select 4 converter modes for 1st and 3rd.
sysParams.LMFSHdFb                	= ["22210","22210"]
sysParams.LMFSHdTx                	= ["44210","44210","44210","44210"]
sysParams.jesdTxProtocol            = [0,0]
sysParams.jesdRxProtocol            = [0,0]
sysParams.serdesFirmware			= True 		# If you want to lead any firmware, please speify the path here. Otherwise it will not write any firmware
sysParams.jesdTxLaneMux				= [0,1,2,3,4,5,6,7]	
												# Enter which lanes you want in each location. 
												# Note that across 2T Mux is not possible in 0.5.
												# For example, if you want to exchange the first two lines of each 2T, this should be [[1,0,2,3],[5,4,6,7]]
sysParams.jesdRxLaneMux				= [0,1,2,3,4,5,6,7]	
												# Enter which lanes you want in each location.
												# Note that across 2R Mux is not possible in 0.5.
												# For example, if you want to exchange the first two lines of each 2R, this should be [[1,0,2,3],[5,4,6,7]]

sysParams.jesdRxRbd					= [4, 4]

sysParams.rxJesdTxScr				= [False,False,False,False]
sysParams.fbJesdTxScr				= [False,False]
sysParams.jesdRxScr					= [False,False,False,False]

sysParams.rxJesdTxK					= [32,32,32,32]
sysParams.fbJesdTxK					= [32,32]
sysParams.jesdRxK					= [16,16,16,16]
	
sysParams.ncoFreqMode 				= "1KHz"

sysParams.txNco0					= 	[[3500,2600],		#Band0, Band1 for TxA for NCO0
										[3500,2600],        #Band0, Band1 for TxB for NCO0
										[3500,2600],        #Band0, Band1 for TxC for NCO0
										[3500,2600]]        #Band0, Band1 for TxD for NCO0

sysParams.rxNco0					= 	[[3500,2600],		#Band0, Band1 for RxA for NCO0
										[3500,2600],        #Band0, Band1 for RxB for NCO0
										[3500,2600],        #Band0, Band1 for RxC for NCO0
										[3500,2600]]        #Band0, Band1 for RxD for NCO0

sysParams.fbNco0					= 	[3500,2200]			#FBA, FBC for NCO0
sysParams.fbNco1					= 	[3500,2200]			#FBA, FBC for NCO1
sysParams.fbNco2					= 	[3500,2200]			#FBA, FBC for NCO2
sysParams.fbNco3					= 	[3500,2200]			#FBA, FBC for NCO3

sysParams.numBandsRx				= [0]*4					# 0 for single, 1 for dual
sysParams.numBandsFb				= [0,0]				
sysParams.numBandsTx				= [0,0,0,0]

sysParams.ddcFactorRx             	= [12,12,12,12]			# DDC decimation factor for RX A, B, C and D
sysParams.ddcFactorFb             	= [6,6]
sysParams.ducFactorTx             	= [18,18,18,18]

AFE.systemStatus.loadTrims			=1

## The following parameters sets up the LMK04828 clocking schemes
lmkParams.pllEn						=	True#False
lmkParams.inputClk					=	1474.56#737.28
lmkParams.sysrefFreq				=	2949.12/1024
lmkParams.lmkFrefClk				=	True

## The following parameters sets up the register and macro dumps
logDumpInst.setFileName(ASTERIX_DIR+DEVICES_DIR+r"\Afe79xxPg1.txt")
logDumpInst.logFormat				= 0x0f
logDumpInst.rewriteFile				= 1
logDumpInst.rewriteFileFormat4		= 1
device.optimizeWrites				= 0
device.rawWriteLogEn				= 1

## The following parameters sets up the SYNCIN and SYNCOUT to interface with the TSW14J57
sysParams.jesdABLvdsSync			= 1
sysParams.jesdCDLvdsSync			= 1
sysParams.rxJesdTxSyncMux			= [0,0,0,0]
sysParams.fbJesdTxSyncMux			= [0,0]
sysParams.jesdRxSyncMux				= [0,0,0,0]		#[0,0,1,1]
sysParams.syncLoopBack				= True

# ## The following parameters sets up the AGC
# sysParams.agcParams[0].agcMode = 1 ##internal AGC
# sysParams.agcParams[0].gpioRstEnable = 0 ##disable GPIO based reset to AGC detector 
# sysParams.agcParams[0].atken = [0, 1, 0] ##enable big and small step attack
# sysParams.agcParams[0].decayen = [0,1,0] ##enable big and small step decay
# sysParams.agcParams[0].atksize = [2,1,0] ## bigs step = 2dB, small step = 1dB
# sysParams.agcParams[0].decaysize = [2,1,0] ##big step = 2dB, small step = 1dB
# sysParams.agcParams[0].atkthreshold = [-1, -2, -14] ##attack threshold
# sysParams.agcParams[0].decaythreshold = [-14, -6, -20] ##decay threshold
# sysParams.agcParams[0].atkwinlength = [170, 170] ## detector time constant expressed inn absolute time in ns. 
# sysParams.agcParams[0].decaywinlength = 87380 ##detector time constant expressed in absolute time in ns. All detectors use the same value for decay time constant
# sysParams.agcParams[0].atkNumHitsAbs = [8,8] ##absolute number of times signal crosses threshold. These crossing are with respect to the FADC/8 clock
# sysParams.agcParams[0].decayNumHitsAbs = [100,100] ##absolute number of times signal crosses threshold. These crossing are with respect to the FADC/8 clock
# sysParams.agcParams[0].minDsaAttn = 0 ##minimum DSA attenuation used by AGC
# sysParams.agcParams[0].maxDsaAttn = 22 ##maximum DSA attenuation used by AGC
# sysParams.agcParams[0].totalGainRange = 22 ##total gain range used by ALC for gain compensation
# sysParams.agcParams[0].minAttnAlc = 0 ##minimum attenuation used by ALC for compensation when useMinAttnAgc = 0
# sysParams.agcParams[0].useMinAttnAgc = 1 ##enable ALC to use minimum attenuation from AGC for which compensation is required.
# sysParams.agcParams[0].alcEn = 1
# sysParams.agcParams[0].alcMode = 0 ##floating point DGC
# sysParams.agcParams[0].fltPtMode = 0 ##if exponent > 0, dont send MSB
# sysParams.agcParams[0].fltPtFmt = 1 ##3 bit exponent


## The following parameters sets up the GPIOs
sysParams.gpioMapping={
		'H8': 'ADC_SYNC0',
		'H7': 'ADC_SYNC1',
		'N8': 'ADC_SYNC2',
		'N7': 'ADC_SYNC3',
		'H9': 'DAC_SYNC0',
		'G9': 'DAC_SYNC1',
		'N9': 'DAC_SYNC2',
		'P9': 'DAC_SYNC3',
		'P14': 'GLOBAL_PDN',
		'K14': 'FBABTDD',
		'R6': 'FBCDTDD',
		'H15': ['TXATDD','TXBTDD'],
		'V5': ['TXCTDD','TXDTDD'],
		'E7': ['RXATDD','RXBTDD'],
		'R15': ['RXCTDD','RXDTDD']}
		
#AFE.systemParams.papParams[0]['enable'] = True
#AFE.systemParams.papParams[1]['enable'] = True
#AFE.systemParams.papParams[2]['enable'] = True
#AFE.systemParams.papParams[3]['enable'] = True
		

## Initiates LMK04828 and AFE79xx Bring-up
AFE.deviceBringup()

AFE.TOP.overrideTdd(15,3,15)