This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] AFE7900EVM:AFE7900EVM 中继器模式、无法看到输出

Guru**** 2770975 points

Other Parts Discussed in Thread: AFE7900EVM

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/rf-microwave-group/rf-microwave/f/rf-microwave-forum/1217686/afe7900evm-afe7900evm-repeater-mode-can-not-see-the-output

器件型号:AFE7900EVM

提前感谢您的帮助。

我使用 AFE7900EVM 的中继器模式、以800MHz 输入单信号到 RXA、成功运行代码、但在 TXA 输出端未接收到任何信号(仅噪声)、

为什么选择?

1,我运行安装和 devlnit

2.运行代码清理(与 AFE79XX EVM 模式5几乎相同)

下面是我的代码和日志。

'''
setupParams.skipFpga 				= 1
sysParams							= AFE.systemParams
sysParams.externalClockTx			= False
sysParams.externalClockRx			= False


setupParams.fpgaRefClk 				= 245.76
AFE.systemStatus.loadTrims			= 1

sysParams.FRef                    	= 491.52
sysParams.FadcRx                  	= 1474.56
sysParams.FadcFb				  	= 1474.56
sysParams.Fdac                    	= 1474.56*3

sysParams.enableDacInterleavedMode	= False 					#DAC interleave mode to save power consumption. Fs/2 - Fin spur occurs

sysParams.modeTdd 					= 0		
										# 0- Single TDD Pin for all Channels
										# 1- Separate Control for 2T/2R/1F
										# 2- Separate Control for 1T/1R/1F	
enableAdcDacSync					= True										
sysParams.topLevelSystemMode		= 'StaticTDDMode'
sysParams.RRFMode 					= 0  #4T4R2F FDD mode
sysParams.jesdSystemMode			= [1,1]
										#SystemMode 0:	2R1F-FDD						; rx1-rx2-fb-fb
										#SystemMode 1:	1R1F-FDD						; rx1-rx1-fb-fb
										#SystemMode 2:	2R-FDD							; rx1-rx1-rx2-rx2
										#SystemMode 3:	1R								; rx1-rx1-rx1-rx1
										#SystemMode 4:	1F								; fb-fb-fb-fb
										#SystemMode 5:	1R1F-TDD						; rx1/fb-rx1/fb-rx1/fb-rx1/fb
										#SystemMode 8:	1R1F-TDD 1R-FDD	(FB-2Lanes)(RX1 RX2 interchanged)		; rx2/fb-rx2/fb-rx1-rx1

sysParams.jesdLoopbackEn			= 1 	#Make it 1 to Enable the JESDTX to JESDRX internal loopback
sysParams.LMFSHdRx                	= ['24410', '24410', '24410', '24410']	#14810
										# The 2nd and 4th are valid only for jesdSystemMode values in (2,6,7,8). For other modes, select 4 converter modes for 1st and 3rd.
sysParams.LMFSHdFb                	= ["24410","24410"]
sysParams.LMFSHdTx                	= ["24410","24410","24410","24410"]

sysParams.jesdTxProtocol            = [0,0]
sysParams.jesdRxProtocol            = [0,0]
sysParams.serdesFirmware			= True 		# If you want to lead any firmware, please speify the path here. Otherwise it will not write any firmware
sysParams.jesdTxLaneMux				= [0,1,2,3,4,5,6,7]
												# Enter which lanes you want in each location. 
												# Note that across 2T Mux is not possible in 0.5.
												# For example, if you want to exchange the first two lines of each 2T, this should be [[1,0,2,3],[5,4,6,7]]
sysParams.jesdRxLaneMux				= [0,1,2,3,4,5,6,7]
												# Enter which lanes you want in each location. [0,1,4,5,2,3,6,7].
												# Note that across 2R Mux is not possible in 0.5.
												# For example, if you want to exchange the first two lines of each 2R, this should be [[1,0,2,3],[5,4,6,7]]
												
sysParams.jesdRxRbd					= [4, 4]

sysParams.rxJesdTxScr				= [False,False,False,False]
sysParams.fbJesdTxScr				= [False,False]
sysParams.jesdRxScr					= [False,False,False,False]

sysParams.rxJesdTxK					= [16,16,16,16]
sysParams.fbJesdTxK					= [16,16]
sysParams.jesdRxK					= [16,16,16,16]

sysParams.ncoFreqMode 				= "1KHz"
	
sysParams.txNco0					= 	[[797,797],		#Band0, Band1 for TxA for NCO0[1747,2600],[2047,2600]
										[797,797],        #Band0, Band1 for TxB for NCO0
										[797,797],        #Band0, Band1 for TxC for NCO0
										[797,797] ]        #Band0, Band1 for TxD for NCO0

sysParams.rxNco0					= 	[[797,797],		#Band0, Band1 for RxA for NCO0
										[797,797],        #Band0, Band1 for RxB for NCO0
										[797,797],        #Band0, Band1 for RxC for NCO0
										[797,797] ]       #Band0, Band1 for RxD for NCO0

sysParams.fbNco0					= 	[797,797]		#FBA, FBC for NCO0
sysParams.fbNco1					= 	[797,797]		#FBA, FBC for NCO1
sysParams.fbNco2					= 	[797,797]			#FBA, FBC for NCO2
sysParams.fbNco3					= 	[797,797]	#FBA, FBC for NCO3



sysParams.numBandsRx				= [0]*4					# 0 for single, 1 for dual
sysParams.numBandsFb				= [0,0]				
sysParams.numBandsTx				= [0,0,0,0]


sysParams.ddcFactorRx             	= [6,6,6,6]
sysParams.ddcFactorFb             	= [6,6]
sysParams.ducFactorTx             	= [18,18,18,18]

AFE.systemStatus.loadTrims			=1

## The following parameters sets up the register and macro dumps
logDumpInst.setFileName(ASTERIX_DIR+DEVICES_DIR+r"\Afe79xxPg1.txt")
logDumpInst.logFormat				= 0x0f
logDumpInst.rewriteFile				= 1
logDumpInst.rewriteFileFormat4		= 1
device.optimizeWrites				= 0
device.rawWriteLogEn			    = 1
## The following parameters sets up the LMK04828 clocking schemes
lmkParams.pllEn						=	True#False
lmkParams.inputClk					=	1474.56#737.28
lmkParams.sysrefFreq				=	3.84
lmkParams.lmkFrefClk				=	True
	
## The following parameters sets up the SYNCIN and SYNCOUT to interface with the TSW14J57
sysParams.jesdABLvdsSync			= 1
sysParams.jesdCDLvdsSync			= 1
sysParams.rxJesdTxSyncMux			= [0,0,0,0]
sysParams.fbJesdTxSyncMux			= [1,1]
sysParams.jesdRxSyncMux				= [0,0,0,0]		#[0,0,1,1]
sysParams.syncLoopBack				= False

# ## The following parameters sets up the AGC
# sysParams.agcParams[0].agcMode = 1 ##internal AGC
# sysParams.agcParams[0].gpioRstEnable = 0 ##disable GPIO based reset to AGC detector 
# sysParams.agcParams[0].atken = [0, 1, 0] ##enable big and small step attack
# sysParams.agcParams[0].decayen = [0,1,0] ##enable big and small step decay
# sysParams.agcParams[0].atksize = [2,1,0] ## bigs step = 2dB, small step = 1dB
# sysParams.agcParams[0].decaysize = [2,1,0] ##big step = 2dB, small step = 1dB
# sysParams.agcParams[0].atkthreshold = [-1, -2, -14] ##attack threshold
# sysParams.agcParams[0].decaythreshold = [-14, -6, -20] ##decay threshold
# sysParams.agcParams[0].atkwinlength = [170, 170] ## detector time constant expressed inn absolute time in ns. 
# sysParams.agcParams[0].decaywinlength = 87380 ##detector time constant expressed in absolute time in ns. All detectors use the same value for decay time constant
# sysParams.agcParams[0].atkNumHitsAbs = [8,8] ##absolute number of times signal crosses threshold. These crossing are with respect to the FADC/8 clock
# sysParams.agcParams[0].decayNumHitsAbs = [100,100] ##absolute number of times signal crosses threshold. These crossing are with respect to the FADC/8 clock
# sysParams.agcParams[0].minDsaAttn = 0 ##minimum DSA attenuation used by AGC
# sysParams.agcParams[0].maxDsaAttn = 22 ##maximum DSA attenuation used by AGC
# sysParams.agcParams[0].totalGainRange = 22 ##total gain range used by ALC for gain compensation
# sysParams.agcParams[0].minAttnAlc = 0 ##minimum attenuation used by ALC for compensation when useMinAttnAgc = 0
# sysParams.agcParams[0].useMinAttnAgc = 1 ##enable ALC to use minimum attenuation from AGC for which compensation is required.
# sysParams.agcParams[0].alcEn = 1
# sysParams.agcParams[0].alcMode = 0 ##floating point DGC
# sysParams.agcParams[0].fltPtMode = 0 ##if exponent > 0, dont send MSB
# sysParams.agcParams[0].fltPtFmt = 1 ##3 bit exponent


## The following parameters sets up the GPIOs
sysParams.gpioMapping={
		'H8': 'ADC_SYNC0',
		'H7': 'ADC_SYNC1',
		'N8': 'ADC_SYNC2',
		'N7': 'ADC_SYNC3',
		'H9': 'DAC_SYNC0',
		'G9': 'DAC_SYNC1',
		'N9': 'DAC_SYNC2',
		'P9': 'DAC_SYNC3',
		'P14': 'GLOBAL_PDN',
		'K14': 'FBABTDD',
		'R6': 'FBCDTDD',
		'H15': ['TXATDD','TXBTDD'],
		'V5': ['TXCTDD','TXDTDD'],
		'E7': ['RXATDD','RXBTDD'],
		'R15': ['RXCTDD','RXDTDD']}
## Initiates LMK04828 and AFE79xx Bring-up
setupParams.skipLmk	=	False

AFE.deviceBringup()

AFE.TOP.overrideTdd(15,3,15)
#AFE.adcDacSync()
#AFE.LMK.lmkSysrefEn(1)
#AFE.LMK.lmkSysrefEn(0)
#AFE.JESD.SUBCHIP.toggleSync()

#======
#Executing .. AFE79xx/bringup/AFE79xx_EVM_Mode5.py
#Start Time 2023-04-18 16:26:35.280000 
The External Sysref Frequency should be an integer factor of: 3.84MHz
2T2R1F Number: 0
Valid Configuration: True
laneRateRx: 9830.4
laneRateFb: 9830.4
laneRateTx: 9830.4
2T2R1F Number: 1
Valid Configuration: True
laneRateRx: 9830.4
laneRateFb: 9830.4
laneRateTx: 9830.4
Device Initialization for ChipVersion: 2.0
LMK Clock Divider - Device registers reset.
LMK Clock Divider - Device registers reset.
REFCLOCK is used from LMK source, ensure board connections are ok to do the same
DONOT_OPEN_Atharv_FULL - Device registers reset.
chipType: 0xa
chipId: 0x78
chipVersion: 0x20
SPIA has got control of PLL pages
PLL Pages SPI control relinquished.
Fuse farm load autoload done successful
No autload error
Fuse farm load autoload done successful
No autload error
SPIA has got control of PLL pages
PLL Locked
PLL Pages SPI control relinquished.
SPIA has got control of PLL pages
PLL Pages SPI control relinquished.
SPIA has got control of PLL pages
PLL Pages SPI control relinquished.
SPIA has got control of PLL pages
PLL Pages SPI control relinquished.
Sysref Read as expected
###########Device DAC JESD-RX 0 Link Status###########
CS State TX0: 0b00001010 . It is expected to be 0b00001010
FS State TX0: 0b00000101 . It is expected to be 0b00000101
Could get the link up for device RX: 0
###################################
###########Device DAC JESD-RX 1 Link Status###########
CS State TX0: 0b00001010 . It is expected to be 0b00001010
FS State TX0: 0b00000101 . It is expected to be 0b00000101
Could get the link up for device RX: 1
###################################
#Done executing .. AFE79xx/bringup/AFE79xx_EVM_Mode5.py
#End Time 2023-04-18 16:28:14.793000
#Execution Time = 99.5130000114 s 
#================ ERRORS:0, WARNINGS:1 ================#

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    抱歉,我复制了上面的错误代码,我使用的代码是 blow。

    setupParams.skipFpga 				= 1
    sysParams							= AFE.systemParams
    sysParams.externalClockTx			= False
    sysParams.externalClockRx			= False
    
    
    setupParams.fpgaRefClk 				= 245.76
    AFE.systemStatus.loadTrims			= 1
    
    sysParams.FRef                    	= 491.52
    sysParams.FadcRx                  	= 1474.56
    sysParams.FadcFb				  	= 1474.56
    sysParams.Fdac                    	= 1474.56*3
    
    sysParams.enableDacInterleavedMode	= False 					#DAC interleave mode to save power consumption. Fs/2 - Fin spur occurs
    
    sysParams.modeTdd 					= 0		
    										# 0- Single TDD Pin for all Channels
    										# 1- Separate Control for 2T/2R/1F
    										# 2- Separate Control for 1T/1R/1F										
    sysParams.topLevelSystemMode		= 'StaticTDDMode'
    sysParams.RRFMode 					= 0  #4T4R2F FDD mode
    sysParams.jesdSystemMode			= [1,1]
    										#SystemMode 0:	2R1F-FDD						; rx1-rx2-fb-fb
    										#SystemMode 1:	1R1F-FDD						; rx1-rx1-fb-fb
    										#SystemMode 2:	2R-FDD							; rx1-rx1-rx2-rx2
    										#SystemMode 3:	1R								; rx1-rx1-rx1-rx1
    										#SystemMode 4:	1F								; fb-fb-fb-fb
    										#SystemMode 5:	1R1F-TDD						; rx1/fb-rx1/fb-rx1/fb-rx1/fb
    										#SystemMode 8:	1R1F-TDD 1R-FDD	(FB-2Lanes)(RX1 RX2 interchanged)		; rx2/fb-rx2/fb-rx1-rx1
    
    sysParams.jesdLoopbackEn			= 1 	#Make it 1 to Enable the JESDTX to JESDRX internal loopback
    sysParams.LMFSHdRx                	= ['24410', '24410', '24410', '24410']	#14810
    										# The 2nd and 4th are valid only for jesdSystemMode values in (2,6,7,8). For other modes, select 4 converter modes for 1st and 3rd.
    sysParams.LMFSHdFb                	= ["24410","24410"]
    sysParams.LMFSHdTx                	= ["24410","24410","24410","24410"]
    
    sysParams.jesdTxProtocol            = [0,0]
    sysParams.jesdRxProtocol            = [0,0]
    sysParams.serdesFirmware			= True 		# If you want to lead any firmware, please speify the path here. Otherwise it will not write any firmware
    sysParams.jesdTxLaneMux				= [0,1,2,3,4,5,6,7]
    												# Enter which lanes you want in each location. 
    												# Note that across 2T Mux is not possible in 0.5.
    												# For example, if you want to exchange the first two lines of each 2T, this should be [[1,0,2,3],[5,4,6,7]]
    sysParams.jesdRxLaneMux				= [0,1,2,3,4,5,6,7]
    												# Enter which lanes you want in each location. [0,1,4,5,2,3,6,7].
    												# Note that across 2R Mux is not possible in 0.5.
    												# For example, if you want to exchange the first two lines of each 2R, this should be [[1,0,2,3],[5,4,6,7]]
    												
    sysParams.jesdRxRbd					= [4, 4]
    
    sysParams.rxJesdTxScr				= [False,False,False,False]
    sysParams.fbJesdTxScr				= [False,False]
    sysParams.jesdRxScr					= [False,False,False,False]
    
    sysParams.rxJesdTxK					= [16,16,16,16]
    sysParams.fbJesdTxK					= [16,16]
    sysParams.jesdRxK					= [16,16,16,16]
    
    sysParams.ncoFreqMode 				= "1KHz"
    	
    sysParams.txNco0					= 	[[797,797],		#Band0, Band1 for TxA for NCO0[1747,2600],[2047,2600]
    										[797,797],        #Band0, Band1 for TxB for NCO0
    										[797,797],        #Band0, Band1 for TxC for NCO0
    										[797,797] ]        #Band0, Band1 for TxD for NCO0
    
    sysParams.rxNco0					= 	[[797,797],		#Band0, Band1 for RxA for NCO0
    										[797,797],        #Band0, Band1 for RxB for NCO0
    										[797,797],        #Band0, Band1 for RxC for NCO0
    										[797,797] ]       #Band0, Band1 for RxD for NCO0
    
    sysParams.fbNco0					= 	[797,797]		#FBA, FBC for NCO0
    sysParams.fbNco1					= 	[797,797]		#FBA, FBC for NCO1
    sysParams.fbNco2					= 	[797,797]			#FBA, FBC for NCO2
    sysParams.fbNco3					= 	[797,797]	#FBA, FBC for NCO3
    
    
    
    sysParams.numBandsRx				= [0]*4					# 0 for single, 1 for dual
    sysParams.numBandsFb				= [0,0]				
    sysParams.numBandsTx				= [0,0,0,0]
    
    
    sysParams.ddcFactorRx             	= [6,6,6,6]
    sysParams.ddcFactorFb             	= [6,6]
    sysParams.ducFactorTx             	= [18,18,18,18]
    
    AFE.systemStatus.loadTrims			=1
    
    ## The following parameters sets up the register and macro dumps
    logDumpInst.setFileName(ASTERIX_DIR+DEVICES_DIR+r"\Afe79xxPg1.txt")
    logDumpInst.logFormat				= 0x0f
    logDumpInst.rewriteFile				= 1
    logDumpInst.rewriteFileFormat4		= 1
    device.optimizeWrites				= 0
    device.rawWriteLogEn			    = 1
    ## The following parameters sets up the LMK04828 clocking schemes
    lmkParams.pllEn						=	True#False
    lmkParams.inputClk					=	1474.56#737.28
    lmkParams.sysrefFreq				=	3.84
    lmkParams.lmkFrefClk				=	True
    	
    ## The following parameters sets up the SYNCIN and SYNCOUT to interface with the TSW14J57
    sysParams.jesdABLvdsSync			= 1
    sysParams.jesdCDLvdsSync			= 1
    sysParams.rxJesdTxSyncMux			= [0,0,0,0]
    sysParams.fbJesdTxSyncMux			= [0,0]
    sysParams.jesdRxSyncMux				= [0,0,0,0]		#[0,0,1,1]
    sysParams.syncLoopBack				= False
    
    # ## The following parameters sets up the AGC
    # sysParams.agcParams[0].agcMode = 1 ##internal AGC
    # sysParams.agcParams[0].gpioRstEnable = 0 ##disable GPIO based reset to AGC detector 
    # sysParams.agcParams[0].atken = [0, 1, 0] ##enable big and small step attack
    # sysParams.agcParams[0].decayen = [0,1,0] ##enable big and small step decay
    # sysParams.agcParams[0].atksize = [2,1,0] ## bigs step = 2dB, small step = 1dB
    # sysParams.agcParams[0].decaysize = [2,1,0] ##big step = 2dB, small step = 1dB
    # sysParams.agcParams[0].atkthreshold = [-1, -2, -14] ##attack threshold
    # sysParams.agcParams[0].decaythreshold = [-14, -6, -20] ##decay threshold
    # sysParams.agcParams[0].atkwinlength = [170, 170] ## detector time constant expressed inn absolute time in ns. 
    # sysParams.agcParams[0].decaywinlength = 87380 ##detector time constant expressed in absolute time in ns. All detectors use the same value for decay time constant
    # sysParams.agcParams[0].atkNumHitsAbs = [8,8] ##absolute number of times signal crosses threshold. These crossing are with respect to the FADC/8 clock
    # sysParams.agcParams[0].decayNumHitsAbs = [100,100] ##absolute number of times signal crosses threshold. These crossing are with respect to the FADC/8 clock
    # sysParams.agcParams[0].minDsaAttn = 0 ##minimum DSA attenuation used by AGC
    # sysParams.agcParams[0].maxDsaAttn = 22 ##maximum DSA attenuation used by AGC
    # sysParams.agcParams[0].totalGainRange = 22 ##total gain range used by ALC for gain compensation
    # sysParams.agcParams[0].minAttnAlc = 0 ##minimum attenuation used by ALC for compensation when useMinAttnAgc = 0
    # sysParams.agcParams[0].useMinAttnAgc = 1 ##enable ALC to use minimum attenuation from AGC for which compensation is required.
    # sysParams.agcParams[0].alcEn = 1
    # sysParams.agcParams[0].alcMode = 0 ##floating point DGC
    # sysParams.agcParams[0].fltPtMode = 0 ##if exponent > 0, dont send MSB
    # sysParams.agcParams[0].fltPtFmt = 1 ##3 bit exponent
    
    
    ## The following parameters sets up the GPIOs
    sysParams.gpioMapping={
    		'H8': 'ADC_SYNC0',
    		'H7': 'ADC_SYNC1',
    		'N8': 'ADC_SYNC2',
    		'N7': 'ADC_SYNC3',
    		'H9': 'DAC_SYNC0',
    		'G9': 'DAC_SYNC1',
    		'N9': 'DAC_SYNC2',
    		'P9': 'DAC_SYNC3',
    		'P14': 'GLOBAL_PDN',
    		'K14': 'FBABTDD',
    		'R6': 'FBCDTDD',
    		'H15': ['TXATDD','TXBTDD'],
    		'V5': ['TXCTDD','TXDTDD'],
    		'E7': ['RXATDD','RXBTDD'],
    		'R15': ['RXCTDD','RXDTDD']}
    ## Initiates LMK04828 and AFE79xx Bring-up
    setupParams.skipLmk	=	False
    
    AFE.deviceBringup()
    
    AFE.TOP.overrideTdd(15,3,15)
    #AFE.adcDacSync()
    #AFE.LMK.lmkSysrefEn(1)
    #AFE.LMK.lmkSysrefEn(0)
    #AFE.JESD.SUBCHIP.toggleSync()

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    我对 RXD 执行了相同的操作并获得了输出、但有两个额外的杂波、但 FREQ-DCC-FILTER-CALC 工具中没有杂波

    那么我有几个问题(1)为什么您不能在 TX1中做同样的事情并获得信号

                          (2)其他杂波的原因

                          (3)为何信号只存在一段时间后消失

    期待您的 回复

    你好

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好、Wang、

    Tx1的问题是 Tx1和 Rx1的输入/输出网络匹配5.4GHz、这两个通道上的平衡-非平衡变压器仅下降4.7GHz。 这意味着要获得800MHz 信号、您需要将信号驱动得远高于其他通道才能获得输出。 请尝试提高 Rx1通道的输入功率。  

    对于您看到的第二个问题、这可能是由于对 Tx 通道进行过驱导致的更多杂散。 您能否尝试降低 ADC 输入功率、看看 DAC 输出是否看起来更好?

    此致、

    David Chaparro

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    你(们)好

    我会尝试它。

    你好