This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] AFE7950EVM:将 AFE7950EVM 与 TSW14J57EVM 配合使用时、存在一些没有任何射频输入的杂散

Guru**** 2914580 points

Other Parts Discussed in Thread: TSW14J57EVM, AFE7950EVM

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/rf-microwave-group/rf-microwave/f/rf-microwave-forum/1227430/afe7950evm-there-are-some-spurs-without-any-rf-input-when-using-the-afe7950evm-with-tsw14j57evm

器件型号:AFE7950EVM
主题中讨论的其他器件:TSW14J57EVM

您好、TI 团队、

在将 AFE7950EVM 与 TSW14J57EVM 搭配使用时、存在一些没有任何射频输入的杂散

所有输入端接。

我只使用4RX ( FPGA 固件:AFE79xx_2x2RX_24410 )

下图是 HSDC Pro 中的 ADC 输出  

RxA(很好)

RxB(69MHz 和21MHz )

RXC (113MHz)

RXD (-53MHz)

Latte 启动文件(OnboardClk_RX_250m)

##############		Read me			##############
#In HSDC Pro DAC tab, Select AFE79xx_2x2TX_44210; Data Rate = 491.52M
#In HSDC Pro ADC tab, Select AFE79xx_2x2RX_24410; Data Rate = 245.76M ---> To capture 4 RX channels
#In HSDC Pro ADC tab, Select AFE79xx_1x2FB_44210; Data Rate = 491.52M ---> To capture 2 FB channels

sysParams=AFE.systemParams
sysParams.__init__();sysParams.chipVersion=chipVersion

setupParams.skipFpga = 1 # setup FPGA (TSW14J56) using HSDC Pro 

##############		Top Level			##############
sysParams.FRef			= 491.52
sysParams.FadcRx		= 2949.12
sysParams.FadcFb		= 2949.12
sysParams.Fdac			= 2949.12*4
sysParams.externalClockRx=False
sysParams.externalClockTx=False
													
##############		Digital Chain		##############

		#####	RX	#####
sysParams.ddcFactorRx	=	[12,12,12,12]			#DDC decimation factor for RX A, B, C and D
sysParams.rxNco0		= 	[[4600,4600],			#Band0, Band1 for RXA 
							[4600,4600],        	#Band0, Band1 for RXB 
							[4600,4600],        	#Band0, Band1 for RXC 
							[4600,4600]]        	#Band0, Band1 for RXD 

		#####	FB	#####
sysParams.ddcFactorFb	=	[6,6]					#DDC decimation factor for FB 1 and 2
sysParams.fbNco0		= 	[4600,4600]				#Band0 for FB1 and FB2 

		#####	TX	#####
sysParams.ducFactorTx	=	[24,24,24,24]			#DUC interpolation factor for TX A, B, C and D
sysParams.txNco0		= 	[[4600,4600],			#Band0, Band1 for TXA 
							[4600,4600],        	#Band0, Band1 for TXB 
							[4600,4600],        	#Band0, Band1 for TXC 
							[4600,4600]]        	#Band0, Band1 for TXD


##############		JESD		##############

		#####	ADC-JESD	#####
sysParams.jesdSystemMode= [1,1]
													#SystemMode 0:	2R1F-FDD						; rx1-rx2-fb -fb
													#SystemMode 1:	1R1F-FDD						; rx -rx -fb -fb
													#SystemMode 2:	2R-FDD							; rx1-rx1-rx2-rx2
													#SystemMode 3:	1R								; rx -rx -rx -rx
													#SystemMode 4:	1F								; fb -fb- fb -fb
													#SystemMode 5:	1R1F-TDD						; rx/fb-rx/fb-rx/fb-rx/fb
													
sysParams.jesdTxProtocol= [0,0]						# 0 - 8b/10b encoding; 2 - 64b/66b encoding 
sysParams.LMFSHdRx		= ["24410","24410","24410","24410"]
													# The 2nd and 4th are valid only for jesdSystemMode values in (0,2).
													# For other modes, select 4 converter modes for 1st and 3rd.
sysParams.LMFSHdFb		= ["22210","22210"]

sysParams.rxJesdTxScr	= [True,True,True,True]
sysParams.fbJesdTxScr	= [True,True]

sysParams.rxJesdTxK		= [16,16,16,16]
sysParams.fbJesdTxK		= [16,16]

sysParams.jesdTxLaneMux	= [0,1,2,3,4,5,6,7]			# Enter which lanes you want in each location. 
													# For example, if you want to exchange the first two lines of each 2T,
													#		this should be [[1,0,2,3],[5,4,6,7]]

		#####	DAC-JESD	#####
sysParams.jesdRxProtocol= [0,0]
sysParams.LMFSHdTx		= ["44210","44210","44210","44210"]
sysParams.jesdRxLaneMux	= [0,1,2,3,4,5,6,7]			# Enter which lanes you want in each location.
													# For example, if you want to exchange the first two lines of each 2R
													#		this should be [[1,0,2,3],[5,4,6,7]]
sysParams.jesdRxRbd		= [4, 4]
sysParams.jesdRxScr		= [True,True,True,True]
sysParams.jesdRxK		= [16,16,16,16]

		#####	JESD Common	#####
	
sysParams.jesdABLvdsSync= True
sysParams.jesdCDLvdsSync= True
sysParams.syncLoopBack	= True	#JESD Sync signal is connected to FPGA

##############		GPIO		##############
sysParams.gpioMapping	= {
						'H8': 'ADC_SYNC0',
						'H7': 'ADC_SYNC1',
						'N8': 'ADC_SYNC2',
						'N7': 'ADC_SYNC3',
						'H9': 'DAC_SYNC0',
						'G9': 'DAC_SYNC1',
						'N9': 'DAC_SYNC2',
						'P9': 'DAC_SYNC3',
						'P14': 'GLOBAL_PDN',
						'K14': 'FBABTDD',
						'R6': 'FBCDTDD',
						'H15': ['TXATDD','TXBTDD'],
						'V5': ['TXCTDD','TXDTDD'],
						'E7': ['RXATDD','RXBTDD'],
						'R15': ['RXCTDD','RXDTDD']}

##############		LMK Params		##############
lmkParams.pllEn			= True
lmkParams.inputClk		= 983.04 # Valid only when lmkParams.pllEn = False
lmkParams.lmkFrefClk	= True
setupParams.fpgaRefClk	= 245.76 # Should be equal to LaneRate/40 for TSW14J56

##############		Logging		##############
logDumpInst.setFileName(ASTERIX_DIR+DEVICES_DIR+r"\Afe79xxPg1.txt")
logDumpInst.logFormat=0x1 #Modify to 0x1 to save register scequence to log file. Script takes more time to execute.
logDumpInst.rewriteFile=1
logDumpInst.rewriteFileFormat4=1
device.optimizeWrites=0
device.rawWriteLogEn=1

device.delay_time = 0
#-------------------------------------------------------------------------------------------------#
setupParams.skipLmk	=	False
AFE.initializeConfig()
lmkParams.sysrefFreq = AFE.systemStatus.sysrefFreq
lmkParams.lmkPulseSysrefMode = False
AFE.LMK.lmkConfig()

## Initiates AFE79xx Bring-up
setupParams.skipLmk	=	True
sysParams.txEnable = [False,False,False,False] 
AFE.deviceBringup()

AFE.TOP.overrideTdd(15,3,15)

如何 消除这些杂散?

谢谢~

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    我发现,杂散在 RXB ( 69.439MHz )和杂散在 RXD (-53.441MHz )

    69.439 - 122.88 =-53.441

    它们之间似乎有一些数学关系。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    张乃文先生,

    由于来自内部分频时钟速率的耦合、在小于-90dBFS 的水平下会有一些杂散。 例如、在与 NCO 频率混频之前、复数 FFT 中69.44MHz 的 RxB 杂散为4600+69.44= 4669.44MHz。 在第一个奈奎斯特区域中、该频率混叠到1228.8MHz (2 * 2949.12 - 4669.44 = 1228.8)。 此速率等于 SERDES 通道速率(9830.4Mbps) 8分频。  

    在一些窄带用例中、 可以计划将这些杂散置于带外频率。 但如果无法实现、 在设计用户系统时应考虑约-90dBFS 的动态范围。   在使用相同时钟频率时无法消除这些杂散。  

    此致、

    维贾伊

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    非常感谢~