This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] AFE7950EVM:使用外部时钟进行采样时基本消失

Guru**** 2813875 points

Other Parts Discussed in Thread: AFE7950

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/rf-microwave-group/rf-microwave/f/rf-microwave-forum/1236500/afe7950evm-fundamental-disappear-when-use-the-external-clock-to-sample

器件型号:AFE7950EVM
主题中讨论的其他器件:AFE7950

尊敬的 TI:

我使用外部时钟来避免来自 AFE7950内部 PLL 的相位噪声

当输入 RX 等于 NCO 频率时、HSDC pro 中显示的信号将消失

NCO = 4840MHz 和输入 RX = 4850MHz (正常)

NCO = 4840MHz 且输入 RX = 4840MHz (异常)

这种 现象的原因是什么?

Latte 脚本

sysParams=AFE.systemParams
sysParams.__init__();sysParams.chipVersion=chipVersion

setupParams.skipFpga = 1 # setup FPGA (TSW14J56) using HSDC Pro 

##############		Top Level			##############
sysParams.FRef			= 3000*4
sysParams.FadcRx		= 3000
sysParams.FadcFb		= 3000
sysParams.Fdac			= 3000*4
sysParams.externalClockRx = True
sysParams.externalClockTx = True
													
##############		Digital Chain		##############

		#####	RX	#####
sysParams.ddcFactorRx	=	[24,24,24,24]			#DDC decimation factor for RX A, B, C and D
sysParams.rxNco0		= 	[[4840,4840],			#Band0, Band1 for RXA 
							[4840,4840],        	#Band0, Band1 for RXB 
							[4840,4840],        	#Band0, Band1 for RXC 
							[4840,4840]]        	#Band0, Band1 for RXD 

		#####	FB	#####
sysParams.ddcFactorFb	=	[24,24]					#DDC decimation factor for FB 1 and 2
sysParams.fbNco0		= 	[4840,4840]				#Band0 for FB1 and FB2 

		#####	TX	#####
sysParams.ducFactorTx	=	[24,24,24,24]			#DUC interpolation factor for TX A, B, C and D
sysParams.txNco0		= 	[[4840,4840],			#Band0, Band1 for TXA 
							[4840,4840],        	#Band0, Band1 for TXB 
							[4840,4840],        	#Band0, Band1 for TXC 
							[4840,4840]]        	#Band0, Band1 for TXD
sysParams.txEnable = [False,False,False,False]

##############		JESD		##############

		#####	ADC-JESD	#####
sysParams.jesdSystemMode= [1,1]
													#SystemMode 0:	2R1F-FDD						; rx1-rx2-fb -fb
													#SystemMode 1:	1R1F-FDD						; rx -rx -fb -fb
													#SystemMode 2:	2R-FDD							; rx1-rx1-rx2-rx2
													#SystemMode 3:	1R								; rx -rx -rx -rx
													#SystemMode 4:	1F								; fb -fb- fb -fb
													#SystemMode 5:	1R1F-TDD						; rx/fb-rx/fb-rx/fb-rx/fb
													
sysParams.jesdTxProtocol= [0,0]						# 0 - 8b/10b encoding; 2 - 64b/66b encoding 
sysParams.LMFSHdRx		= ["24410","24410","24410","24410"]
													# The 2nd and 4th are valid only for jesdSystemMode values in (0,2).
													# For other modes, select 4 converter modes for 1st and 3rd.
sysParams.LMFSHdFb		= ["12410","12410"]

sysParams.rxJesdTxScr	= [True,True,True,True]
sysParams.fbJesdTxScr	= [True,True]

sysParams.rxJesdTxK		= [16,16,16,16]
sysParams.fbJesdTxK		= [16,16]

sysParams.jesdTxLaneMux	= [0,1,2,3,4,5,6,7]			# Enter which lanes you want in each location. 
													# For example, if you want to exchange the first two lines of each 2T,
													#		this should be [[1,0,2,3],[5,4,6,7]]

		#####	DAC-JESD	#####
sysParams.jesdRxProtocol= [0,0]
sysParams.LMFSHdTx		= ["44210","44210","44210","44210"]
sysParams.jesdRxLaneMux	= [0,1,2,3,4,5,6,7]			# Enter which lanes you want in each location.
													# For example, if you want to exchange the first two lines of each 2R
													#		this should be [[1,0,2,3],[5,4,6,7]]
sysParams.jesdRxRbd		= [4, 4]
sysParams.jesdRxScr		= [True,True,True,True]
sysParams.jesdRxK		= [16,16,16,16]

		#####	JESD Common	#####
	
sysParams.jesdABLvdsSync= True
sysParams.jesdCDLvdsSync= True
sysParams.syncLoopBack	= True	#JESD Sync signal is connected to FPGA

##############		GPIO		##############
sysParams.gpioMapping	= {
						'H8': 'ADC_SYNC0',
						'H7': 'ADC_SYNC1',
						'N8': 'ADC_SYNC2',
						'N7': 'ADC_SYNC3',
						'H9': 'DAC_SYNC0',
						'G9': 'DAC_SYNC1',
						'N9': 'DAC_SYNC2',
						'P9': 'DAC_SYNC3',
						'P14': 'GLOBAL_PDN',
						'K14': 'FBABTDD',
						'R6': 'FBCDTDD',
						'H15': ['TXATDD','TXBTDD'],
						'V5': ['TXCTDD','TXDTDD'],
						'E7': ['RXATDD','RXBTDD'],
						'R15': ['RXCTDD','RXDTDD']}

##############		LMK Params		##############
lmkParams.pllEn			= False
lmkParams.inputClk		= 1500.0 # Valid only when lmkParams.pllEn = False
lmkParams.sysrefFreq    = 3000/1024
lmkParams.lmkFrefClk	= False
setupParams.fpgaRefClk	= 125 # Should be equal to LaneRate/40 for TSW14J56

##############		Logging		##############
logDumpInst.setFileName(ASTERIX_DIR+DEVICES_DIR+r"\Afe79xxPg1.txt")
logDumpInst.logFormat=0x0 #Modify to 0x1 to save register scequence to log file. Script takes more time to execute.
logDumpInst.rewriteFile=1
logDumpInst.rewriteFileFormat4=1
device.optimizeWrites=0
device.rawWriteLogEn=1

device.delay_time = 0
#-------------------------------------------------------------------------------------------------#
setupParams.skipLmk	=	False
AFE.initializeConfig()
lmkParams.sysrefFreq = AFE.systemStatus.sysrefFreq
lmkParams.lmkPulseSysrefMode = False
AFE.LMK.lmkConfig()
setupParams.skipLmk	=	True
## Initiates AFE79xx Bring-up

 
AFE.deviceBringup()

AFE.TOP.overrideTdd(15,3,15)

谢谢~

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    是否需要确定其他参数?  

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    你好,奈文,

    需要检查的一点是、您没有移除直流周围的箱。 要检查此项、您可以转到"Test Options">"陷波频率区间"、然后将直流后要删除的区间数量更改为0。 请尝试一下您的设置。

    此致、

    大卫·查帕罗