This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] AFE7950EVM:有关 AFE7950EVM 的 Latte 配置错误

Guru**** 2595805 points
Other Parts Discussed in Thread: AFE7950, AFE7950EVM

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/rf-microwave-group/rf-microwave/f/rf-microwave-forum/1241523/afe7950evm-latte-configuration-errors-about-the-afe7950evm

器件型号:AFE7950EVM
主题中讨论的其他器件:AFE7950

尊敬的 TI 工程师:

我曾尝试使用 TI 的 AFE7950EVM 板和 Xinlinx 的 ACU128 FPGA 来进行 ADC/DAC 处理。 但我失败了。 我认为可能有两个问题。 一个是 AFE7950的 Latte 配置。 我使用的 Latte 程序和 日志错误  在下面,我不知道如何处理的错误,因为它不工作后,我更改了 RBD 值. 我认为这与 FPGA 无关。 您能否在 AFE7950EVM 上试用此 Latte 程序、了解问题是什么、如何修改该程序才能正确运行?

 

sysParams.__init__();sysParams.chipVersion=chipVersion # Set sysParms to default
setupParams.skipFpga 				= 1
sysParams							=	AFE.systemParams

AFE.systemStatus.loadTrims			= 1
sysParams.fbEnable 					= [False]*2
sysParams.externalClockTx			= False
sysParams.externalClockRx			= False
sysParams.FRef                    	= 491.52
sysParams.FadcRx                  	= 2949.12
sysParams.FadcFb				  	= 2949.12
sysParams.Fdac                    	= 2949.12*4
sysParams.enableDacInterleavedMode	= False				#DAC interleave mode to save power consumption. Fs/2 - Fin spur occurs

sysParams.modeTdd 					= 0	                 
										# 0- Single TDD Pin for all Channels
										# 1- Separate Control for 2T/2R/1F
										# 2- Separate Control for 1T/1R/1F			

sysParams.RRFMode 					= 0   #4T4R2F FDD mode
sysParams.jesdSystemMode			= [3,3]            
										#SystemMode 0:	2R1F-FDD						; rx1-rx2-fb-fb
										#SystemMode 1:	1R1F-FDD						; rx1-rx1-fb-fb
										#SystemMode 2:	2R-FDD							; rx1-rx1-rx2-rx2
										#SystemMode 3:	1R								; rx1-rx1-rx1-rx1
										#SystemMode 4:	1F								; fb-fb-fb-fb
										#SystemMode 5:	1R1F-TDD						; rx1/fb-rx1/fb-rx1/fb-rx1/fb
										#SystemMode 8:	1R1F-TDD 1R-FDD	(FB-2Lanes)(RX1 RX2 interchanged)		; rx2/fb-rx2/fb-rx1-rx1
sysParams.jesdLoopbackEn			= 1 #Make it 1 to Enable the JESDTX to JESDRX internal loopback
sysParams.LMFSHdRx                	= ["44210","44210","44210","44210"]	
										# The 2nd and 4th are valid only for jesdSystemMode values in (2,6,7,8). For other modes, select 4 converter modes for 1st and 3rd.
sysParams.LMFSHdFb                	= ["22210","22210"]
sysParams.LMFSHdTx                	= ["44210","44210","44210","44210"]
sysParams.jesdTxProtocol            = [2,2]
sysParams.jesdRxProtocol            = [2,2]
sysParams.serdesFirmware			= True 		# If you want to lead any firmware, please speify the path here. Otherwise it will not write any firmware
sysParams.jesdTxLaneMux				= [0,1,2,3,4,5,6,7]	
												# Enter which lanes you want in each location. 
												# Note that across 2T Mux is not possible in 0.5.
												# For example, if you want to exchange the first two lines of each 2T, this should be [[1,0,2,3],[5,4,6,7]]
sysParams.serdesTxLanePolarity		= [False]*8
sysParams.jesdRxLaneMux				= [0,1,2,3,4,5,6,7]	#[0,1,2,3,4,5,7,6]
												# Enter which lanes you want in each location.
												# Note that across 2R Mux is not possible in 0.5.
												# For example, if you want to exchange the first two lines of each 2R, this should be [[1,0,2,3],[5,4,6,7]]
sysParams.serdesRxLanePolarity	= [False]*8
sysParams.jesdRxRbd					= [28,28]
sysParams.jesdTxRbd					= [28,28]
sysParams.rxJesdTxScr				= [False]*4
sysParams.fbJesdTxScr				= [False]*2
sysParams.jesdRxScr					= [False]*4

sysParams.rxJesdTxK					= [32]*4
sysParams.fbJesdTxK					= [32]*2
sysParams.jesdRxK					= [32]*4

sysParams.ncoFreqMode 				="1KHz" #"FCW" 

		#####	RX	#####
sysParams.ddcFactorRx	=	[6,6,6,6]			#DDC decimation factor for RX A, B, C and D
sysParams.rxNco0		= 	[[9500,9500],			#Band0, Band1 for RXA 
							[9500,9500],        	#Band0, Band1 for RXB 
							[9500,9500],        	#Band0, Band1 for RXC 
							[9500,9500]]       	    #Band0, Band1 for RXD  

		#####	TX	#####
sysParams.txEnable		=	[True,True,True,True]
sysParams.ducFactorTx	=	[24,24,24,24]			#DUC interpolation factor for TX A, B, C and D
sysParams.txNco0		= 	[[9500,9500],			#Band0, Band1 for TXA 
							[9500,9500],        	#Band0, Band1 for TXB 
							[9500,9500],        	#Band0, Band1 for TXC 
							[9500,9500]]        	#Band0, Band1 for TXD

sysParams.numBandsRx				= [0]*4					# 0 for single, 1 for dual
sysParams.numBandsFb				= [0,0]				
sysParams.numBandsTx				= [0]*4

## The following parameters sets up the LMK04828 clocking schemes
lmkParams.pllEn						=	True#False  #
lmkParams.inputClk					=	983.04   # Valid only when lmkParams.pllEn = False
lmkParams.lmkFrefClk				=	True
setupParams.fpgaRefClk 				=   122.88  # Should be equal to LaneRate/40

## The following parameters sets up the SYNCIN and SYNCOUT to interface with the TSW14J57
sysParams.jesdABLvdsSync			= True
sysParams.jesdCDLvdsSync			= True
sysParams.rxJesdTxSyncMux			= [0,0,0,0]
sysParams.fbJesdTxSyncMux			= [0,0]
sysParams.jesdRxSyncMux				= [0,0,0,0]		#[0,0,1,1]
sysParams.syncLoopBack				= True


sysParams.gpioMapping	= {
						'H8': 'ADC_SYNC0',
						'H7': 'ADC_SYNC1',
						'N8': 'DAC_SYNC0',
						'N7': 'DAC_SYNC1',
						'H9': 'ADC_SYNC2',
						'G9': 'ADC_SYNC3',
						'N9': 'DAC_SYNC2',
						'P9': 'DAC_SYNC3',
						'P14': 'GLOBAL_PDN',
						'K14': 'FBABTDD',
						'R6': 'FBCDTDD',
						'H15': ['TXATDD','TXBTDD'],
						'V5': ['TXCTDD','TXDTDD'],
						'E7': ['RXATDD','RXBTDD'],
						'R15': ['RXCTDD','RXDTDD']}
						
												
device.delay_time=0					

AFE.initializeConfig()
lmkParams.sysrefFreq = AFE.systemStatus.sysrefFreq
lmkParams.lmkPulseSysrefMode = False
AFE.LMK.lmkConfig()

AFE.TOP.sendSysref(1)
AFE.adcDacSync()  

setupParams.skipLmk	=	True
AFE.deviceBringup()
AFE.TOP.overrideTdd(15,3,15)

#======
#Executing .. AFE7950/bringup/script14.py
#Start Time 2023-06-26 10:05:26.988000 
The External Sysref Frequency should be an integer factor of: 1.28MHz
2T2R1F Number: 0
Valid Configuration: True
laneRateRx: 8110.08
laneRateFb: 8110.08
laneRateTx: 8110.08
2T2R1F Number: 1
Valid Configuration: True
laneRateRx: 8110.08
laneRateFb: 8110.08
laneRateTx: 8110.08
SPIA has got control of PLL pages
PLL Pages SPI control relinquished.
SPIA has got control of PLL pages
PLL Pages SPI control relinquished.
###########Device DAC JESD-RX 0 Link Status###########
lane0 Errors=0b10000; Got errors: elastic buffer overflow (bad RBD value); 
lane1 Errors=0b10000; Got errors: elastic buffer overflow (bad RBD value); 
lane2 Errors=0b10000; Got errors: elastic buffer overflow (bad RBD value); 
lane3 Errors=0b10000; Got errors: elastic buffer overflow (bad RBD value); 
CS State TX0: 0b10101010 . It is expected to be 0b10101010
BUF State TX0: 0b11111111 . It is expected to be 0b11111111
Couldn't get the link up for device RX: 0; Alarms: 0x1010101000000000L
###################################
###########Device DAC JESD-RX 1 Link Status###########
lane0 Errors=0b10000; Got errors: elastic buffer overflow (bad RBD value); 
lane1 Errors=0b10000; Got errors: elastic buffer overflow (bad RBD value); 
lane2 Errors=0b10000; Got errors: elastic buffer overflow (bad RBD value); 
lane3 Errors=0b10000; Got errors: elastic buffer overflow (bad RBD value); 
CS State TX0: 0b10101010 . It is expected to be 0b10101010
BUF State TX0: 0b11111111 . It is expected to be 0b11111111
Couldn't get the link up for device RX: 1; Alarms: 0x1010101000000000L
###################################
The External Sysref Frequency should be an integer factor of: 1.28MHz
2T2R1F Number: 0
Valid Configuration: True
laneRateRx: 8110.08
laneRateFb: 8110.08
laneRateTx: 8110.08
2T2R1F Number: 1
Valid Configuration: True
laneRateRx: 8110.08
laneRateFb: 8110.08
laneRateTx: 8110.08
Device Initialization for ChipVersion: 1.3
DONOT_OPEN_Atharv_FULL - Device registers reset.
chipType: 0xa
chipId: 0x78
chipVersion: 0x11
SPIA has got control of PLL pages
PLL Pages SPI control relinquished.
Fuse farm load autoload done successful
No autload error
Fuse farm load autoload done successful
No autload error
//Firmware Version = 11000
//PG Version = 1
//Release Date [dd/mm/yy] = 10/7/19
patchSize=11697
//Patch Version = 165
//PG Version = 0
//Release Date [dd/mm/yy] = 27/11/21
SPIA has got control of PLL pages
PLL Locked
PLL Pages SPI control relinquished.
SPIA has got control of PLL pages
PLL Pages SPI control relinquished.
SPIA has got control of PLL pages
PLL Pages SPI control relinquished.
SPIA has got control of PLL pages
PLL Pages SPI control relinquished.
Sysref Read as expected
SPIA has got control of PLL pages
PLL Pages SPI control relinquished.
Setting RBD to: 28
Setting RBD to: 28
SPIA has got control of PLL pages
PLL Pages SPI control relinquished.
###########Device DAC JESD-RX 0 Link Status###########
lane0 Errors=0b10000; Got errors: elastic buffer overflow (bad RBD value); 
lane1 Errors=0b10000; Got errors: elastic buffer overflow (bad RBD value); 
lane2 Errors=0b10000; Got errors: elastic buffer overflow (bad RBD value); 
lane3 Errors=0b10000; Got errors: elastic buffer overflow (bad RBD value); 
CS State TX0: 0b10101010 . It is expected to be 0b10101010
BUF State TX0: 0b11111111 . It is expected to be 0b11111111
Couldn't get the link up for device RX: 0; Alarms: 0x1010101000000000L
###################################
###########Device DAC JESD-RX 1 Link Status###########
lane0 Errors=0b10000; Got errors: elastic buffer overflow (bad RBD value); 
lane1 Errors=0b10000; Got errors: elastic buffer overflow (bad RBD value); 
lane2 Errors=0b10000; Got errors: elastic buffer overflow (bad RBD value); 
lane3 Errors=0b10000; Got errors: elastic buffer overflow (bad RBD value); 
CS State TX0: 0b10101010 . It is expected to be 0b10101010
BUF State TX0: 0b11111111 . It is expected to be 0b11111111
Couldn't get the link up for device RX: 1; Alarms: 0x1010101000000000L
###################################
#Done executing .. AFE7950/bringup/script14.py
#End Time 2023-06-26 10:06:20.337000
#Execution Time = 53.3489999771 s 
#================ ERRORS:20, WARNINGS:0 ================#

顺便说一下、我使用的 FPGA 程序还来自 TI 的 vcu118_64b66b IP、我更改了引脚和收发器向导的参数、以适应 VCU128和我的 LMFS/线路速率。 但 ILA 仅在示波器上显示具有输入正弦信号的寄存器、但在示波器上没有信号、ADC 在 ILA 中也没有响应、即0000。 Vivado 消息日志中有一些警告、如下所示:

Synthesis
synth_1
[Constraints 18-1056] Clock 'fpga_ref_clk' completely overrides clock 'sys_clk_p'.
New: create_clock -period 6.400 -name fpga_ref_clk [get_ports sys_clk_p], ["D:/Users/ww/vcu128_6466b/vcu118_64b66b/constraints.xdc": and 2]
Previous: create_clock -period 8.138 [get_ports sys_clk_p], ["d:/Users/ww/vcu128_6466b/vcu118_64b66b/xilinx_ip/sys_pll/sys_pll/sys_pll_in_context.xdc": and 1]
Implementation
Design Initialization
[Constraints 18-1055] Clock 'fpga_ref_clk' completely overrides clock 'sys_clk_p', which is referenced by one or more other constraints. Any constraints that refer to the overridden clock will be ignored.
New: create_clock -period 6.400 -name fpga_ref_clk [get_ports sys_clk_p], ["D:/Users/ww/vcu128_6466b/vcu118_64b66b/constraints.xdc": and 2]
Previous: create_clock -period 8.138 [get_ports sys_clk_p], ["d:/Users/ww/vcu128_6466b/vcu118_64b66b/xilinx_ip/sys_pll/sys_pll.xdc": and 56]
[Designutils 20-1281] Could not find module 'vio_ilas'. The XDC file d:/Users/ww/vcu128_6466b/vcu118_64b66b/xilinx_ip/vio_ilas/vio_ilas.xdc will not be read for this module.
[Vivado 12-4739] set_clock_groups:No valid object(s) found for '-group [get_clocks -of_objects [get_pins TI_IP_inst/mgt_tx_usrclk2]]'. ["D:/Users/ww/vcu128_6466b/vcu118_64b66b/constraints.xdc":10]
[Vivado 12-5201] set_clock_groups: cannot set the clock group when only one non-empty group remains. ["D:/Users/ww/vcu128_6466b/vcu118_64b66b/constraints.xdc":10]
Route Design[Timing 38-282] The design failed to meet the timing requirements. Please see the timing summary report for details on the timing violations.

这一切都与 XDC 文件有关、但我只更改了 vcu128和 AFE7950的引脚位置。

我现在很困惑。 您能帮助我找到可能的原因吗?   对此、我将不胜感激。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    尊敬的 Wei:

    首先、我建议检查的是使用的是 AFE79xx GUI 的最新版本。 这在 AFE79xx 加密文件夹中提供。

    还应检查 JESD_LINK_PARAMS.VH 文件中的通道多路复用器和通道极性设置。 根据 AFE SERDES 通道与 FPGA 通道之间的连接、应进行相应更新。 这一点很重要、因为从 AFE 到 FPGA 的通道可能不会一映射到一个、并且某些通道可能会反转。  

    如果在进行上述更改后仍收到错误的 RBD 值错误,则可以尝试运行 setGoodRbd 命令来找到合适的 RBD 值,这 是在运行脚本时完成的。  

    需要运行的两个命令如下。

    AFE.JESD.DACJESD[0].setGoodRbd ()

    AFE.JESD.DACJESD[1].setGoodRbd ()

    此致、

    大卫·查帕罗