This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] AFE7950EVM:关于 AFE7950 JESD204B

Guru**** 2766525 points

Other Parts Discussed in Thread: AFE7950

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/rf-microwave-group/rf-microwave/f/rf-microwave-forum/1273188/afe7950evm-about-afe7950-jesd204b

器件型号:AFE7950EVM
主题中讨论的其他器件:AFE7950

您好、TI 团队、

   AFE7950启动期间发生错误。

   此步骤中有错误:  开始:读取 JESD RX 状态以检查链路是否已建立。   

   检查寄存器0x0119的值时出错。    

     我正在使用的 Latte 脚本是:S4_OnboardClk_RX_TX_250M_5Gbps_8Lanes.py  。  

##############		Read me			##############
#In HSDC Pro DAC tab, Select AFE79xx_2x2TX_44210; Data Rate = 245.76M
#In HSDC Pro ADC tab, Select AFE79xx_2x2RX_44210; Data Rate = 245.76M ---> To capture 4 RX channels

sysParams=AFE.systemParams
sysParams.__init__();sysParams.chipVersion=chipVersion

setupParams.skipFpga = 1 # setup FPGA (TSW14J56) using HSDC Pro 
##############		Top Level			##############
sysParams.FRef			= 491.52
sysParams.FadcRx		= 2949.12
sysParams.FadcFb		= 2949.12
sysParams.Fdac			= 2949.12*4
sysParams.externalClockRx=False
sysParams.externalClockTx=False
sysParams.spiMode		= 0			#wuyf add for 3wire SPI Mode										
##############		Digital Chain		##############

		#####	RX	#####
sysParams.ddcFactorRx	=	[12,12,12,12]			#DDC decimation factor for RX A, B, C and D
sysParams.rxNco0		= 	[[9500,9500],			#Band0, Band1 for RXA 
							[9500,9500],        	#Band0, Band1 for RXB 
							[9500,9500],        	#Band0, Band1 for RXC 
							[9500,9500]]        	#Band0, Band1 for RXD  

		#####	FB	#####
sysParams.fbEnable		=	[False,False]
sysParams.ddcFactorFb	=	[12,12]					#DDC decimation factor for FB 1 and 2
sysParams.fbNco0		= 	[9500,9500]				#Band0 for FB1 and FB2 

		#####	TX	#####
sysParams.ducFactorTx	=	[48,48,48,48]			#DUC interpolation factor for TX A, B, C and D
sysParams.txNco0		= 	[[9500,9500],			#Band0, Band1 for TXA 
							[9500,9500],        	#Band0, Band1 for TXB 
							[9500,9500],        	#Band0, Band1 for TXC 
							[9500,9500]]        	#Band0, Band1 for TXD


##############		JESD		##############

		#####	ADC-JESD	#####
sysParams.jesdSystemMode= [3,3]
													#SystemMode 0:	2R1F-FDD						; rx1-rx2-fb -fb
													#SystemMode 1:	1R1F-FDD						; rx -rx -fb -fb
													#SystemMode 2:	2R-FDD							; rx1-rx1-rx2-rx2
													#SystemMode 3:	1R								; rx -rx -rx -rx
													#SystemMode 4:	1F								; fb -fb- fb -fb
													#SystemMode 5:	1R1F-TDD						; rx/fb-rx/fb-rx/fb-rx/fb
													
sysParams.jesdTxProtocol= [0,0]						# 0 - 8b/10b encoding; 2 - 64b/66b encoding 
sysParams.LMFSHdRx		= ["44210","44210","44210","44210"]
													# The 2nd and 4th are valid only for jesdSystemMode values in (0,2).
													# For other modes, select 4 converter modes for 1st and 3rd.
sysParams.LMFSHdFb		= ["22210","22210"]

sysParams.rxJesdTxScr	= [True,True,True,True]
sysParams.fbJesdTxScr	= [True,True]

sysParams.rxJesdTxK		= [16,16,16,16]
sysParams.fbJesdTxK		= [16,16]

sysParams.jesdTxLaneMux	= [0,1,2,3,4,5,6,7]			# Enter which lanes you want in each location. 
													# For example, if you want to exchange the first two lines of each 2T,
													#		this should be [[1,0,2,3],[5,4,6,7]]

		#####	DAC-JESD	#####
sysParams.jesdRxProtocol= [0,0]
sysParams.LMFSHdTx		= ["44210","44210","44210","44210"]
sysParams.jesdRxLaneMux	= [0,1,2,3,4,5,6,7]			# Enter which lanes you want in each location.
													# For example, if you want to exchange the first two lines of each 2R
													#		this should be [[1,0,2,3],[5,4,6,7]]
sysParams.jesdRxRbd		= [4, 4]
sysParams.jesdRxScr		= [True,True,True,True]
sysParams.jesdRxK		= [16,16,16,16]

		#####	JESD Common	#####
	
sysParams.jesdABLvdsSync= True
sysParams.jesdCDLvdsSync= True
sysParams.syncLoopBack	= True	#JESD Sync signal is connected to FPGA

##############		GPIO		##############
sysParams.gpioMapping	= {
						'H8': 'ADC_SYNC0',
						'H7': 'ADC_SYNC1',
						'N8': 'ADC_SYNC2',
						'N7': 'ADC_SYNC3',
						'H9': 'DAC_SYNC0',
						'G9': 'DAC_SYNC1',
						'N9': 'DAC_SYNC2',
						'P9': 'DAC_SYNC3',
						'P14': 'GLOBAL_PDN',
						'K14': 'FBABTDD',
						'R6': 'FBCDTDD',
						'H15': ['TXATDD','TXBTDD'],
						'V5': ['TXCTDD','TXDTDD'],
						'E7': ['RXATDD','RXBTDD'],
						'R15': ['RXCTDD','RXDTDD']}

##############		LMK Params		##############
lmkParams.pllEn			= False
lmkParams.inputClk		= 983.04 # Valid only when lmkParams.pllEn = False
lmkParams.lmkFrefClk	= True
setupParams.fpgaRefClk	= 122.88 # Should be equal to LaneRate/40 for TSW14J56

##############		Logging		##############
logDumpInst.setFileName("d:\\afe_save\\AFE79xxConfig.txt")
logDumpInst.logFormat=0x1 #Modify to 0x1 to save register scequence to log file. Script takes more time to execute.
#logDumpInst.setFileName(ASTERIX_DIR+DEVICES_DIR+r"\Afe79xxPg1.txt")
#logDumpInst.logFormat=0x0 #Modify to 0x1 to save register scequence to log file. Script takes more time to execute.
logDumpInst.rewriteFile=1
logDumpInst.rewriteFileFormat4=1
device.optimizeWrites=0
device.rawWriteLogEn=1

device.delay_time = 0
#-------------------------------------------------------------------------------------------------#
AFE.deviceBringup()

AFE.TOP.overrideTdd(15,3,15)	# bit-wise; 4R,2F,4T

   我使用的是 Xilinx 的 JESD IP。   线路速率为4.9152Gbps、每个链路的通道数为8。

    

    我有以下问题:

 AFE 芯片具有4个 SYNCOUT 引脚和4个 SYNCOUT 引脚。 哪个引脚应该连接到相应的 FPGA JESD TX/Rx 同步引脚?

2. 当 AFE 使用8个通道时,我应该在 Xilinx FPGA 上使用多少个 JESD IP ?     一对 TX/Rx IP 还是两对?

顺便说一下:当我执行"checkDeviceHealth"函数时、 出现以下错误:错误:  DAC JESD RX AB。 连接未建立。 未通过 CS 状态。  错误:串行器/解串器 Rx 通道0遇到 LOS 错误。 可能存在串行器/解串器眼图问题。

   

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好、

    默认情况下、所有 Rx 通道都组合到单个链路中并共享一个 SYNC 信号。 您应该用于下面给出的 ADC 通道的 LVDS 同步信号。
    'H8':'ADC_SYNC0'、
    'H7':'ADC_SYNC1'、

    DAC 通道类似、LVDS Sync 信号连接到以下引脚。

    'h9':'DAC_SYNC0'、
    'G9':'DAC_SYNC1'、

    由于 JESD/Tx 通道共享 SYNC 信号、因此侧的 Rx 链路应配置为单个8通道 IP。  

    LOS 错误表示 DAC 在 FPGA 的 SERDES 通道上未看到任何数据。  在配置 AFE 之前、您能否确认已在 FPGA 侧连接了正确的通道并且 FPGA 正在在 SERDES 通道上发送数据?  

    此致、

    大卫·查帕罗

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好,David,

       我想确认 AFE 的 JESD 是否可以在启用环回后建立链路。 我尝试启用 AFE7950的 JESD 环回功能、但此时没有 LOS 错误。

    sysParams.jesdABLvdsSync= True
    sysParams.jesdCDLvdsSync= True
    sysParams.syncLoopBack	= False	#JESD Sync signal is connected to FPGA
    sysParams.jesdLoopbackEn= True
    

    但 JESD 仍然没有建立链路。   我执行了这个函数:adcDacSync,遇到一些错误:

    这些误差是什么意思?  1 μ s 未)CS 状态  2)串行器/解串器 Rx 通道0发生 FIFO 错误。 可能存在串行器/解串器眼图问题或 FIFO 偏移问题。

    在测试过程中、我仅打开了 TXA、TXB、RXA、RXB。   因此通道0-3没有 LOS 错误。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好,David,

         启用 JESD 的环回功能后、如果 RXA 未接收数据、JESD 是否也会建立链路?

         由于 AFE 的同步输入/输出均连接到 FPGA、这在启用环回时是否会影响 JESD 的链路?

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    您好、

     是的、无论 ADC 是否具有输入、都应出现 JESD。  由于您将 sysParams.syncLoopBack 设置为"False"、因此与 FPGA 的同步连接无关紧要。

    在 IP 中、您是否已将 Tx 从复位中释放出来、以便 FPGA 在启动 AFE 之前发送数据?

    对于 JESD204 IP、我推荐 TI204c-IP、因为我们提供了 AFE 的参考设计。 我们向您发送了一封包含申请表的电子邮件、填写完毕后、我可以授予您 IP 的访问权限。

    此致、

    大卫·查帕罗