This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] AFE7950EVM:正在发生 JESD 配置不匹配

Guru**** 2847400 points

Other Parts Discussed in Thread: AFE7950EVM

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/rf-microwave-group/rf-microwave/f/rf-microwave-forum/1453189/afe7950evm-jesd-configuration-mismatch-is-happening

器件型号:AFE7950EVM

工具与软件:

AFE7950EVM 和 ZCU106、FPGA 编程为 LMFSH = 28810、AFE7950EVM 通过 Python 脚本编程、 LMFSHK = 14810。

这是我正在运行的 python 脚本

##############		Read me			##############
#In HSDC Pro DAC tab, Select AFE79xx_2x2TX_44210; Data Rate = 245.76M
#In HSDC Pro ADC tab, Select AFE79xx_2x2RX_44210; Data Rate = 245.76M ---> To capture 4 RX channels

sysParams=AFE.systemParams
sysParams.__init__();sysParams.chipVersion=chipVersion

setupParams.skipFpga = 1 # setup FPGA (TSW14J56) using HSDC Pro 
##############		Top Level			##############
sysParams.FRef			= 491.52
sysParams.FadcRx		= 2949.12
sysParams.FadcFb		= 2949.12
sysParams.Fdac			= 2949.12*4
sysParams.externalClockRx=False
sysParams.externalClockTx=False
													
##############		Digital Chain		##############

		#####	RX	#####
sysParams.ddcFactorRx	=	[12,12,12,12]			#DDC decimation factor for RX A, B, C and D
sysParams.rxNco0		= 	[[9500,9500],			#Band0, Band1 for RXA 
							[9500,9500],        	#Band0, Band1 for RXB 
							[9500,9500],        	#Band0, Band1 for RXC 
							[9500,9500]]        	#Band0, Band1 for RXD  

		#####	FB	#####
sysParams.fbEnable		=	[False,False]
sysParams.ddcFactorFb	=	[12,12]					#DDC decimation factor for FB 1 and 2
sysParams.fbNco0		= 	[9500,9500]				#Band0 for FB1 and FB2 

		#####	TX	#####
sysParams.ducFactorTx	=	[48,48,48,48]			#DUC interpolation factor for TX A, B, C and D
sysParams.txNco0		= 	[[9500,9500],			#Band0, Band1 for TXA 
							[9500,9500],        	#Band0, Band1 for TXB 
							[9500,9500],        	#Band0, Band1 for TXC 
							[9500,9500]]        	#Band0, Band1 for TXD


##############		JESD		##############

		#####	ADC-JESD	#####
sysParams.jesdSystemMode= [1,1]
													#SystemMode 0:	2R1F-FDD						; rx1-rx2-fb -fb
													#SystemMode 1:	1R1F-FDD						; rx -rx -fb -fb
													#SystemMode 2:	2R-FDD							; rx1-rx1-rx2-rx2
													#SystemMode 3:	1R								; rx -rx -rx -rx
													#SystemMode 4:	1F								; fb -fb- fb -fb
													#SystemMode 5:	1R1F-TDD						; rx/fb-rx/fb-rx/fb-rx/fb
													
sysParams.jesdTxProtocol= [0,0]						# 0 - 8b/10b encoding; 2 - 64b/66b encoding 
sysParams.LMFSHdRx		= ["14810","14810","14810","14810"]   #changed by Lakshmi ["44210","44210","44210","44210"] 
													# The 2nd and 4th are valid only for jesdSystemMode values in (0,2).
													# For other modes, select 4 converter modes for 1st and 3rd.
sysParams.LMFSHdFb		= ["14810","14810"]

sysParams.rxJesdTxScr	= [True,True,True,True] #changed by Lakshmi
sysParams.fbJesdTxScr	= [False,False]

sysParams.rxJesdTxK		= [16,16,16,16]
sysParams.fbJesdTxK		= [16,16]

sysParams.jesdTxLaneMux	= [0,1,2,3,4,5,6,7]			# Enter which lanes you want in each location. 
													# For example, if you want to exchange the first two lines of each 2T,
													#		this should be [[1,0,2,3],[5,4,6,7]]

		#####	DAC-JESD	#####
sysParams.jesdRxProtocol= [0,0]
sysParams.LMFSHdTx		= ["14810","14810","14810","14810"]  	#changed by Lakshmi ["44210","44210","44210","44210"] 
sysParams.jesdRxLaneMux	= [0,1,2,3,4,5,6,7]			# Enter which lanes you want in each location.
													# For example, if you want to exchange the first two lines of each 2R
													#		this should be [[1,0,2,3],[5,4,6,7]]
sysParams.jesdRxRbd		= [4, 4]
sysParams.jesdRxScr		= [True,True,True,True]
sysParams.jesdRxK		= [16,16,16,16]

		#####	JESD Common	#####
	
sysParams.jesdABLvdsSync= True
sysParams.jesdCDLvdsSync= True
sysParams.syncLoopBack	= True	#JESD Sync signal is connected to FPGA

##############		GPIO		##############
sysParams.gpioMapping	= {
						'H8': 'ADC_SYNC0',
						'H7': 'DAC_SYNC0',  	#'ADC_SYNC1',
						'N8': 'ADC_SYNC2',
						'N7': 'ADC_SYNC3',
						'H9': 'ADC_SYNC1',		#'DAC_SYNC0',
						'G9': 'DAC_SYNC1',
						'N9': 'DAC_SYNC2',
						'P9': 'DAC_SYNC3',
						'P14': 'GLOBAL_PDN',
						'K14': 'FBABTDD',
						'R6': 'FBCDTDD',
						'H15': ['TXATDD','TXBTDD'],
						'V5': ['TXCTDD','TXDTDD'],
						'E7': ['RXATDD','RXBTDD'],
						'R15': ['RXCTDD','RXDTDD']}

##############		LMK Params		##############
lmkParams.pllEn			= True
lmkParams.inputClk		= 983.04 # Valid only when lmkParams.pllEn = False
lmkParams.lmkFrefClk	= True
setupParams.fpgaRefClk	= 122.88 # Should be equal to LaneRate/40 for TSW14J56

##############		Logging		##############
logDumpInst.setFileName(ASTERIX_DIR+DEVICES_DIR+r"\Afe79xxPg1.txt")
logDumpInst.logFormat=0x0 #Modify to 0x1 to save register scequence to log file. Script takes more time to execute.
logDumpInst.rewriteFile=1
logDumpInst.rewriteFileFormat4=1
device.optimizeWrites=0
device.rawWriteLogEn=1

device.delay_time = 0
#--------------------------------------#
#setupParams.skipLmk	=	False
#AFE.initializeConfig()
#lmkParams.sysrefFreq = AFE.systemStatus.sysrefFreq
#lmkParams.lmkPulseSysrefMode = False
#AFE.LMK.lmkConfig()
#-------------------------------------------------------------------------------------------------#


AFE.deviceBringup()

AFE.TOP.overrideTdd(15,3,15)	# bit-wise; 4R,2F,4T

#setupParams.skipLmk	=	1 
#AFE.deviceBringup()
#AFE.TOP.overrideTdd(15,0,15)
#setupParams.skipLmk	=	0

运行该脚本后、我们会收到以下错误。

在 FPGA 端、我们可以看到 tx_reset_done 和 rx_reset_done 信号、但 tx_sync 和 rx_sync 信号根本不会发出。

CTRL_8B10B_CFG ( 03C )=0x03010f07

CTRL_TX_ILA_CFG1 (074) =0x000f0f07

CTRL_TX_ILA_CFG1 (078) =0x00000000

 我们将这些寄存器配置为根据 pg242-jesd204c-en-us-4.2 PDF 设置所需的参数

 

下面是写入这三个寄存器的屏幕截图

TX_CORE IP 配置:

RX_CORE IP 配置:

JESD phy IP 配置:

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    Ajay、您好!

    我相信这里有几个问题。 第一个问题是 AFE 和 FPGA 上的 JESD 设置不匹配。 通道速率设置不同。 在 AFE 端、通道速率为~19.6Gbps、我们不建议将其用于8b10b 编码、而在 FPGA 端、通道速率为4.952Gbps。 为此、我建议更改通道数或编码、然后在 FPGA 上将通道速率设置为相同的值。  

    另一个问题是、我认为 FPGA 可能在 AFE 未使用的不同串行器/解串器通道上发送数据。  

    您能否看一下这些问题、看看解决它们是否可以解决问题?  

    此致、

    David Chaparro  

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    尊敬的 David:

    我已将 AFE 和 FPGA 的通道速率配置为9.8304Gbps。 在 FPGA 端、LMFSH 设置为24810、而在 AFE 端、LMFSH 也配置为24810、具有一个实例。 我按照前面所述的 Latte 配置脚本操作、但 Latte 日志中会出现错误。 此外、来自 DAC 侧的 FPGA 侧同步信号不会通过、我们的 Rx 内核也不会生成任何同步信号。

    此外、我注意到、我们从 AFE 接收的 SYSREF 信号的频率为3.84 MHz、占空比为50%。 然而、根据我的研究、SYSREF 信号应该类似于脉冲信号、而不是占空比为50%的信号。 您能否确认我们接收的 SYSREF 信号是否正确?

    能否帮助我解决上述问题?

    #In HSDC Pro DAC tab, Select AFE79xx_2x2TX_44210; Data Rate = 245.76M
    #In HSDC Pro ADC tab, Select AFE79xx_2x2RX_44210; Data Rate = 245.76M ---> To capture 4 RX channels
    
    sysParams=AFE.systemParams
    sysParams.__init__();sysParams.chipVersion=chipVersion
    
    setupParams.skipFpga = 1 # setup FPGA (TSW14J56) using HSDC Pro 
    ##############		Top Level			##############
    sysParams.FRef			= 491.52
    sysParams.FadcRx		= 2949.12
    sysParams.FadcFb		= 2949.12
    sysParams.Fdac			= 2949.12*4
    sysParams.externalClockRx=False
    sysParams.externalClockTx=False
    													
    ##############		Digital Chain		##############
    
    		#####	RX	#####
    sysParams.ddcFactorRx	=	[12,12,12,12]			#DDC decimation factor for RX A, B, C and D
    sysParams.rxEnable		=   [True,True,False,False]
    sysParams.rxNco0		= 	[[9500,9500],			#Band0, Band1 for RXA 
    							[9500,9500],        	#Band0, Band1 for RXB 
    							[9500,9500],        	#Band0, Band1 for RXC 
    							[9500,9500]]        	#Band0, Band1 for RXD  
    
    		#####	FB	#####
    sysParams.fbEnable		=	[False,False]
    sysParams.ddcFactorFb	=	[12,12]					#DDC decimation factor for FB 1 and 2
    sysParams.fbNco0		= 	[9500,9500]				#Band0 for FB1 and FB2 
    
    		#####	TX	#####
    sysParams.ducFactorTx	=	[48,48,48,48]			#DUC interpolation factor for TX A, B, C and D
    sysParams.txEnable		=   [True,True,False,False]
    sysParams.txNco0		= 	[[9500,9500],			#Band0, Band1 for TXA 
    							[9500,9500],        	#Band0, Band1 for TXB 
    							[9500,9500],        	#Band0, Band1 for TXC 
    							[9500,9500]]        	#Band0, Band1 for TXD
    
    
    ##############		JESD		##############
    
    		#####	ADC-JESD	#####
    sysParams.jesdSystemMode= [3,3]
    													#SystemMode 0:	2R1F-FDD						; rx1-rx2-fb -fb
    													#SystemMode 1:	1R1F-FDD						; rx -rx -fb -fb
    													#SystemMode 2:	2R-FDD							; rx1-rx1-rx2-rx2
    													#SystemMode 3:	1R								; rx -rx -rx -rx
    													#SystemMode 4:	1F								; fb -fb- fb -fb
    													#SystemMode 5:	1R1F-TDD						; rx/fb-rx/fb-rx/fb-rx/fb
    													
    sysParams.jesdTxProtocol= [0,0]						# 0 - 8b/10b encoding; 2 - 64b/66b encoding 
    sysParams.LMFSHdRx		= ["24410","24410","24410","24410"]   #changed by Lakshmi ["44210","44210","44210","44210"] 
    													# The 2nd and 4th are valid only for jesdSystemMode values in (0,2).
    													# For other modes, select 4 converter modes for 1st and 3rd.
    sysParams.LMFSHdFb		= ["14810","14810"]
    
    sysParams.rxJesdTxScr	= [True,True,True,True] #changed by Lakshmi
    sysParams.fbJesdTxScr	= [True,True]
    
    sysParams.rxJesdTxK		= [16,16,16,16]
    sysParams.fbJesdTxK		= [16,16]
    
    sysParams.jesdTxLaneMux	= [0,1,2,3,4,5,6,7]			# Enter which lanes you want in each location. 
    													# For example, if you want to exchange the first two lines of each 2T,
    													#		this should be [[1,0,2,3],[5,4,6,7]]
    
    		#####	DAC-JESD	#####
    sysParams.jesdRxProtocol= [0,0]
    sysParams.LMFSHdTx		= ["24410","24410","24410","24410"]  
    sysParams.jesdRxLaneMux	= [0,1,2,3,4,5,6,7]			# Enter which lanes you want in each location.
    sysParams.serdesRxLanePolarity = [1,1,0,0,1,1,0,0]													# For example, if you want to exchange the first two lines of each 2R
    													#		this should be [[1,0,2,3],[5,4,6,7]]
    sysParams.jesdRxRbd		= [4, 4]
    sysParams.jesdRxScr		= [True,True,True,True]
    sysParams.jesdRxK		= [16,16,16,16]
    
    		#####	JESD Common	#####
    	
    sysParams.jesdABLvdsSync= True
    sysParams.jesdCDLvdsSync= True
    sysParams.syncLoopBack	= True	#JESD Sync signal is connected to FPGA
    
    ##############		GPIO		##############
    sysParams.gpioMapping	= {
    						'H8': 'ADC_SYNC0',
    						'H7': 'DAC_SYNC0',  	#'ADC_SYNC1',
    						'N8': 'ADC_SYNC2',
    						'N7': 'ADC_SYNC3',
    						'H9': 'ADC_SYNC1',		#'DAC_SYNC0',
    						'G9': 'DAC_SYNC1',
    						'N9': 'DAC_SYNC2',
    						'P9': 'DAC_SYNC3',
    						'P14': 'GLOBAL_PDN',
    						'K14': 'FBABTDD',
    						'R6': 'FBCDTDD',
    						'H15': ['TXATDD','TXBTDD'],
    						'V5': ['TXCTDD','TXDTDD'],
    						'E7': ['RXATDD','RXBTDD'],
    						'R15': ['RXCTDD','RXDTDD']}
    
    ##############		LMK Params		##############
    lmkParams.pllEn			= True
    lmkParams.inputClk		= 983.04 # Valid only when lmkParams.pllEn = False
    lmkParams.lmkFrefClk	= True
    setupParams.fpgaRefClk	= 245.76 # Should be equal to LaneRate/40 for TSW14J56
    
    ##############		Logging		##############
    logDumpInst.setFileName(ASTERIX_DIR+DEVICES_DIR+r"\Afe79xxPg1.txt")
    logDumpInst.logFormat=0x0 #Modify to 0x1 to save register scequence to log file. Script takes more time to execute.
    logDumpInst.rewriteFile=1
    logDumpInst.rewriteFileFormat4=1
    device.optimizeWrites=0
    device.rawWriteLogEn=1
    
    device.delay_time = 0
    
    AFE.deviceBringup()
    
    AFE.TOP.overrideTdd(15,3,15)	# bit-wise; 4R,2F,4T

    日志结果:

     ...

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    Ajay、您好!

    我看到有两个问题。 第一个是、如果您想使用 CMOS 同步信号、则应将以下两个参数设置为"False"。

    sysParams.jesdABLvdsSync= True
    sysParams.jesdCDLvdsSync= True

    第二个问题是您看到的 LOS 错误表示 FPGA 可能在不同的串行器/解串器通道上发送数据。 您能否确认您的 FPGA 已配置为在连接到 SRX1和 SRX2的 FPGA 通道上发送数据?

    此致、

    David Chaparro  

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    尊敬的 David:

    关于串行器/解串器通道连接、我们目前仅将数据传输到 SRX1和 SRX2。

    根据您的说明、我们已将两个参数更新为"false"。 但是、仍没有接收到 SYNC 信号、并且我们在 Latte 日志中会遇到错误。 此外、我之前在上一个问题中询问了 SYSREF 信号。 您能确认一下它的状态吗?

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    尊敬的 David:

    我们拥有 DC135-AFE7950EVM 电路板;但是我们无法找到其原理图。 因此、我们使用了 DC150A-AFE7950EVM 原理图作为参考。 请您确认这种方法是否可以接受? 如果不能、您能否将我引导至能找到所需原理图的位置? 是否可以共享原理图 DC135A 板的链接。