This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] LDC3114:应用建议

Guru**** 2434370 points
Other Parts Discussed in Thread: LDC1612, LDC3114, LDC1314, LDC0851

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/sensors-group/sensors/f/sensors-forum/1516519/ldc3114-application-recommendation

器件型号:LDC3114
主题中讨论的其他部件:LDC1612LDC1314、LDC0851

工具/软件:

尊敬的团队:

设计门锁、例如 LDC3114、LDC1612、LDC1314、这一项更合适或推荐使用哪种型号。

1、该产品由3V 扭转按钮电池供电,因此该传感器需要支持低功耗,平均待机电流不超过50uA。
2.允许传感器定期运行,循环不超过100毫秒。
3、脏潮湿环境不会影响传感器,所以应优先选择电感式传感器。
4、金属锁舌的材料有两种:铁和不锈钢。 当锁舌接近并离开传感区域时、系统有两种不同的输出状态可识别。
5、金属锁舌在传感区域长时间内时,不应增加太多功耗。
6.该传感器有一个中断输出引脚,可在状态变化时唤醒系统。
7、如果满足上述条件,可接受纯硬件传感器解决方案,但也可以是 I2C/UART/SPI 接口传感器,其可靠性和稳定性得到优先考虑。