This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TPS8802EVM:从睡眠状态唤醒期间的 INT_MCU 引脚锁存问题。

Guru**** 2581345 points
Other Parts Discussed in Thread: TPS8802

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/sensors-group/sensors/f/sensors-forum/1554775/tps8802evm-int_mcu-pin-latching-issue-during-wakeup-from-sleep

器件型号:TPS8802EVM
主题中讨论的其他器件:TPS8802

工具/软件:

TI 团队大家好、

我观察到 TPS8802 EVM 存在异常行为。

我配置了 TPS8802 睡眠计时器 10 秒。 计时器到期后、INT_MCU引脚变为高电平以向 MCU 发出信号、并使 STATUS1 获取 SLP_DONE。

但是、我注意到、INT_MCU当我连续读取STATUS1寄存器(偏移= 0x01)时、该引脚仅从低电平转换为高电平。 如果我不读取STATUS1、该INT_MCU引脚保持锁存为高电平。

在显示 INT_MCU 行为的日志之后 一方 之间的比较 读取STATUS1寄存器:

------------------------

AFE in SLEEP MODE (><)    <----- With Read Status register 

------------------------ 

Sleep Timer Start...

AFE is suspend for 11sec [0]

 

INT_STATUS: 0

Status Value: 0

AFE is suspend for 11sec [1]

 

INT_STATUS: 0

Status Value: 0

AFE is suspend for 11sec [2]

 

INT_STATUS: 0

Status Value: 0

AFE is suspend for 11sec [3]

 

INT_STATUS: 0

Status Value: 0

AFE is suspend for 11sec [4]

 

INT_STATUS: 0

Status Value: 0

AFE is suspend for 11sec [5]

 

INT_STATUS: 0

Status Value: 0

AFE is suspend for 11sec [6]

 

INT_STATUS: 0

Status Value: 0

AFE is suspend for 11sec [7]

 

INT_STATUS: 0

Status Value: 0

AFE is suspend for 11sec [8]

 

INT_STATUS: 0

Status Value: 0

AFE is suspend for 11sec [9]

 

INT_STATUS: 1

Status Value: 128

SLP_DONE

AFE is suspend for 11sec [10]

 

INT_STATUS: 0

Status Value: 0

 

==============================
--------------------------
 
AFE in SLEEP MODE (><)   <---- without read Status register

-------------------------- 

Sleep Timer Start...

AFE is suspend for 11sec [0]

 

INT_STATUS: 1        <----------------- getting INT_MCU bit High.

AFE is suspend for 11sec [1]

 

INT_STATUS: 1

AFE is suspend for 11sec [2]

 

INT_STATUS: 1

AFE is suspend for 11sec [3]

 

INT_STATUS: 1

AFE is suspend for 11sec [4]

 

INT_STATUS: 1

AFE is suspend for 11sec [5]

 

INT_STATUS: 1

AFE is suspend for 11sec [6]

 

INT_STATUS: 1

AFE is suspend for 11sec [7]

 

INT_STATUS: 1

AFE is suspend for 11sec [8]

 

INT_STATUS: 1

AFE is suspend for 11sec [9]

 

INT_STATUS: 1

AFE is suspend for 11sec [10]

 

INT_STATUS: 1


以下寄存器 I 配置为基于 INT_MCU/中断的唤醒

void afe_i2c_sleep_timer(uint16_t sleep_time)
{
    SetSleeptime = sleep_time;

    // Mask all interrupts, enable INT_MCU
    i2c_write_data(i2c_dev, TPS880X_REG_MASK, 0x7F); // SLP_DONEM = 0, STATUS_INT = 1 allows SLP_DONE flag to appear on INT_MCU pin

    i2c_write_data(i2c_dev, TPS880X_REG_CONFIG1, 0x32); //SLP_MCU = SLP_BST = 0, SLP_ANALOG = 1 

    // TPS ---> MCU Interupt , INT_EN = 0
    i2c_write_data(i2c_dev, TPS880X_REG_ENABLE1, 0x1D); // INT_EN = 0

    if (sleep_time == 0) {
        // Disable the Sleep timer
        i2c_write_data(i2c_dev, TPS880X_REG_SLPTMR1, 0x00);
        i2c_write_data(i2c_dev, TPS880X_REG_SLPTMR2, 0x00);
    }
    else
    {
        // Validate interval
        if (sleep_time < DUALRAYSMOKEAFE_HAL_TIMING_ULPTIMER_MIN_INTERVAL_MS)
        {
            sleep_time = DUALRAYSMOKEAFE_HAL_TIMING_ULPTIMER_MIN_INTERVAL_MS;
        }
        else if (sleep_time > DUALRAYSMOKEAFE_HAL_TIMING_ULPTIMER_MAX_INTERVAL_MS)
        {
            sleep_time = DUALRAYSMOKEAFE_HAL_TIMING_ULPTIMER_MAX_INTERVAL_MS;
        }
    }
    // MSB
    i2c_write_data(i2c_dev, TPS880X_REG_SLPTMR1, sleep_time >> 8);
    // LSB
    i2c_write_data(i2c_dev, TPS880X_REG_SLPTMR2, sleep_time & 0xFF);

    // TPS ---> MCU Interupt , INT_DIR = 0
    i2c_write_data(i2c_dev, TPS880X_REG_ENABLE2, 0x85); // Put TPS8802 to sleep with SLP_EN = 1, LEDPIN_EN = LEDSEL = 1, INT_DIR = 0
    
    printk("Sleep Timer Start...\n");

    StartSleepTimerHandler();
}
 


您能否澄清为什么会发生这种行为、以及 在到期后是否可以在不读取 STATUS1 寄存器的情况下将 INT_MCU 引脚保持高电平(因为我想将 MCU 与 I2C 外设一起完全置于睡眠状态)?

此致、
Pratik Panchal