Other Parts Discussed in Thread: AWR1843BOOST
器件型号: DCA1000EVM
Thread 中讨论的其他器件: AWR1843BOOST
AWR1843BOOST 和 DCA1000 数据采集卡是使用 12.6V 1000mA 电源错误连接的
再次错误使用时、发现 DCA1000 左上角有一行红灯亮起。 使用普通电源替换后、无法使用 mmWave Studio 正常执行数据采集工作。 主要问题是它无法连接到 DCA1000、如所示
[19:58:25] [RadarAPI]: ar1.CaptureCardConfig_EthInit("192.168.33.30", "192.168.33.180", "12:34:56:78:90:12", 4096, 4098)
[19:58:25] [RadarAPI]: ar1.CaptureCardConfig_Mode(1, 2, 1, 2, 3, 30)
[19:58:25] [RadarAPI]: ar1.CaptureCardConfig_PacketDelay(25)
[19:58:25] [RadarAPI]: Sending fpga command to DCA1000
[19:58:35] [RadarAPI]:
[19:58:35] FPGA Configuration :
[19:58:35] Timeout Error! System disconnected
[19:58:35] [RadarAPI]: Sending record command to DCA1000
[19:58:45] [RadarAPI]:
[19:58:45] Configure Record :
[19:58:45] Timeout Error! System disconnected
[19:58:45] [RadarAPI]: ar1.GetCaptureCardFPGAVersion()
[19:58:45] [RadarAPI]: Sending fpga_version command to DCA1000
[19:58:55] [RadarAPI]:
[19:58:55]
[19:58:55] Unable to read FPGA Version. [error -5]
[19:58:55]
[19:59:51] [RadarAPI]: ar1.CaptureCardConfig_EthInit("192.168.33.30", "192.168.33.180", "12:34:56:78:90:12", 4096, 4098)
[19:59:51] [RadarAPI]: ar1.CaptureCardConfig_Mode(1, 2, 1, 2, 3, 30)
[19:59:51] [RadarAPI]: ar1.CaptureCardConfig_PacketDelay(25)
[19:59:51] [RadarAPI]: Sending fpga command to DCA1000
[20:00:01] [RadarAPI]:
[20:00:01] FPGA Configuration :
[20:00:01] Timeout Error! System disconnected
[20:00:01] [RadarAPI]: Sending record command to DCA1000
[20:00:11] [RadarAPI]:
[20:00:11] Configure Record :
[20:00:11] Timeout Error! System disconnected
[20:00:11] [RadarAPI]: ar1.GetCaptureCardFPGAVersion()
[20:00:11] [RadarAPI]: Sending fpga_version command to DCA1000
[20:00:21] [RadarAPI]:
[20:00:21]
[20:00:21] Unable to read FPGA Version. [error -5]
DCA1000 是否会因电源电压过大而烧毁?
但我可以正常使用演示可视化工具。