This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] IWR1642BOOST:无法启动 mmWave Studio Matlab 引擎#39;t。

Guru**** 2540720 points
Other Parts Discussed in Thread: IWR1642BOOST

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/sensors-group/sensors/f/sensors-forum/995288/iwr1642boost-mmwave-studio-matlab-engine-couldn-t-be-started

器件型号:IWR1642BOOST

我有一个连接到 DCA1000的 IWR1642BOOST。 按照 mmWave Studio 用户指南第2节中的说明操作后、以下错误将向我表示欢迎、如下所示。 我在 C:\Program Files (x86)\MATLAB RUNTIME\v851安装了 Matlab 运行时引擎8.5.1 32位

gm:构造函数
GM:2021年4月20日14:33:05日星期二
RSTD.Transmit ("/设置")
[14:33:05]
[14:33:05]###正在运行启动脚本:"C:\ti\mmwave_studio:02_01_01_00\mmWaveStudio\Scripts\Startup.lua"###
[14:33:05] RSTD.SetAndTransmit (“/Settings/Scripter/Display DateTime”,“1”)
[14:33:05] RSTD.SetAndTransmit ("/Settings/Scripter/DateTime 格式"、"HH:mm:ss")
[14:33:05]脚本编辑被忽略:再次尝试 UnBuild()或在编译之前。
[14:33:05] RSTD.SetVar ("/Settings/Clients/Client 0/dll"、"C:\\ti\\mmwave_studio 02_01_01_00\\mmWaveStudio\\Clients\\LabClients.dll")
[14:33:05] RSTD.SetVar ("/Settings/Clients/Client 0/use"、"true")
[14:33:05] RSTD.SetVar ("/Settings/Clients/Client 1/使用"、"false")
[14:33:05] RSTD.SetVar ("/Settings/Clients/Client 2/使用"、"false")
[14:33:05] RSTD.SetVar (“/Settings/Clients/Client 3/use”,“false”)
[14:33:05] RSTD.SetVar (“/Settings/Clients/Client 4/use”,“false”)
[14:33:05] RSTD.SetVar ("/Settings/AL Client/Al dll"、"C:\\ti\\mmwave_studio 02_01_01_00\\mmWaveStudio\\RUNTIME\\SAL.dll")
[14:33:05] RSTD.SetVar (“/Settings/Clients/Client 0/GuiDll",“”)
[14:33:05] RSTD.SetVar ("/Settings/AutoUpdate/Enabled "、"真")
[14:33:05] RSTD.SetVar (“/Settings/AutoUpdate/Interval”,“1”)
[14:33:05] RSTD.SetVar ("/Settings/Monitors/UpdateDisplay "、"真")
[14:33:05] RSTD.SetVar ("/Settings/Monitors/OneClickStart "、"真")
[14:33:05] RSTD.SetVar (“/Settings/Automation/Automation Mode”,“false”)
[14:33:05] RSTD.Transmit ("/")
[14:33:05] RSTD.SaveSettings():设置保存到"C:\Users\salehc\AppData\Roaming\RSTD\config.xml"
[14:33:05] RSTD.BUILD ()
[14:33:05] RSTD.SaveSettings():设置保存到"C:\Users\salehc\AppData\Roaming\RSTD\config.xml"
[14:33:05] RSTD.Transmit ("/")
[14:33:05] RSTD.AL_BUILD ()
[14:33:05] RSTD.AL_LoadXml ()
[14:33:05] RSTD.Transmit ("/")
[14:33:05] RSTD.Al_Init ()
[14:33:05] RSTD.Clients_build()
[14:33:05] gm:初始化
[14:33:05] gm:加载了'C:\ti\mmwave_studio_02_01_00\mmWaveStudio\clients\LabClient.dll
[14:33:05] gm:1个访客(s)初始化
[14:33:05] GM:1个模块初始化
[14:33:05] gm:2选项卡(s)初始化
[14:33:05] RSTD.Client_LoadXml()
[14:33:06][RadarAPI]:ar1.selectRadarMode(0)
[14:33:06][RadarAPI]:状态:已通过
[14:33:06]已安装 Matlab 运行时引擎
[14:33:06][RadarAPI]:启动 Matlab 引擎..
[14:33:06][RadarAPI]:错误:'MatlabPostProcGui.MatlabPostProceGUIClass'的类型初始化程序抛出异常。
[14:33:06]跟踪:
[14:33:06],MatlabPostProcGui.MatlabPostProceGUIClass..ctor ()
[14:33:06],网址为 AR1xController.frmAR1Main.InitMatlabPostProcEngine(String PostProcess 类路径)
[14:33:06][RadarAPI]:错误:Matlab 初始化中发生错误
[14:33:06][RadarAPI]:无法启动 MATLAB 引擎..
[14:33:08][RadarAPI]:ar1.selectCascadeMode(0)
[14:33:08][RadarAPI]:状态:已通过
[14:33:08][RadarAPI]:ar1.LoadSettings ('C:\Users\salehc\AppData\Roaming\RSTD\ar1gui.ini')
[14:33:08][RadarAPI]:错误:对象引用未设置为对象的实例。
[14:33:08]跟踪:
[14:33:08] at AR1xController.ScriptOps.getMatlabPostProcVersion()
[14:33:08]
[14:33:08]&&&&&&&&&&&&&&&&&&&&&&
[14:33:08]***脚本失败!***
[14:33:08]&&&&&&&&&&&&&&&&&&&&&&
[14:33:08]异常消息是:
[14:33:08]无法加载 DLL 'mclmcrrt8_5_1.dll':找不到指定的模块。 (HRESULT 例外:0x8007007E)