请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:HDC1080 您好!
我在项目中使用 HDC1080传感器、该传感器将长期测量现场湿度超过80%。
我的问题是、当我需要激活加热位以去除水分时、传感器将持续感应80%的湿度
当我的感应条件始终湿度超过80%时。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.