This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] AWR1642BOOST:AWR1642支持的带宽是4 GHz 还是5 GHz?

Guru**** 2606725 points


请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/sensors-group/sensors/f/sensors-forum/662281/awr1642boost-awr1642-supported-bandwidth-is-4-ghz-or-5ghz

器件型号:AWR1642BOOST

各位专家、您好!

从纸质 swrs203中,我们可以获得以下信息:

问:76至81GHz 意味着5GHz、为什么这是4GHz?

BS  

南山