This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] AWR1443BOOST:固定射频频率输出

Guru**** 2587365 points


请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/sensors-group/sensors/f/sensors-forum/651386/awr1443boost-fixed-rf-frequency-output

器件型号:AWR1443BOOST

您好!

我有一个新问题:能否对毫米波传感器芯片(以及其他模型)进行编程、使其与固定射频频率输出(无斜坡)一样工作? 例如在78GHz 时?  

是否可以调制输出(通过简单的方波、开/关)?

谢谢!