请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:LM96080 大家好、
我的客户对 LM96080有2个问题:
值 RAM 的长度是20h 至29h? 它是1字节或2字节(10位)值?
2. 读回 ID 寄存器0x3E 的值为0x1A。 但在数据表中、它应该默认为0x01?
谢谢你
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.