请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:LM35 你(们)好
我对 LM35有疑问。
采用 TO-46封装的 LM35能否感应底部的温度?
如果 在 TO92、TO-46和 SOIC 封装中提供 LM35的安装和安装指南,请与任何人分享。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.