Other Parts Discussed in Thread: DRV5032
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:DRV5032 大家好、
3V 电源下5Hz 时的功耗是多少?
我的客户非常关心功耗、我只发现5Hz 和1.8V 时的功耗。
或者、您是否对具有更低功耗的霍尔传感器有更好的建议?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.