请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:AWRL6432 主题中讨论的其他器件:AWR6843、
Champs,
AWRL6432是否也像 AWR6843一样支持动态节能功能(rlRfDynamicPowerSave)?
此致、
海登
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好!
在 SDK MMWAVE_DFP 中、可以选择节能"T_RL_API_SENS_DYN_PWR_SAVE_DIS"。
(dfp_sensor.h)
/*! * @brief Sensor inter-chirp (during chirp idle time) dynamic power save disable override * mode. \n This field provides various RX and TX chain dynamic rapid power save disable * option in inter-chirp idle time. * | Value | Definition | * |-------|----------- | * | 0 | Dynamic Power Save Enable (default)| * | 1 | Dynamic Power Save Disable | * Bit field definition: \n * | Bit Field | Definition | * |-------|----------- | * | Bit 0 | TX PA POWERSAVE_DISABLE control | * | Bit 1 | TX LO POWERSAVE_DISABLE control | * | Bit 2 | RX RF POWERSAVE_DISABLE control | * | Bit 3 | RX BB POWERSAVE_DISABLE control | * | Bit 4 | RX LO POWERSAVE_DISABLE control | * | Bits [7:5] | Reserved | * By default these power save modes are enabled in FECSS. \n * Recommended settings: * | Chirp Idle Time | INTER_CHIRP_PS_DIS | * |-----------------| ------------------ | * | > max of (6us - tx start time, 3.1us) | 0x00 (Power save Enabled) | * | > max of (4us - tx start time, 3.1us) and <= max of (6us - tx start time, 3.1us) | 0x1F (Power save Disabled) | * | < max of (4us - tx start time, 3.1us) | Not Supported idle time | * Note: The minimum idle time can not go lower than max of (4us - tx start time, 3.1us). * */ UINT8 c_InterChirpPsDis;
此致、
海登