请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
主题中讨论的其他器件:OPT3101您好,Gordon
我有一个新问题。
opt3101指定可配置电流值是否为 ILLUM_DAC_H_TX0 x ILLUM_SCALE_H_TX0+ILLUM_DC_CURR_DAC。 最大值为31*5.6ma+7.5ma=181.1。
谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.