This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
工具与软件:
工作环境:IWR6843AOPEMV + MMWAVEICBOOST + DCA1000EVM + Windows 10
目标:通过 Python 脚本控制 DCA1000EVM、以使用 CLI 命令操作 IWR6843AOPEMV 毫米波雷达来进行数据采集。
文件:两个配置文件、 cf.json
和 profile.cfg
、如下所示:
{ "DCA1000Config": { "dataLoggingMode": "raw", "dataTransferMode": "LVDSCapture", "dataCaptureMode": "ethernetStream", "lvdsMode": 2, "dataFormatMode": 3, "packetDelay_us": 25, "ethernetConfig": { "DCA1000IPAddress": "192.168.33.180", "DCA1000ConfigPort": 4096, "DCA1000DataPort": 4098 }, "ethernetConfigUpdate": { "systemIPAddress": "192.168.33.30", "DCA1000IPAddress": "192.168.33.180", "DCA1000MACAddress": "12.34.56.78.90.12", "DCA1000ConfigPort": 4096, "DCA1000DataPort": 4098 }, "captureConfig": { "fileBasePath": "data", "filePrefix": "adc_data", "maxRecFileSize_MB": 1024, "sequenceNumberEnable": 1, "captureStopMode": "infinite", "bytesToCapture": 4000, "durationToCapture_ms": 180000, "framesToCapture": 12000 }, "dataFormatConfig": { "MSBToggle": 0, "laneFmtMap": 0, "reorderEnable": 1, "dataPortConfig": [ { "portIdx": 0, "dataType": "complex" }, { "portIdx": 1, "dataType": "complex" }, { "portIdx": 2, "dataType": "complex" }, { "portIdx": 3, "dataType": "complex" }, { "portIdx": 4, "dataType": "complex" } ] } } }
profile.cfg
用于控制 IWR6843AOPEMV 的内容:
% *************************************************************** % Created for SDK ver:03.06 % Created using Visualizer ver:3.6.0.0 % Frequency:60 % Platform:xWR68xx_AOP % *************************************************************** sensorStop flushCfg % 1:frame based chirps, 2:continuous chirp, 3:adv frame config [1/3] dfeDataOutputMode 1 %* <rxChanEn><TxChanEn><0(cascading)>[15][x][0] channelCfg 15 7 0 %* <numADCBits 0:12bit,1:14bit,2:16bit>[2] % <adcOutputFmt 0:real,1:complex1,2:complex2>[1/2] adcCfg 2 1 %* <subFrameIdx>[-1] % <adcOutFmt 0:Complex,1:Real>[0] % <sampleSwap 0:I in LSB Q in MSB,1 otherwise>[1] % <ChanInterleave 0:Interleaved,1:NonItl>[1] % <ChirpThreshold..MUST be 1 for LVDS>[1] adcbufCfg -1 0 1 1 1 % =========================================================================== %* <profID> <startFreq:GHz> <ideleTime:us> <adcStartTime:us> % <rampEndTime:us> <txOutPower>[0] <txPhaseShift>[0] % <freqSlopeConst:MHz/us> <txStartTime:us> <numAdcSample> % <digOutSampleRate:ksps> % <hpfCornerFreq1 0:175KHz,1:235,2:350,3:700> % <hpfCornerFreq2 0:350KHz,1:700,2:1400,3:2800> % <rxGain> profileCfg 0 60 7 6 60 0 0 64.985 1 256 5000 0 0 48 %* <startIdx> <endIdx> <profID> % <startFreqVar>[0] <freqSlopeVar>[0] <idleTimeVar>[0] % <AdcStartTimeVar>[0] <txEnableMask> chirpCfg 0 0 0 0 0 0 0 1 chirpCfg 1 1 0 0 0 0 0 2 chirpCfg 2 2 0 0 0 0 0 4 %* <startIdx> <endIdx> % <loopNum> <frameNum> <framePerio:ms> % <trigSel 1:Software,2:Hardware>[1] <frameTrigDelay:ms> frameCfg 0 2 16 12000 5 1 0 % =========================================================================== %* <Ignored>[0] <AdcMode 0:Regular,1:LP Mode> lowPower 0 0 % <subFrameIdx For Demo Visualizer,streamed on UART not LVDS>[-1] % <detectedObj 0:disable,1:enable Point Cloud&side info,2:enable PC> % <logMagRange 0:disable,1:enable> % <noiseProf 0:disable,1:enable>[0] % <rangeAziHeatmap 0,1>[0] % <rangeDFSHeatmap 0,1>[0] % <stasInfo 0,1>[0] guiMonitor -1 1 1 0 0 0 1 % Must be two lines % <subFrameIdx> <procDirection> <mode> <noiseWin> % <guardLen> <divShift> <cyclic mode or Wrapped around mode> <Threshold scale> <Peak grouping> cfarCfg -1 0 2 8 4 3 0 15.0 1 cfarCfg -1 1 0 4 2 3 1 15.0 1 % <subFrameIdx> <Feature Enabled> <threshold>[0] multiObjBeamForming -1 1 0.5 % <subFrameIdx> <Enable static clutter removal technique>[0] clutterRemoval -1 0 % <subFrameIdx> <Enable DC removal using first few chirps>[0] % <negativeBinIdx> <positiveBinIdx> <numAvg> calibDcRangeSig -1 0 -5 8 256 % <subFrameIdx> <Enable velocity disambiguation technique>[0] extendedMaxVelocity -1 0 % <subFrameIdx> <enabled>[0] <chirp0Idx> <chirp1Idx> % bpmCfg -1 0 0 1 %* <subFramIdx>[-1] <enableHeader 0,1>[0] % <dataFmt 0:HW disable,1:ADC,2:CP_ADC_CQ>[1] <enableSW 0,1>[0] lvdsStreamCfg -1 0 1 0 % <rangeBias> <I/Q Bias compen for 3Tx*4Rx> compRangeBiasAndRxChanPhase 0.0 1 0 -1 0 1 0 -1 0 1 0 -1 0 1 0 -1 0 1 0 -1 0 1 0 -1 0 % <disable compRangeBiasAndRxChanPhase>[0] <targetDistance> <searchWin> measureRangeBiasAndRxChanPhase 0 1.5 0.2 % <profile> <satMonSel> <priSliceDuration> <numSlices> <rxChanMask> CQRxSatMonitor 0 3 5 121 0 % <profile> <numSlices> <numSamplePerSlice> CQSigImgMonitor 0 127 4 % <disable CQRxSatMonitor 0,1>[0] <disable CQSigImgMonitor 0,1>[0] analogMonitor 0 0 % <subFrameIdx>[-1] <minAzimuthDeg> <maxAzimuthDeg> % <minElevationDeg> <maxElevationDeg> aoaFovCfg -1 -90 90 -90 90 % <subFrameIdx>[-1] <0:range,1:Doppler> % <min> <max> cfarFovCfg -1 0 0 8.92 cfarFovCfg -1 1 -1 1.00 % <save enable> <restore enable> <Flash offset> calibData 0 0 0 sensorStart
问题:
在该 profile.cfg
文件中、我 frameCfg
按如下方式设置了参数:
frameCfg 0 2 16 12000 5 1 0
当 loopNum
设置为16时、可以启动毫米波雷达来收集数据。 但是、当我设置 loopNum
为1时、将无法使用以下配置收集任何数据:
frameCfg 0 2 1 12000 5 1 0
然而,在 Wmare Studio 中,我可以将"线性调频脉冲循环数"设置为1 ,这对应于 loopNum
中 frameCfg
。 在 Wmare Studio 中,我可以成功获取数据,但在使用 Python 脚本控制的 CLI 命令时,我无法收集数据。
是否存在配置不正确的参数? 或者不支持设置 loopNum
为1吗?
当 loopNum 设置为介于1和8之间的值时、毫米波雷达无法收集数据。 但是、当该值设置为介于9和32之间的数字时、毫米波雷达能够收集数据。
我没有使用 mmWave Studio 软件来收集数据。 相反、我利用 Python 脚本在 Windows 10上运行 DCA1000EVM_CLI_Control.exe 和 DCA1000EVM_CLI_Record.exe、以收集毫米波雷达数据。 Python 脚本将 cf.json 和 profile.cfg 等配置文件传输到 DCA1000和 IWR6843AOP。
我录制了一段视频、其中展示了收集毫米波雷达数据以及对 loopNum 配置参数进行修改的现场过程。 有关详细信息、请参阅视频。
mmware_sdk_collect_data.mp4
您好!
我们不能以您使用这些工具的方式支持这些工具。 我建议您使用 mmWave Studio、或者直接丢弃前8个样本、每次收集9个样本。
此致!
耐特