This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] PMP10098:使用电流检测电阻来限制负载电流、所用变压器的功率传输计算、在低输入电压范围内调节12V 输出轨

Guru**** 2931100 points

Other Parts Discussed in Thread: PMP10098

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/tools/simulation-hardware-system-design-tools-group/sim-hw-system-design/f/simulation-hardware-system-design-tools-forum/1504406/pmp10098-limiting-load-current-using-current-sense-resistor-power-transfer-calculations-of-transformer-used-regulating-12v-output-rail-at-low-input-voltage-range

部件号:PMP10098
主题中讨论的其他部件: PMP

工具/软件:

您好、  

我讲解了 PMP10098的原理图、这是一款采用反激式拓扑的 LM3481MM 离线开关评估板。

链接: https://www.ti.com/tool/PMP10098

e2e.ti.com/.../0083.Schematic.pdflOAFthere 是否有针对该 EVM 的任何设计计算文档?