This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] UCC28056:UCC28056

Guru**** 2908170 points
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/tools/simulation-hardware-system-design-tools-group/sim-hw-system-design/f/simulation-hardware-system-design-tools-forum/1514779/ucc28056-ucc28056

器件型号:UCC28056

工具/软件:

我希望设计一个 PFC 来满足以下要求:

输入电压:240VAC
输入频率:50Hz
输出电压:380V 直流
输出功率:180W

请提供参考设计。