This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TIDA-01371:关于TPS7A3301RGWR的负压输出

Guru**** 2933110 points
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/tools/simulation-hardware-system-design-tools-group/sim-hw-system-design/f/simulation-hardware-system-design-tools-forum/1558235/tida-01371-tps7a3301rgwr

器件型号:TIDA-01371


工具/软件:

您好、关于负压输出我有一个问题、我用的是该设计方案的pcb源板进行调试、VCNTRL(-ve)为 Neg大概为–0.1V(-GND-)的21倍、但是TPS7A3301RGWR的输出电压相比于Virtual VCNTRL Neg为0电势、其中-ve VIN电压是-GND-、测量c14两端电压为–12v、但是输出电压(相比于Virtual –3.3V)为0v、也就是c15两端电压为0v、请问问题可能出在哪里-GND-Neg、运放电源vcc为12v、输出的Virtual