This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TPSM82822:PSM82822SILR 能否输出负电压?

Guru**** 2931100 points
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/tools/simulation-hardware-system-design-tools-group/sim-hw-system-design/f/simulation-hardware-system-design-tools-forum/1638121/tpsm82822-can-the-psm82822silr-output-a-negative-voltage

器件型号: TPSM82822

你(们)好

当输入电压为 3.3V~4.2V 时、PSM82822SILR 是否输出负 2.2V 电压?