This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TIDA-00795:TIDA-00795、ucc27712-Q1

Guru**** 2528330 points
Other Parts Discussed in Thread: UCC27712-Q1

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/tools/simulation-hardware-system-design-tools-group/sim-hw-system-design/f/simulation-hardware-system-design-tools-forum/1020131/tida-00795-tida-00795-ucc27712-q1

器件型号:TIDA-00795
主题中讨论的其他器件:UCC27712-Q1

你(们)好

我正在寻找几乎相同的解决方案、但我的信号可以双向流动、最高可达300V

我想使用2 N 沟道 MOSFET 作为双向 SW、但无法生成如此高(315V)的 Vgate

我应该使用什么电路?  ucc27712-Q1是否可以完成此工作?

Thx

Eli