请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:LM5122 主题中讨论的其他器件:TPS43060
工具/软件:WEBENCH设计工具
我使用以下输入:
12V-16V 至36.00V @ 4A
计算成功、但占空比图看起来很奇怪
此外、如果我尝试更改频率、我会看到一个错误"设计更新失败-此器件/拓扑不支持所需的输出功率。"。 即使我想将其更改为0.1Khz、误差也会始终存在
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.