This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] WEBENCH®︎工具/LMR33630:LMR33630消除了电压波动咨询

Guru**** 2587345 points
Other Parts Discussed in Thread: LMR33630

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/tools/simulation-hardware-system-design-tools-group/sim-hw-system-design/f/simulation-hardware-system-design-tools-forum/960206/webench-tools-lmr33630-lmr33630-eliminates-voltage-fluctuation-consultation

器件型号:LMR33630

工具/软件:WEBENCHRegistered设计工具

我们之前使用过 L6984芯片、但由于输入电压波动为下图所示的黄色线(正常值:24V)、因此输出电压也会像蓝色线一样波动(正常电压值4.7)。 我们想知道、如果输入电压类似于黄线、LMR33630是否能够输出稳定电压(5V)。 如果无法输出稳定的电压、请推荐使用芯片。 我们的要求:输入电压:5-36V,输出电压:5V,谢谢。