请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:PMP21639 主题中讨论的其他器件:UCC28780
您好!
我想知道热像的部件位置、尤其是第7页、第8页中介绍的90VAC、50Hz 输入、20V、3.25A 输出情况下 LMG3411和 UCC28780的位置、以便更好地了解 LMG3411如何变热。 Bx4热像是否位于 LMG3411第8页?
此致、
TI.IMI
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.