This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] WEBENCH®︎工具/LM5166:LM5166:负输出电压

Guru**** 2618835 points

Other Parts Discussed in Thread: LM5166, LM5007

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/tools/simulation-hardware-system-design-tools-group/sim-hw-system-design/f/simulation-hardware-system-design-tools-forum/837787/webench-tools-lm5166-lm5166-negative-output-voltage

器件型号:LM5166
主题中讨论的其他器件: LM5007

工具/软件:WEBENCHRegistered设计工具

团队、

我的客户正在寻找反相降压/升压:36V 输入、-8V 输出@ 0.3A。 我正在查看 LM5166。 这是可行的吗? 如何配置我的设计以成为负输出?