This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] WEBENCH®︎工具/PMP9256:PMP9256

Guru**** 2568585 points
Other Parts Discussed in Thread: LM5122, PMP9256

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/tools/simulation-hardware-system-design-tools-group/sim-hw-system-design/f/simulation-hardware-system-design-tools-forum/847539/webench-tools-pmp9256-pmp9256

器件型号:PMP9256
主题中讨论的其他器件:LM5122

工具/软件:WEBENCHRegistered设计工具

测试 CE102的 EMI 传导问题:

在电源输入上需要一个 LC 滤波器、该滤波器可以抑制200kHz 至5MHz 范围内的发射问题、使用基于 LM5122的演示板 PMP9256原理图设计。