This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TIDA-00443:输入电容 RMS 电流计算

Guru**** 675280 points
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/tools/simulation-hardware-system-design-tools-group/sim-hw-system-design/f/simulation-hardware-system-design-tools-forum/1182784/tida-00443-input-cap-rms-current-calculation

器件型号:TIDA-00443

参考设计文档中的第4.2.6节、我可以发现 IRIPPLE = 2.75A。

我计算了 RMS 电流、如下所示:

所选电容器的数据表显示、在100kHz 时、它可以承载接近2A 的 RMS 电流:

我想知道以下几点:

1.我的 rms 计算是否正确  
2.如果是、为什么在设计中使用两个电容器

谢谢、