This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TINA/Spice/LMZM33603:在 LMZM33603上、我能否在+28V 输入下获得-28V 输出

Guru**** 2556590 points
Other Parts Discussed in Thread: TINA-TI, LMZM33603

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/tools/simulation-hardware-system-design-tools-group/sim-hw-system-design/f/simulation-hardware-system-design-tools-forum/711085/tina-spice-lmzm33603-on-lmzm33603-can-i-get--28v-output-with-28v-input

器件型号:LMZM33603
主题中讨论的其他器件:TINA-TI

工具/软件:TINA-TI 或 Spice 模型

您好!

使用 LMZM33603,我能否设计-28V 和28V 作为输入?

谢谢、

Vinayak