This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] PMP7413:采用 PMP7413的50W、5V 设计参考

Guru**** 2966500 points

Other Parts Discussed in Thread: UCC2897A

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/tools/simulation-hardware-system-design-tools-group/sim-hw-system-design/f/simulation-hardware-system-design-tools-forum/1204271/pmp7413-50w-5v-design-using-pmp7413-reference

器件型号:PMP7413
主题中讨论的其他器件:UCC2897A

您好、TI 团队:

我想使用此参考设计设计设计50W、5V 电源、以便在本设计中实现90%以上的效率、我的输入电压范围是103-127Vac、并且我想此设计的仿真文件能不能请您提供仿真文件以便我可以使用 自行验证设计。

此致、

Mayur Nakarani.